Can i install processor sdk linux for 66ak2g12 and let it work properly on ubuntu 22.04.01?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can i install processor sdk linux for 66ak2g12 and let it work properly on ubuntu 22.04.01?
Can i install processor sdk linux for 66ak2g12 and let it work properly on ubuntu 22.04.01?
The "latest" SDK for this platform requires you to use Ubuntu 18.04, as per SDK setup instructions as https://software-dl.ti.com/processor-sdk-linux/esd/docs/06_03_00_106/linux/Overview_Building_the_SDK.html. This applies to both installing the SDK installer, and also setting up a Yocto build. I would strongly recommend AGAINST using Ubuntu 22.04, as this will very likely cause various issues that you would then need to analyze, understand, and debug yourself - while can be done - will likely not be a good use of your time.
One good way to get this setup on more recent PCs is through using of a virtual machine (for example, VMware Workstation Player, see https://www.vmware.com/products/workstation-player/workstation-player-evaluation.html), then setting up an Ubuntu 18.04-based virtual machine by downloading and installing the appropriate disk image (see https://releases.ubuntu.com/18.04/), and then installing the 66AK2G12 SDK or setting up the Yocto build from within the virtual machine.
Regards, Andreas