This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6442: GPMC settings in SysConfig do not support 16bit data width

Guru 13885 points

Part Number: AM6442
Other Parts Discussed in Thread: SYSCONFIG

Hi, 

Question 1
It seems that the GPMC settings in SysConfig do not support 16bit data width. Please refer to Question 2 ① for details. Please let me know when it will be compatible with 16bit.

Question 2
As a workaround for question 1, I am thinking of configuring the GPMC pin settings in "do not specify a software product" mode.
① **.sysconfig file created by “Specify Software product”

② **.sysconfig file created with “Do not specify Software product”

Please tell me how to use two **.sysconfig files in one project. Note that ① is required for pin settings and initialization (baud rate, etc.) of other peripherals such as UART, and ② is required for GPMC pin settings.

Thanks,

Conor