Other Parts Discussed in Thread: ADS7951, THS10064
Hi, i m using C6742 DSP with ADC ADS7951, could anyone advise where to find the schematic diagram for connecting to this ADC? Please advise thanks.
Hi, i m using C6742 DSP with ADC ADS7951, could anyone advise where to find the schematic diagram for connecting to this ADC? Please advise thanks.
hello Stan woldes,
Thank you for the query.
Any available information would be on TI.com product folder.
We do not have the required information to share.
Please start a thread with title
ADS7951 ADC interface for the ADC team to support.
if you do not have any additional inputs, i can reassign the same thread.
Regards,
Sreenivasa
Hello Stan woldes,
Thanks. Reassigning to the ADC team to check if they have some suggestions.
Regards,
Sreenivasa
Hello Stan woldes,
Thanks.
I guess this is part of the data sheet.
https://www.ti.com/lit/ds/symlink/tms320c6742.pd
Did you have a chance to look at the TRM and the data sheet for the required information.
Regards,
Sreenivasa
Hi Kali your website is not wiring..., i download c6742 data sheet no pin out there..
Hi Kali, the c6742 TRM SPI pin out page 23 is very confusing, why is there so many SPI1_SCS[1] to SPI1_SCS[5] ? Isn't that c6742 only has 1 single channel of SPI? i m using SPI for device communication, i m choosing SPI1_SCS[0] - pin E19, SPI1_SIMO - G17, SPI1_SOMI - H17 and SPI1_CLK - G19. Is this arrangement fine ?
Hello Stan woldes,
he c6742 TRM SPI pin out page 23 is very confusing, why is there so many SPI1_SCS[1] to SPI1_SCS[5] ? Isn't that c6742 only has 1 single channel of SPI?
This may be use case dependent and have no additional thoughts.
i m choosing SPI1_SCS[0] - pin E19, SPI1_SIMO - G17, SPI1_SOMI - H17 and SPI1_CLK - G19. Is this arrangement fine ?
Should be fine.
Regards,
Sreenivasa
Hi Kali, i m designing c6742 with THS10064 ADC, this ADC requires 2 Vref of 1.5v and 3.5v respectively, could you help to advise any circuit that can churn-out 1.5v and 3.5v ? please advise soon.
Hello Stan woldes,
Thank you.
I do not have any recommendations.
I have assigned to the ADC team to support.
Regards,
Sreenivasa