Other Parts Discussed in Thread: TPS65910
Hi Support Team,
The following voltages are applied to the VDDSHVs of AM3352.
VDDSHV1,2,5: 1.8V
VDDSHV3,4,6: 3.3V
3.3V is taken from a different IC from TPS65910,
The rise time of 3.3V is about 2ms faster than 1.8V.
The CPU is operating normally with the current settings,
but the datasheet seems to indicate that 1.8V => 3.3V is appropriate.
Can you please confirm that there is no problem with the above usage?
Best Regards,
Kanae