Hello,
Can you support in extending CDD IPC app example to run on MCU1_0 communicating with MCU2_0 core ?
Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Can you support in extending CDD IPC app example to run on MCU1_0 communicating with MCU2_0 core ?
Regards
Hello,
Since we have cdd ipc app example running on MCU2_1 communicating with MCU2_0 core i am going to extend the example by integrating SCIServer and make freertos instead of baremetal. SCIServer is mandatory to run on MCU1_0 to address the sci client requests ,as we need to create tasks (sci server and IPC) we cannot create a baremetal example so in the below patch attached i have integrated sci server with IPC , keeping sci server as high priority task and another task as IPC.
Steps to apply the patch and see the files changed in Linux machine :
0001-J784S4_MCU1_0_with_MCU2_0.patch
Changes in patch are explained below
1) CddIpcApp.c , major changes in the file where sci server with high priority is integrated along with CDD IPC.
2) CddIpcAppStartup.c , the interrupt routing needs to be taken care as per the mailbox used between MCU1_0 and MCU2_0.
3) CddIpcR5Mpu.c, VRING address and Size needs to match with number of cores in the variant.
4) Cdd_IpcCfg.c and Cdd_IpcCfg.h files needs to be generated from EB tresos tool to communicate with MCU2_0.
5) linker_r5_freertos.lds linker file to match the freertos requirements.
6) makefile & mcusw_mcal_component.mk to include cdd ipc app example to run on MCU1_0.
7) ipc_remote/main_rtos.c to run on MCU2_0 and communicate with MCU1_0 rather than MCU2_1.
Regards
Tarun Mukesh