This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI experts
We plan to use SDK 9.2, but during testing, we found that using the latest script from that website(git.ti.com/.../default_DCC_profile_gen, the generated dcc_2a_wdr. bin and dccvis_wdr. bin did not light up properly.The results are shown in the following figure:
Let me describe the operational steps:
1.download imaging-main.zip
2.Edit x3c configuration file
SENSOR_ID 233 PRJ_DIR ../X3C SENSOR_NAME x3c SENSOR_DCC_NAME SENSOR_OX3C SENSOR_WIDTH 1920 SENSOR_HEIGHT 1280 # 0=RGGB; 1=GRBG; 2=GBRG; 3=BGGR, 4=MONO, #10=RGGI, 11=GRIG, 12=BGGI, 13=GBIG, 14=GIRG, 15=IGGR, 16=GIBG, 17=IGGB COLOR_PATTERN 3 #sensor mode :0 for linear, 1 for WDR WDR_MODE 1 # BIT_DEPTH may be 12, 10, or 8 for linear mode BIT_DEPTH 12 #raw sensor image BIT_DEPTH WDR_BIT_DEPTH 24 #WDR decompanding knee points WDR_KNEE_X 0,1023,1279,1535,2303,2559,2943,3071,3327,3455,3519,3647,3775,3903,3999,4095 WDR_KNEE_Y 0,1023,2047,4095,16383,24575,49151,65535,131071,196607,262143,524287,1048575,2097151,4194303,16777215 #Sensor black level to subtract before decompanding (for linear sensors only and some Sony WDR sensors) BLACK_PRE 0 # Sensor black level to subtract after decompanding (for most WDR sensors and all linear sensors) BLACK_POST 0 # GAMMA value for compressing 20/24-bit WDR raw to 16-bit ISP internal # typically around 50 (0.5) for 24-bit WDR sensors and 70 (0.7) for 20-bit sensors GAMMA_PRE 60 # LSB location for H3A input bit range (from bit-H3A_INPUT_LSB to bit-H3A_INPUT_LSB+9) H3A_INPUT_LSB 0
3.Then enter sensor driver folder and run the "generate_dcc.sh" script from there.At this point, there is a problem of not being able to produce the image
4.I will put the XML file for DCC3.0 generated image quality debugging into sensor driver folder and run the "generate_dcc.sh" script.
5.At this point, there is an issue: Uable to init TIOVX module.As shown in the following figure.
May I ask how to solve this problem?
Hello Peng Qiang,
3.Then enter sensor driver folder and run the "generate_dcc.sh" script from there.At this point, there is a problem of not being able to produce the image
The PRJ_DIR folder must be under imaging/sensor_srv/src, for example, ../../../sensor_drv/src/X3C.
5.At this point, there is an issue: Uable to init TIOVX module.As shown in the following figure.
Would you mind sharing your complete GStreamer pipeline?
In addition, have you validated receiving raw data from the sensor using yavta or v4l2 utility?
Regards,
Jianzhong
Hi jianzhong
The PRJ_DIR folder must be under imaging/sensor_srv/src, for example, ../../../sensor_drv/src/X3C.
After trying to modify the directory location, the screen is still pitch black.
Would you mind sharing your complete GStreamer pipeline?
gst-launch-1.0 \
v4l2src device=/dev/video3 io-mode=5 ! \
video/x-bayer, width=1920, height=1280, format=bggr12, framerate=60/1 ! \
tiovxisp sensor-name=SENSOR_OX3C \
dcc-isp-file=/opt/edgeai-gst-apps/firmwarebuilder_output/pengqiang/dcc_viss_wdr.bin \
sink_0::dcc_2a_file=/opt/edgeai-gst-apps/firmwarebuilder_output/pengqiang/dcc_2a_wdr.bin sink_0::device=/dev/v4l-subdev2 format-msb=11 \
sink_0::pool-size=2 src::pool-size=2 ! \
tiovxldc dcc-file=/opt/edgeai-gst-apps/firmwarebuilder_output/pengqiang/dcc_ldc_wdr.bin sensor-name=SENSOR_OX3C \
sink::pool-size=2 src::pool-size=2 ! \
video/x-raw, format=NV12, width=1920, height=1280,framerate=60/1 ! queue ! \
kmssink driver-name=tidss async=false sync=false
In addition, have you validated receiving raw data from the sensor using yavta or v4l2 utility?
On the left is the result when the wdR_mode parameter is 1 in the configuration file, and on the right is the result of 0. This means that using different bins and the same gst pipeline has different effects.
Hi Jianzhong,
Please allow me to add some more details.
The "unable to init TIOVX module" was seen before, mostly happened when files compiled from firmware builder are not used together(libtivision_app.so.x.x and tispl.bin). As the detail suggests, it should be API mismatch or something similiar.
As for SDK9.2, my experience is that with original file system untouched and dcc_xxx.bin from previous build, the TIOVX module error above will occur. In Peng Qiang's latest reply , the picture in the right captured when running gstreamer with dcc.bin from the SDK9.2. I simply followed the instruction in this link and generated the bins in the linear subdir. The configuration file in use is basically the same as the one in Peng Qiang's initial post, with WDR_MODE = 0 as the only difference.
My first assumption is that in the dcc_xxx.bin there are some API calls that are mismatched. Maybe it would be better to identify the key problems, i.e. differences in utility APIs. Is there any file that lists the modifications in the new SDK?
The second thing is that when generating xmls with the python scripts, numpy will get involved if WDR_MODE = 1. Could the black screen problem be caused by the difference in python verison and/or numpy version?
Regards
Huang Jingjie
The second thing is that when generating xmls with the python scripts, numpy will get involved if WDR_MODE = 1. Could the black screen problem be caused by the difference in python verison and/or numpy version?
If you have numpy installed, the output xml files should be OK.
The difference between 0 and 1 is about WDR decompanding.
Do you see anything if you point the camera to a bright scene?
Hi Gang,
I tried pointing the flashlight of my cell phone to the camra, there was a small but bright round showing in the video stream.
So this could be a data processing issue. Please further discuss the detail with Peng Qiang. Thank you !
Regards,
Huang Jingjie
Hi Gang
I tried pointing the flashlight of my cell phone to the camra, there was a small but bright round showing in the video stream.
The current situation seems to be caused by not enabling the glbce function.
We set sensor_wdr_enable to 1.But without any effect, the picture is still very dark.
May I ask if there are any other parameters in SDK 9.2 that affect image quality?
Hi Gang
At this point, there is an issue: Uable to init TIOVX module.As shown in the following figure.
Replace the XML file in the SDK 9.2 script with the XML file generated by DCC3.0.
The generated dcc_2a_wdr. bin and dccvis_wdr. bin have the issues shown in the above figure.
Is it caused by a mismatch between the XML generated by DCC3.0 and SDK 9.2?
We set sensor_wdr_enable to 1.But without any effect, the picture is still very dark.
May I ask if there are any other parameters in SDK 9.2 that affect image quality?
The tiovx interface should be the same as before.
I am not sure of any recent changes.
In a previous thread about 9.0, there was the same question about WDR.
Jianzhong may comment on if there is any recent changes on gstreamer for enabling WDR.
Is it caused by a mismatch between the XML generated by DCC3.0 and SDK 9.2?
There might be some issue with very old version of XML files, but I don't recall anything for 3.0.
Do you see any difference in the data structures in the header of any XML file?
Hi Peng,
On the left is DCC3.0, and on the right is SDK 9.2 by default
Those differences should not really matter.
Are you able to locate a particular xml file causing the error?
Hi Gang
Among them, x3c is an automatically generated XML file in 9.2, and x3c_ele is an XML file generated in 3.0.
I cannot locate which files are causing the problem by comparing their differences.
Hi Peng,
I cannot locate which files are causing the problem by comparing their differences.
It looks like you used a specially made rgb2rgb xml file which is not supported by DCC.
Please merge your pervious changes under "imaging/algo/dcc/" to support that.