This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
May I have question about AM64x?
Q1
What processing is recommanded for the pin that not listed that how to processing if unused in DS 5.4 Pin Connectivity Requirements ?
Open or pulldown/pullup(in external of SoC)?
Q2
If Q1 answer is open.
Do you recommand to set internal pull up/down? or default setting?
Thanks,
GR
Hello GR,
Thank you for the query.
What processing is recommanded for the pin that not listed that how to processing if unused in DS 5.4 Pin Connectivity Requirements ?
Open or pulldown/pullup(in external of SoC)?
If you do not have a trace connected, you could leave it open.
If you have a TP connected or the GPIO connected to a connector, an external pull is recommended. Pull depends on the future use case.
If Q1 answer is open.
Do you recommand to set internal pull up/down? or default setting?
No issues leaving with default setting.
If customers have some specific requirement to enable the pull , they could enable the internal after power-up.
Regards,
Sreenivasa