Tool/software:
Dear Experts,
I would like to know the maximum voltage of VBST pin when the Vin is 12V, in order to know the ceramic 0.1uF capacitor voltage that I need to place.
current Im using Ceramic Capacitor 0.1uF 25V 5% X7R 0603
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Dear Experts,
I would like to know the maximum voltage of VBST pin when the Vin is 12V, in order to know the ceramic 0.1uF capacitor voltage that I need to place.
current Im using Ceramic Capacitor 0.1uF 25V 5% X7R 0603
Hi Daniel,
The voltage on boot capacitor is about 5.5V, so 25V capacitor is OK.
Regards,
Shipeng