This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: How to Loopback Two Ethernet Ports on AM625 Board for Data Transfer

Part Number: AM625

Tool/software:

Hi,

I have two Ethernet ports available on my AM625 board. I would like to perform a loopback test between these Ethernet ports and transfer data between them.

Could someone guide me on how to configure the Ethernet ports for loopback? Specifically, I need to know:

  • How to set up the loopback for these ports.
  • Which registers need to be configured to enable this functionality.
  • Hi 

    I go threw this document but not able to find out ethernet loopback.

    i explain my doubt below can you please help me out.

    i connect my 2 ethrenet port which is shown in below image

    now my two ethernet ports  ip is mantioned below

    root@ACM1000:~# ifconfig eth0
    eth0 Link encap:Ethernet HWaddr 98:AE:71:04:8F:A4
    inet addr:169.254.2.224 Bcast:169.254.255.255 Mask:255.255.0.0
    inet6 addr: fe80::9aae:71ff:fe04:8fa4/64 Scope:Link
    UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
    RX packets:0 errors:0 dropped:0 overruns:0 frame:0
    TX packets:28 errors:0 dropped:0 overruns:0 carrier:0
    collisions:0 txqueuelen:1000
    RX bytes:0 (0.0 B) TX bytes:3940 (3.8 KiB)

    root@ACM1000:~# ifconfig eth1
    eth1 Link encap:Ethernet HWaddr 98:AE:71:04:8F:A5
    inet addr:192.168.0.225 Bcast:192.168.255.255 Mask:255.255.0.0
    inet6 addr: fe80::9aae:71ff:fe04:8fa5/64 Scope:Link
    UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
    RX packets:0 errors:0 dropped:0 overruns:0 frame:0
    TX packets:28 errors:0 dropped:0 overruns:0 carrier:0
    collisions:0 txqueuelen:1000
    RX bytes:0 (0.0 B) TX bytes:3293 (3.2 KiB)





    Now i trying to ping 192.168.0.225 this ip using my eth0 port using below command
    root@ACM1000:~# ping -I eth0 192.168.0.225
    PING 192.168.0.225 (192.168.0.225) from 169.254.2.224 eth0: 56(84) bytes of data.
    From 169.254.2.224 icmp_seq=1 Destination Host Unreachable
    From 169.254.2.224 icmp_seq=2 Destination Host Unreachable
    From 169.254.2.224 icmp_seq=3 Destination Host Unreachable



    but not able to ping ip using this command 


    my doubt is its possible to ping two ethernet if its connected in loopback and if yes than how ?

  • Hi ,

    Thanks for the logs.

    I am adding Linux networking expert here.

    Please allow some time to review and provide inputs.

    Regards

    Ashwani

  • Hi,

    I answered your question on this thread that you posted.

    Best Regards,

    Schuyler

  • Hi Schuyler 

    Thank for reply

    I have one more question I ask on previous thread 

    You can close this thread.