Hi,
I got Android Gingerbread.2.3.4 up and running on the Beagleboard-xm. I also managed to setup the internet connection as follows:
netcfg usb0 dhcp
setprop net.dns1 8.8.8.8 (8.8.8.8 is the google public dns)
When i ping e.g. google.com from the android prompt it succeeds.
When I open the browser in android it shows the message "No network connection", however, if I ignore that and try to browse to a website, this also succeeds. Surfing the web is no problem.
The problem I face is related to applications that try to access the internet. They all fail to "see" or "detect" the internet connection and then exit or abort.
One of the apps that has this problem is SlideME which can be downloaded from: http://slideme.org/sam2.apk
(SlideME is an android application marketplace)
Any ideas how to fix this? Thanks in advance..
Regards, Benjamin