This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hey there,
I have two questions regarding the power supply and the design of the eval board (AM62A7 / AM62A3 LOW POWER STARTER KIT SK (EVM)
WITH TPS65931211-Q1 PMIC).
Thank you in advance.
Best regards,
Daniel
Hello Daniel,
I have assigned your thread to one of our team members. Please note that this is a holiday week in India. Feel free to ping the thread next week if you do not get a response within a few business days.
Regards,
Nick
Hello Daniel
Is it mandatory to connect VDDSHV5 to a supply voltage or can it be left floating if IO group 5 is not used?
The recommendation is to connect a valid power supply to VDDSHV5.
The schematic of the eval board in pdf file "PROC135A" shows a level translator between AM62A and PMIC (page 33). Why is it used? Datasheet of TPS6593 reads that VIL(DIG) is 0.54 V and VIH(DIG) is 1.26 V for the used IO pin. This should be fine with 1.8 V output of AM62A on "MCU_ERRORn". Do you have further information on this and a recommendation?
Are you checking if the level shifter can be removed?
The SK is a generic design designed parallel to the SOC and PMIC design.
Customer are allowed/encouraged to review and do the required optimization preferably after testing.
Regards,
Sreenivasa
Hello Daniel
Please refer to the notes below the section referenced.
Is it mandatory to connect VDDSHV5 to a supply voltage or can it be left floating if IO group 5 is not used?The recommendation is to connect a valid power supply to VDDSHV5.
5.4 Pin Connectivity Requirements
Regards,
Sreenivasa