This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM57X: Every 600 seconds or so, "Time jumped backwards, rotating."

Part Number: PROCESSOR-SDK-AM57X

Tool/software:

Hi.

I am working to upgrade our project from version 6 to 9 of the linux rt sdk.

Using the new file systems running on target (bb x15) I get new and interesting behavior.

Every 600 seconds or so, time jumps backwards?

Fullscreen
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
root@am57xx-evm:~# [ 1296.309570] systemd-journald[112]: Time jumped backwards, rotating.
[ 1897.645996] systemd-journald[112]: Time jumped backwards, rotating.
[ 2499.001068] systemd-journald[112]: Time jumped backwards, rotating.
[ 3100.349639] systemd-journald[112]: Time jumped backwards, rotating.
[ 3701.700286] systemd-journald[112]: Time jumped backwards, rotating.
[ 4303.054473] systemd-journald[112]: Time jumped backwards, rotating.
root@am57xx-evm:~# timedatectl
Local time: Thu 2024-10-31 14:18:32 UTC
Universal time: Thu 2024-10-31 14:18:32 UTC
RTC time: Thu 2024-10-31 14:18:33
Time zone: UTC (UTC, +0000)
System clock synchronized: yes
NTP service: active
RTC in local TZ: no
root@am57xx-evm:~# timedatectl timesync-status
Server: 104.131.155.175 (0.pool.ntp.org)
Poll interval: 1min 4s (min: 32s; max 34min 8s)
Leap: normal
Version: 4
Stratum: 2
Reference: 408E7A25
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

I am not sure if this is an issue or not and I did not find anything about it on the forum, so I'm asking.

Thanks,

Nathan