This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4AL-Q1: kernel panic SError Interrupt on CPU0, code 0xbf000002

Part Number: TDA4AL-Q1

Tool/software:

Hello TI Experts.

              We are using the TDA4AL platform, version sdk0806. 

              We are currently doing power-on and power-off stress testing. In the tens of thousands of tests on multiple boards, we found that some boards have the following errors with probability. idc_iuni.bin is an application we developed. Sometimes it is printed that it is caused by other applications, such as idc_vial.bin. Temporarily infer that it has nothing to do with our own application, because the entire kernel is dead, and it seems that it is not caused by the upper-level process. So I would like to ask what exactly causes such problems and how to solve them.

             

[    4.354984] SError Interrupt on CPU0, code 0xbf000002 -- SError
[    4.354986] CPU: 0 PID: 382 Comm: idc_iuni.bin Not tainted 5.10.162-imotion 1
[    4.354987] Hardware name: Texas Instruments J721S2 EVM (DT)
[    4.354988] pstate: 40000085 (nZcv daIf -PAN -UAO -TCO BTYPE=--)
[    4.354989] pc : _raw_spin_unlock+0x38/0x48
[    4.354990] lr : handle_irq_event+0x40/0xe0
[    4.354992] sp : ffff8000100031d0
[    4.354993] x29: ffff8000100031d0 x28: ffff00083164cf80
[    4.354997] x27: ffff800010a93480 x26: ffff00082e700f28
[    4.354999] x25: ffff00082d547080 x24: ffff00082d724660
[    4.355002] x23: ffff00083164cf80 x22: ffff00082d724600
[    4.355004] x21: ffff00082d5c4cdc x20: ffff00082d5c4cdc
[    4.355006] x19: ffff00082d5c4c00 x18: 0000000000000000
[    4.355009] x17: 0000000000000000 x16: 0000000000000000
[    4.355011] x15: 0000000000000001 x14: ffff800010003850
[    4.355013] x13: 00000000c0a80162 x12: 0000000000000000
[    4.355016] x11: 0000000000000040 x10: ffff800010a5dd10
[    4.355018] x9 : ffff800010a5dd08 x8 : ffff00082c4c6dd8
[    4.355021] x7 : 0000000000000000 x6 : 0000000000000000
[    4.355023] x5 : ffff80086f0a3000 x4 : ffff800010003200
[    4.355025] x3 : ffff80086f0a3000 x2 : ffff00082d5c4c00
[    4.355027] x1 : ffff00083164cf80 x0 : 0000000100010700
[    4.355030] Kernel panic - not syncing: Asynchronous SError Interrupt
[    4.355054] SMP: stopping secondary CPUs
[    4.355055] Kernel Offset: 0x80000 from 0xffff800010000000
[    4.355056] PHYS_OFFSET: 0x80000000
[    4.355057] CPU features: 0x28040022,20806008
[    4.355059] Memory Limit: none