This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4AL-Q1: Can't boot up devices when camera set up on J721E without Fusion1 RevC (UB960)

Part Number: TDA4AL-Q1

Tool/software:

Hi, TI expert,

We plan a custom board without Fusion1 RevC (UB960), and camera plugin the J721E directly.

Does TI support this case?

Now, I meet a problem, if we set camera plugin to CSI2 pin in J721E board, the device board can't boot up.

For confirmed the SD card boot normally or not, so I recovery to normal setting, the SD can confirmed can boot up the device.

So, does it not support if camera plugin to CSI2 pin?