Other Parts Discussed in Thread: DP83869HM, DP83869
Tool/software:
We are using AM64x GP-EVM board for testing.
Boot congratulation is as follows
Primary boot mode SD Card with FS mode
Secondary boot mode is kept to Ethernet.
This takes approximately 40 seconds to boot into u-boot (confirmed by checking debug messages on UART DEBUG port)
By checking waveforms on SD card clk pin and MDIO pins,
it is observed that when SD card with FS mode is selected as primary, it is accessing Ethernet even though SD card it inserted (SD/CD pin low)
and it takes 40 seconds to get any waveform on SD card CLK.
If both primary and backup device is set to SD card, uboot debug messages appear instantly. Also, waveforms are observed instantly on power up on SD card clk.
Please help decoding this bootup behavior.
-------------------------------------------------------------------------------------------------
Another question regarding ethernet boot, which phy's are supported by internal ROM.
Currently DP83869HM is connected to RGMII2 interface with MDIO0 (phy address set to 00001 with auto negotiation enabled)
Is this phy supported by internal ROM?
--------------------------------------------------------------------------------------------------