Part Number: AM62A7
Other Parts Discussed in Thread: SK-AM62A-LP
Tool/software:
- The background information I know is that PHY can only be used in direct read/write mode.
- And in pipeline mode only 16-byte aligned data can be read with PHY, but how to read non-aligned data correctly in case of 133MHz and DTR 8-IO without PHY?
- TAP read delay can not meet the OSPI NOR Flash read timing requirement in 133MHz and DTR 8-IO condition.
- Because read status register(RDSR) operation can only work in STIG mode, does the controller support use PHY in this mode?
- Other information
- EVB: SK-AM62A-LP, replace the OSPI NAND Flash on board with OSPI NOR Flash
- OSPI NOR Flash EPN: MX66UW2G345G