Part Number: TDA4VM
Tool/software:
Hi Ti Team ,
I am trying to create a firmware for C71x, Its not booting, what can be the possible causes for this.
PFB the error which I am getting
Load Remote Processor 8 with data@addr=0x82000000 16723232 bytes: Success!
sdhci_transfer_data: Transfer data timeout
** fs_devread read error - block
Failed to load '/boot/Image'
** No partition table - mmc 1 **
Couldn't find partition mmc 1:2
Can't set block device
libfdt fdt_check_header(): FDT_ERR_BADMAGIC
No FDT memory address configured. Please configure
the FDT address via "fdt addr <address>" command.
Aborting!
** No partition table - mmc 1 **
Couldn't find partition mmc 1:2
Can't set block device
** No partition table - mmc 1 **
Couldn't find partition mmc 1:2
Can't set block device
** No partition table - mmc 1 **
Couldn't find partition mmc 1:2
Can't set block device
** No partition table - mmc 1 **
Couldn't find partition mmc 1:2
Can't set block device
ERROR: Did not find a cmdline Flattened Device Tree
Could not find a valid device tree
MMC Device 0 not found
no mmc device at slot 0
Card did not respond to voltage select! : -110
mmc_init: -95, time 69
starting USB...
Bus usb@6000000: