This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA785: sysboot[5,6] influence

Part Number: DRA785


Tool/software:

Hi,

according to the DRA78x TRM sysboot[5] controls the ADC clock divider:

0: Divide by 2 (assuming SYS_CLK1 = 27MHz)

1: no division (assuming SYS_CLK1 up to 20MHz)


Our question is what would be the effect of having a SYS_CLK1 of 20MHz and at the same time having sysboot[5]=0?
Would it result in only the ADC_CLK to be slower or are there other side effects?
Moreover, is it possible to overwrite the divide by 2 in SW after booting?


The background is that we might have the issue that even though we have a pullup on sysboot[5] and a SYS_CLK1=20MHz, the sysboot[5] pin might be pulled low in some circumstances by other components on our PCB. Hence, the question whether there are any adverse side effects other than the ADC running at a slower clock.


As a side question: what is the influence of sysboot[6]?
The TRM only mentions that it is reserved and must be pulled low. Is it possible that it causes slow or delayed boot times?

BR,
Jacob