This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: AM5728

Part Number: AM5728

Tool/software:

Hi

We are trying to port bolymin lcd for our am5728 based custom board using ti 9.03 linux sdk.
We made the changes in:-

arch/arm/boot/dts/am57xx-beagle-x15-common.dtsi and

edited the drivers/gpu/drm/panel/panel-simple.c as is required for the said LCD panel.


After compiling the kernel we are able to successfully boot the board with sd card containing the updated zImage and dtbs.


In order to test we ran the modetest utility but we are getting the error as below:-
modetest
trying to open device 'i915'...failed
trying to open device 'amdgpu'...failed
trying to open device 'radeon'...failed
trying to open device 'nouveau'...failed
trying to open device 'vmwgfx'...failed
trying to open device 'omapdrm'...failed
trying to open device 'exynos'...failed
trying to open device 'tilcdc'...failed
trying to open device 'msm'...failed
trying to open device 'sti'...failed
trying to open device 'tegra'...failed
trying to open device 'imx-drm'...failed
trying to open device 'rockchip'...failed
trying to open device 'atmel-hlcdc'...failed
trying to open device 'fsl-dcu-drm'...failed
trying to open device 'vc4'...failed
trying to open device 'virtio_gpu'...failed
trying to open device 'mediatek'...failed
trying to open device 'meson'...failed
trying to open device 'pl111'...failed
trying to open device 'stm'...failed
trying to open device 'sun4i-drm'...failed
trying to open device 'armada-drm'...failed
trying to open device 'komeda'...failed
trying to open device 'imx-dcss'...failed
trying to open device 'mxsfb-drm'...failed
no device found


The following are enabled in the kernel's .config

CONFIG_DRM=y
CONFIG_DRM_OMAP=y
CONFIG_OMAP5_DSS_HDMI=y
CONFIG_DRM_TILCDC=y
CONFIG_DRM_PANEL_LVDS=y
CONFIG_DRM_PANEL_SIMPLE=y
CONFIG_DRM_PANEL_EDP=y
CONFIG_DRM_PANEL_OSD_OSD101T2587_53TS=y
CONFIG_DRM_DISPLAY_CONNECTOR=y
CONFIG_DRM_LVDS_CODEC=y

trying to open device 'omapdrm'...failed


Why is it failing ??

Please help!

Thanks!