Hi,
I tried to build the kernel with the provided Package In TI web. We compiled the kernel with omap3_beagle_defconfig (and) omap2plus_defconfig . in both cases we are getting errors. This is the package we are using AM35x-OMAP35x-LINUX-PSP-04.02.00.07.
Please see the below attached information
omap3_beagle_defconfig:
LD drivers/media/IR/keymaps/built-in.o
LD drivers/media/IR/built-in.o
CC drivers/media/common/tuners/tuner-xc2028.o
In file included from drivers/media/common/tuners/tuner-xc2028.c:21:0:
drivers/media/common/tuners/tuner-xc2028.h:10:26: fatal error: dvb_frontend.h: No such file or directory
compilation terminated.
make[4]: *** [drivers/media/common/tuners/tuner-xc2028.o] Error 1
make[3]: *** [drivers/media/common/tuners] Error 2
make[2]: *** [drivers/media/common] Error 2
make[1]: *** [drivers/media] Error 2
make: *** [drivers] Error 2
omap2plus_defconfig:
CC arch/arm/mach-omap2/omap_twl.o
CC arch/arm/mach-omap2/pmic_tps65023.o
CC arch/arm/mach-omap2/omap-smp.o
AS arch/arm/mach-omap2/omap-headsmp.o
arch/arm/mach-omap2/omap-headsmp.S: Assembler messages:
arch/arm/mach-omap2/omap-headsmp.S:36: Error: selected processor does not support ARM mode `smc #0'
make[1]: *** [arch/arm/mach-omap2/omap-headsmp.o] Error 1
make: *** [arch/arm/mach-omap2] Error 2
Can you please help us to solve.
Thanks
Bhimesh