Other Parts Discussed in Thread: SK-AM62A-LP
Tool/software:
Hi experts,
The DDR part number for the SK-AM62A-LP (PROC135E3) and AM62D-EVM (PROC180E2) is the same, "MT53E1G32D2FW-046."
The frequency settings and other conditions are also the same.
Q1: Do you know if there is a difference in the DDR bus clock settings between these two environments?
Q2: Or could you please tell me where in the SDK the bus clock is set?
When my customer ran an executable binary based on the AM62A SDK (am62ax_mcu_plus_sdk_10_00_00_14) on the SK-AM62A-LP and AM62D-EVM, the performance was same.
However, when they ran an executable binary based on the AM62D SDK (freertos_sdk_am62dx_11_01_00_16) on the SK-AM62A-LP and AM62D-EVM, the performance was slightly slower (SK-AM62A-LP > AM62D-EVM).
This is a confirmation of the speculation that data copying on DDR and heavy use of data cache may be affecting performance.
Best regards,
O.H