Part Number: AM620-Q1
Hello team,
is there some type of selection guide or a table showing compatible flash devices to AM620-Q1 using OSPI?
Specifcally in the TRM the following requirement is mentioned: "When using a OSPI\xSPI\QSPI\SPI flash device greater than 128Mb which supports 3-byte and 4-byte addressing modes, a flash device package with a RESET signal (NOR type memories only) must be used "
In the following E2E there are some NAND Flash recommendations: AM62A7-Q1: Automotive NAND Flash Selection with Available Driver - Processors forum - Processors - TI E2E support forums
The recommended NAND flashes do not have a reset pin so I wonder how the TRM requirement can be fulfilled with these NAND flashes. Or does the TRM mean that there is only a RESET signal needed when NOR flashes are used.
Which NAND flashes do you recommend? I saw on the Starterkit this NAND flash is used: W35N01JW_Datasheet_Brief.pdf . For the application the memory is not enough so another memory is needed.