This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I just updated to 4AI.1.3 release in order to be able to use tesla dsp. I did build android according to release notes plus adding support for tesla in kernel via "make menuconfig" (i.e. selecting the tesla option). I was not able to boot android while tesla support was being enabled. I realized if I remove ducati-m3.bin from /system/vendor/firmware (i.e. disable IPU) or deselect tesla support android will bootup just fine. Could anyone help me out with this thing? Being able to use tesla is the sole reason that I moved to this release ... here is the logcat when both tesla and ipu are enabled and android is not booting up:
E/uim-sysfs( 117): uim: Inside main
E/uim-sysfs( 117): uim:ST built into the kernel ?
E/uim-sysfs( 117): uim:BT driver module un-available...
E/uim-sysfs( 117): uim:BT driver built into the kernel ?
E/uim-sysfs( 117): uim:FM driver module un-available...
E/uim-sysfs( 117): uim:FM driver built into the kernel ?
E/uim-sysfs( 117): uim:GPS driver module un-available...
E/uim-sysfs( 117): uim:GPS driver built into the kernel ?
E/uim-sysfs( 117): uim:FM V4L2 driver module un-available...
I/DEBUG ( 120): debuggerd: Apr 18 2012 16:36:44
E/uim-sysfs( 117): uim:FM V4L2 driver built into the kernel ?
E/uim-sysfs( 117): uim:unable to chmod /dev/radio0, might not exist
E/uim-sysfs( 117): uim:found bluetooth rfkill entry @ 0
E/uim-sysfs( 117):
E/uim-sysfs( 117): uim:changed permissions for /sys/class/rfkill/rfkill0/state(0)
E/uim-sysfs( 117):
V/IMGSRV ( 116): Succesfully loaded gfx modules
E/uim-sysfs( 117): uim: Inside st_uart_config
E/uim-sysfs( 117): uim:install set to 1
E/uim-sysfs( 117): uim:opening /dev/ttyO1, while already open
E/uim-sysfs( 117): uim:cleanup
E/uim-sysfs( 117): uim: Inside set_baud_rate
E/uim-sysfs( 117): uim: set_baud_rate() done
E/uim-sysfs( 117): uim: Setting speed to 3686400
E/uim-sysfs( 117): uim: Inside read_command_complete
E/uim-sysfs( 117): uim: Command complete started
E/uim-sysfs( 117): uim: Inside read_hci_event
E/uim-sysfs( 117): uim: read_hci_event
--------- beginning of /dev/log/system
I/Vold ( 115): Vold 2.1 (the revenge) firing up
E/uim-sysfs( 117): uim: Command complete done
E/uim-sysfs( 117): uim: Speed changed to 3686400
E/uim-sysfs( 117): uim: Inside set_custom_baud_rate
E/uim-sysfs( 117): uim: Changing baud rate to 3686400, flow control to 1
E/uim-sysfs( 117): uim: set_custom_baud_rate() done
E/uim-sysfs( 117): uim: Installed N_TI_WL Line displine
D/Vold ( 115): Volume sdcard state changing -1 (Initializing) -> 0 (No-Media)
I/Netd ( 119): Netd 1.0 starting
V/IMGSRV ( 116): pvrsrvinit complete
I/ ( 124): ServiceManager: 0x1df910
I/SurfaceFlinger( 122): SurfaceFlinger is starting
I/SurfaceFlinger( 122): Could not open sysfs entry(/sys/devices/platform/omapdss/display0/s3d_capable)
I/SurfaceFlinger( 122): SurfaceFlinger's main thread ready to run. Initializing graphics H/W...
D/skia ( 123): SkGraphics::Init() - BLTsville (CPU) dlopen success
D/AndroidRuntime( 123):
D/AndroidRuntime( 123): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
D/AndroidRuntime( 123): CheckJNI is OFF
I/ ( 125): ServiceManager: 0x125c958
D/libEGL ( 122): loaded /system/lib/egl/libGLES_android.so
I/audio_hw_primary( 125): boardtype used: blaze(0)
I/AudioFlinger( 125): Loaded primary audio interface from OMAP audio HW HAL (audio)
I/AudioFlinger( 125): Using 'OMAP audio HW HAL' (audio.primary) as the primary audio interface
I/AudioFlinger( 125): Loaded a2dp audio interface from A2DP Audio HW HAL (audio)
I/CameraService( 125): CameraService started (pid=125)
D/libEGL ( 122): loaded /vendor/lib/egl/libEGL_POWERVR_SGX540_120.so
D/libEGL ( 122): loaded /vendor/lib/egl/libGLESv1_CM_POWERVR_SGX540_120.so
D/libEGL ( 122): loaded /vendor/lib/egl/libGLESv2_POWERVR_SGX540_120.so
I/SurfaceFlinger( 122): EGL informations:
I/SurfaceFlinger( 122): # of configs : 33
I/SurfaceFlinger( 122): vendor : Android
I/SurfaceFlinger( 122): version : 1.4 Android META-EGL
I/SurfaceFlinger( 122): extensions: EGL_KHR_image EGL_KHR_image_base EGL_KHR_image_base EGL_KHR_gl_texture_2D_image EGL_KHR_gl_texture_cubemap_image EGL_KHR_gl_renderbuffer_image EGL_KHR_fence_sync EGL_ANDROID_image_native_buffer EGL_ANDROID_image_native_buffer
I/SurfaceFlinger( 122): Client API: OpenGL ES
I/SurfaceFlinger( 122): EGLSurface: 8-8-8-8, config=0x0
I/SurfaceFlinger( 122): OpenGL informations:
I/SurfaceFlinger( 122): vendor : Imagination Technologies
I/SurfaceFlinger( 122): renderer : PowerVR SGX 540
I/SurfaceFlinger( 122): version : OpenGL ES-CM 1.1
I/SurfaceFlinger( 122): extensions: GL_OES_byte_coordinates GL_OES_fixed_point GL_OES_single_precision GL_OES_matrix_get GL_OES_read_format GL_OES_compressed_paletted_texture GL_OES_point_sprite GL_OES_point_size_array GL_OES_matrix_palette GL_OES_draw_texture GL_OES_query_matrix GL_OES_texture_env_crossbar GL_OES_texture_mirrored_repeat GL_OES_texture_cube_map GL_OES_blend_subtract GL_OES_blend_func_separate GL_OES_blend_equation_separate GL_OES_stencil_wrap GL_OES_extended_matrix_palette GL_OES_framebuffer_object GL_OES_rgb8_rgba8 GL_OES_depth24 GL_OES_stencil8 GL_OES_compressed_ETC1_RGB8_texture GL_OES_mapbuffer GL_OES_EGL_image GL_OES_EGL_image_external GL_EXT_multi_draw_arrays GL_OES_required_internalformat GL_IMG_read_format GL_IMG_texture_compression_pvrtc GL_IMG_texture_format_BGRA8888 GL_EXT_texture_format_BGRA8888 GL_OES_egl_sync GL_IMG_vertex_array_object
I/SurfaceFlinger( 122): GL_MAX_TEXTURE_SIZE = 2048
I/SurfaceFlinger( 122): GL_MAX_VIEWPORT_DIMS = 2048 x 2048
I/SurfaceFlinger( 122): flags = 00010000
I/ti_hwc ( 122): clone region is set to (0,0) to (864,480)
I/ti_hwc ( 122): external display changed (state=0, mirror={disabled tform=0deg}, dock={disabled tform=0deg}, tv=0
I/ti_hwc ( 122): omap4_hwc_device_open(rgb_order=1 nv12_only=0)
I/ti_hwc ( 122): blitter present, blits mode 0, blits policy 0
I/ti_hwc ( 122): Attempting to get framebuffer device info.
D/libEGL ( 178): loaded /system/lib/egl/libGLES_android.so
D/libEGL ( 178): loaded /vendor/lib/egl/libEGL_POWERVR_SGX540_120.so
D/libEGL ( 178): loaded /vendor/lib/egl/libGLESv1_CM_POWERVR_SGX540_120.so
D/libEGL ( 178): loaded /vendor/lib/egl/libGLESv2_POWERVR_SGX540_120.so
E/uim-sysfs( 117): uim: Inside st_uart_config
E/uim-sysfs( 117): uim: Un-Installed N_TI_WL Line displine
E/uim-sysfs( 117): uim:cleanup
I/SamplingProfilerIntegration( 123): Profiling disabled.
I/Zygote ( 123): Preloading classes...
D/dalvikvm( 123): GC_EXPLICIT freed 36K, 84% free 409K/2560K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 4K, 82% free 474K/2560K, paused 0ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 20K, 81% free 509K/2560K, paused 0ms+0ms
D/dalvikvm( 123): GC_EXPLICIT freed 27K, 80% free 537K/2560K, paused 0ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 15K, 78% free 576K/2560K, paused 0ms+0ms
D/dalvikvm( 123): GC_EXPLICIT freed 27K, 77% free 603K/2560K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 30K, 76% free 636K/2560K, paused 2ms+1ms
D/TextLayoutCache( 123): Using debug level: 0 - Debug Enabled: 0
W/Zygote ( 123): Class not found for preloading: android.media.AudioManager$2
I/dalvikvm( 123): threadid=1: recursive native library load attempt (/system/lib/libmedia_jni.so)
D/MtpDeviceJNI( 123): register_android_mtp_MtpDevice
I/dalvikvm( 123): threadid=1: recursive native library load attempt (/system/lib/libmedia_jni.so)
I/dalvikvm( 123): threadid=1: recursive native library load attempt (/system/lib/libmedia_jni.so)
W/Zygote ( 123): Class not found for preloading: android.media.IRemoteControlClientDispatcher
W/Zygote ( 123): Class not found for preloading: android.media.IRemoteControlClientDispatcher$Stub
D/dalvikvm( 123): GC_EXPLICIT freed 20K, 74% free 674K/2560K, paused 1ms+1ms
D/dalvikvm( 123): GC_FOR_ALLOC freed 216K, 63% free 969K/2560K, paused 7ms
D/dalvikvm( 123): GC_EXPLICIT freed 44K, 60% free 1025K/2560K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 27K, 59% free 1054K/2560K, paused 2ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 8K, 57% free 1102K/2560K, paused 2ms+3ms
D/dalvikvm( 123): GC_EXPLICIT freed 23K, 55% free 1168K/2560K, paused 2ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 48K, 44% free 1446K/2560K, paused 0ms+1ms
W/Zygote ( 123): Class not found for preloading: android.text.TextDirectionHeuristics$CharCount
W/Zygote ( 123): Class not found for preloading: android.text.method.WordIterator$1
D/dalvikvm( 123): GC_EXPLICIT freed 34K, 43% free 1481K/2560K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 32K, 42% free 1503K/2560K, paused 1ms+1ms
I/dalvikvm( 123): threadid=1: recursive native library load attempt (/system/lib/libwebcore.so)
D/dalvikvm( 123): No JNI_OnLoad found in /system/lib/libchromium_net.so 0x0, skipping init
D/dalvikvm( 123): GC_EXPLICIT freed 26K, 40% free 1552K/2560K, paused 2ms+1ms
W/Zygote ( 123): Class not found for preloading: android.widget.EdgeGlow
D/dalvikvm( 123): GC_EXPLICIT freed 25K, 39% free 1581K/2560K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 71K, 37% free 1626K/2560K, paused 1ms+2ms
E/PhonePolicy( 123): Could not preload class for phone policy: com.android.internal.policy.impl.PhoneWindow$ContextMenuCallback
D/dalvikvm( 123): GC_EXPLICIT freed 33K, 36% free 1648K/2560K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 28K, 35% free 1676K/2560K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 26K, 34% free 1707K/2560K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 32K, 33% free 1733K/2560K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 31K, 32% free 1761K/2560K, paused 2ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 71K, 30% free 1816K/2560K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 39K, 29% free 1832K/2560K, paused 1ms+1ms
I/System ( 123): Loaded time zone names for in 545ms (541ms in ICU)
I/System ( 123): Loaded time zone names for en_US in 277ms (272ms in ICU)
D/dalvikvm( 123): GC_EXPLICIT freed 324K, 24% free 1949K/2560K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 15K, 22% free 2010K/2560K, paused 2ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 51K, 21% free 2042K/2560K, paused 2ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 29K, 20% free 2072K/2560K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 37K, 19% free 2088K/2560K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 32K, 18% free 2111K/2560K, paused 2ms+2ms
I/Zygote ( 123): ...preloaded 2297 classes in 3191ms.
D/dalvikvm( 123): GC_EXPLICIT freed 22K, 18% free 2115K/2560K, paused 2ms+1ms
I/Zygote ( 123): Preloading resources...
D/dalvikvm( 123): GC_EXPLICIT freed 13K, 16% free 2154K/2560K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 22K, 15% free 2199K/2560K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 32K, 12% free 2269K/2560K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 16K, 11% free 2302K/2560K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 15K, 9% free 2337K/2560K, paused 2ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 17K, 8% free 2373K/2560K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 18K, 9% free 2408K/2627K, paused 2ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 19K, 7% free 2446K/2627K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 18K, 8% free 2481K/2691K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 24K, 9% free 2530K/2755K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 18K, 7% free 2565K/2755K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 19K, 8% free 2603K/2819K, paused 2ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 19K, 7% free 2641K/2819K, paused 2ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 22K, 7% free 2686K/2883K, paused 2ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 18K, 8% free 2729K/2947K, paused 2ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 17K, 7% free 2764K/2947K, paused 2ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 19K, 7% free 2802K/3011K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 19K, 6% free 2840K/3011K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 21K, 7% free 2882K/3075K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 18K, 6% free 2917K/3075K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 20K, 6% free 2956K/3139K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 21K, 7% free 2997K/3203K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 17K, 6% free 3033K/3203K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 19K, 5% free 3071K/3203K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 17K, 5% free 3105K/3267K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 20K, 6% free 3144K/3331K, paused 1ms+3ms
D/dalvikvm( 123): GC_EXPLICIT freed 19K, 5% free 3184K/3331K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 23K, 5% free 3233K/3395K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 17K, 6% free 3267K/3459K, paused 2ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 15K, 5% free 3302K/3459K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 15K, 6% free 3336K/3523K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 15K, 5% free 3370K/3523K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 17K, 6% free 3406K/3587K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 18K, 5% free 3442K/3587K, paused 2ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 18K, 5% free 3477K/3651K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 19K, 4% free 3515K/3651K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 19K, 5% free 3552K/3715K, paused 2ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 23K, 4% free 3596K/3715K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 19K, 4% free 3633K/3779K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 20K, 5% free 3675K/3843K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 20K, 4% free 3714K/3843K, paused 2ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 19K, 4% free 3752K/3907K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 20K, 3% free 3792K/3907K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 20K, 4% free 3831K/3971K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 46K, 3% free 3928K/4035K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 44K, 3% free 4005K/4099K, paused 4ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 22K, 3% free 4043K/4163K, paused 2ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 24K, 4% free 4092K/4227K, paused 2ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 18K, 3% free 4130K/4227K, paused 2ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 33K, 3% free 4203K/4291K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 40K, 4% free 4285K/4419K, paused 3ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 19K, 3% free 4326K/4419K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 22K, 3% free 4365K/4483K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 42K, 4% free 4454K/4611K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 18K, 3% free 4491K/4611K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 25K, 5% free 4546K/4739K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 276K, 10% free 5167K/5699K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 18K, 9% free 5207K/5699K, paused 2ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 18K, 9% free 5242K/5699K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 17K, 8% free 5275K/5699K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 19K, 7% free 5314K/5699K, paused 2ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 21K, 6% free 5358K/5699K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 25K, 6% free 5414K/5699K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 18K, 5% free 5454K/5699K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 189K, 5% free 5885K/6147K, paused 2ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 52K, 6% free 5984K/6339K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 21K, 5% free 6027K/6339K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 10K, 5% free 7072K/7427K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 5K, 5% free 8093K/8515K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 16K, 5% free 8128K/8515K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 19K, 5% free 8161K/8515K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 17K, 4% free 8195K/8515K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 17K, 4% free 8229K/8515K, paused 2ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 22K, 3% free 8270K/8515K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 20K, 3% free 8307K/8515K, paused 2ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 21K, 3% free 8343K/8515K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 19K, 2% free 8382K/8515K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 20K, 2% free 8420K/8515K, paused 2ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 19K, 1% free 8457K/8515K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 25K, 1% free 8510K/8579K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 16K, 2% free 8544K/8643K, paused 2ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 22K, 2% free 8591K/8707K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 18K, 1% free 8629K/8707K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 17K, 1% free 8662K/8707K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 18K, 1% free 8695K/8771K, paused 2ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 18K, 1% free 8731K/8771K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 39K, 2% free 8810K/8899K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 23K, 2% free 8856K/8963K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 23K, 1% free 8907K/8963K, paused 2ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 22K, 1% free 8954K/9027K, paused 1ms+1ms
D/dalvikvm( 123): GC_EXPLICIT freed 21K, 1% free 9003K/9027K, paused 2ms+2ms
I/Zygote ( 123): ...preloaded 379 resources in 2394ms.
I/Zygote ( 123): ...preloaded 31 resources in 9ms.
D/dalvikvm( 123): GC_EXPLICIT freed 36K, 1% free 9019K/9091K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed 10K, 1% free 9009K/9091K, paused 1ms+2ms
D/dalvikvm( 123): GC_EXPLICIT freed <1K, 1% free 9009K/9091K, paused 1ms+2ms
I/dalvikvm( 123): System server process 186 has been created
I/Zygote ( 123): Accepting command socket connections
E/BatteryService( 186): batteryPresentPath not found
E/BatteryService( 186): batteryTechnologyPath not found
I/sysproc ( 186): Entered system_init()
I/sysproc ( 186): ServiceManager: 0x1afd1d0
D/SensorService( 186): nuSensorService starting...
I/SensorService( 186): VTI 3 axis accelerometer
I/SensorService( 186): BH1780gli Light sensor
I/SensorService( 186): SFH7741 Proximity sensor
I/SensorService( 186): BMP085 Pressure sensor
I/SensorService( 186): BMP085 Temperature sensor
I/SensorService( 186): HMC5843 3-Axis Magnetometer
I/sysproc ( 186): System server: starting Android runtime.
I/sysproc ( 186): System server: starting Android services.
D/SensorService( 186): nuSensorService thread starting...
I/sysproc ( 186): System server: entering thread pool.
I/SystemServer( 186): Entered the Android system server!
I/SystemServer( 186): Entropy Service
I/SystemServer( 186): Power Manager
I/SystemServer( 186): Activity Manager
I/ActivityManager( 186): Memory class: 48
W/UsageStats( 186): Usage stats version changed; dropping
I/SystemServer( 186): Telephony Registry
I/ActivityManager( 186): Enabled StrictMode logging for AThread's Looper
I/SystemServer( 186): Package Manager
D/dalvikvm( 186): GC_CONCURRENT freed 328K, 5% free 9201K/9607K, paused 1ms+3ms
D/StrictMode( 186): No activity manager; failed to Dropbox violation.
D/dalvikvm( 186): GC_FOR_ALLOC freed 343K, 7% free 9193K/9799K, paused 33ms
D/dalvikvm( 186): GC_CONCURRENT freed 282K, 5% free 9324K/9799K, paused 2ms+5ms
W/PackageParser( 186): No actions in intent filter at /system/app/Bluetooth.apk Binary XML file line #125
W/PackageParser( 186): Problem in package /system/app/Board_id.apk:
W/PackageParser( 186): Unknown element under <activity>: service at /system/app/Board_id.apk Binary XML file line #11
W/PackageManager( 186): Package com.android.camera desires unavailable shared library com.google.android.media.effects; ignoring!
W/PackageManager( 186): Package com.ti.omap4.android.camera desires unavailable shared library com.google.android.media.effects; ignoring!
W/PackageParser( 186): No actions in intent filter at /system/app/Contacts.apk Binary XML file line #525
D/dalvikvm( 186): GC_CONCURRENT freed 145K, 3% free 9594K/9863K, paused 6ms+3ms
W/PackageManager( 186): Package com.android.gallery3d desires unavailable shared library com.google.android.media.effects; ignoring!
D/dalvikvm( 186): GC_CONCURRENT freed 220K, 4% free 9830K/10183K, paused 5ms+4ms
W/PackageParser( 186): Problem in package /system/app/sensor.test.apk:
W/PackageParser( 186): Unknown element under <activity>: action at /system/app/sensor.test.apk Binary XML file line #27
W/PackageParser( 186): Problem in package /system/app/sensor.test.apk:
W/PackageParser( 186): Unknown element under <activity>: category at /system/app/sensor.test.apk Binary XML file line #28
D/PackageManager( 186): No files in app dir /vendor/app
I/installd( 127): new connection
I/Installer( 186): connecting...
I/PackageManager( 186): Time to scan packages: 2.577 seconds
W/PackageManager( 186): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH.mail in package com.android.contacts
W/PackageManager( 186): Unknown permission android.permission.ADD_SYSTEM_SERVICE in package com.android.phone
W/PackageManager( 186): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH in package com.android.providers.calendar
W/PackageManager( 186): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH.cl in package com.android.providers.calendar
D/dalvikvm( 186): GC_CONCURRENT freed 269K, 4% free 10014K/10375K, paused 6ms+4ms
W/PackageManager( 186): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH.mail in package com.android.calendar
W/PackageManager( 186): Not granting permission android.permission.SEND_DOWNLOAD_COMPLETED_INTENTS to package com.android.browser (protectionLevel=2 flags=0x9be45)
W/PackageManager( 186): Unknown permission android.permission.READ_EXTERNAL_STORAGE in package com.android.videoeditor
W/PackageManager( 186): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH in package com.android.settings
W/PackageManager( 186): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH in package com.android.providers.contacts
W/PackageManager( 186): Unknown permission com.google.android.googleapps.permission.GOOGLE_AUTH.cp in package com.android.providers.contacts
W/PackageManager( 186): Not granting permission android.permission.DEVICE_POWER to package com.android.deskclock (protectionLevel=2 flags=0x8be45)
D/dalvikvm( 186): GC_EXPLICIT freed 287K, 6% free 9914K/10503K, paused 5ms+2ms
I/SystemServer( 186): Account Manager
D/PackageManager( 186): generateServicesMap(android.accounts.AccountAuthenticator): 2 services unchanged
I/SystemServer( 186): Content Manager
D/PackageManager( 186): generateServicesMap(android.content.SyncAdapter): 4 services unchanged
I/ActivityThread( 186): Pub settings: com.android.providers.settings.SettingsProvider
I/SystemServer( 186): System Content Providers
D/SettingsProvider( 186): cache for settings table 'secure' rows=34; fullycached=true
D/SettingsProvider( 186): cache for settings table 'system' rows=51; fullycached=true
I/SystemServer( 186): Lights Service
I/SystemServer( 186): Battery Service
E/BatteryStatsImpl( 186): problem reading network stats
E/BatteryStatsImpl( 186): java.lang.IllegalStateException: problem parsing idx 1
E/BatteryStatsImpl( 186): at com.android.internal.net.NetworkStatsFactory.readNetworkStatsDetail(NetworkStatsFactory.java:300)
E/BatteryStatsImpl( 186): at com.android.internal.net.NetworkStatsFactory.readNetworkStatsDetail(NetworkStatsFactory.java:250)
E/BatteryStatsImpl( 186): at com.android.internal.os.BatteryStatsImpl.getNetworkStatsDetailGroupedByUid(BatteryStatsImpl.java:5736)
E/BatteryStatsImpl( 186): at com.android.internal.os.BatteryStatsImpl.doUnplugLocked(BatteryStatsImpl.java:1420)
E/BatteryStatsImpl( 186): at com.android.internal.os.BatteryStatsImpl.setOnBatteryLocked(BatteryStatsImpl.java:4337)
E/BatteryStatsImpl( 186): at com.android.internal.os.BatteryStatsImpl.setBatteryState(BatteryStatsImpl.java:4396)
E/BatteryStatsImpl( 186): at com.android.server.am.BatteryStatsService.setBatteryState(BatteryStatsService.java:434)
E/BatteryStatsImpl( 186): at com.android.server.BatteryService.processValues(BatteryService.java:252)
E/BatteryStatsImpl( 186): at com.android.server.BatteryService.update(BatteryService.java:234)
E/BatteryStatsImpl( 186): at com.android.server.BatteryService.<init>(BatteryService.java:148)
E/BatteryStatsImpl( 186): at com.android.server.ServerThread.run(SystemServer.java:196)
E/BatteryStatsImpl( 186): Caused by: java.io.FileNotFoundException: /proc/net/xt_qtaguid/stats: open failed: ENOENT (No such file or directory)
E/BatteryStatsImpl( 186): at libcore.io.IoBridge.open(IoBridge.java:406)
E/BatteryStatsImpl( 186): at java.io.FileInputStream.<init>(FileInputStream.java:78)
E/BatteryStatsImpl( 186): at com.android.internal.net.NetworkStatsFactory.readNetworkStatsDetail(NetworkStatsFactory.java:269)
E/BatteryStatsImpl( 186): ... 10 more
E/BatteryStatsImpl( 186): Caused by: libcore.io.ErrnoException: open failed: ENOENT (No such file or directory)
E/BatteryStatsImpl( 186): at libcore.io.Posix.open(Native Method)
E/BatteryStatsImpl( 186): at libcore.io.BlockGuardOs.open(BlockGuardOs.java:110)
E/BatteryStatsImpl( 186): at libcore.io.IoBridge.open(IoBridge.java:390)
E/BatteryStatsImpl( 186): ... 12 more
I/SystemServer( 186): Vibrator Service
I/power ( 186): *** set_screen_state 1
D/dalvikvm( 186): GC_CONCURRENT freed 394K, 5% free 10073K/10567K, paused 6ms+3ms
I/SystemServer( 186): Alarm Manager
I/SystemServer( 186): Init Watchdog
I/SystemServer( 186): Window Manager
I/InputManager( 186): Initializing input manager
W/StatusBarManager( 186): warning: no STATUS_BAR_SERVICE
D/EventHub( 186): No input device configuration file found for device 'hmc5843'.
I/InputManager( 186): Starting input manager
I/WindowManager( 186): Enabled StrictMode for PolicyThread's Looper
I/WindowManager( 186): Enabled StrictMode logging for WMThread's Looper
I/SystemServer( 186): Bluetooth Service
D/EventHub( 186): No input device configuration file found for device 'bmp085'.
I/BluetoothProfileState( 186): Message:Entering Stable State
I/BluetoothProfileState( 186): Message:Entering Stable State
I/BluetoothProfileState( 186): Message:Entering Stable State
I/SystemServer( 186): Input Method Service
W/InputManagerService( 186): Couldn't create dir.: /data/system/inputmethod
D/EventHub( 186): No input device configuration file found for device 'bh1780gli'.
W/ResourceType( 186): Failure getting entry for 0x7f060000 (t=5 e=0) in package 0 (error -75)
I/SystemServer( 186): Accessibility Manager
D/EventHub( 186): No input device configuration file found for device 'cma3000-acclerometer'.
I/Display ( 186): Mirroring region is Rect(0, 0 - 1280, 720)
D/PermissionCache( 122): checking android.permission.ACCESS_SURFACE_FLINGER for uid=1000 => granted (335 us)
I/ActivityManager( 186): Config changed: {1.0 0mcc0mnc en_US layoutdir=0 sw320dp w576dp h294dp nrml long land ?uimode ?night -touch -keyb/v/h -nav/h s.2}
I/SystemServer( 186): Device Policy
I/SystemServer( 186): Status Bar
I/SystemServer( 186): Clipboard Service
I/SystemServer( 186): NetworkManagement Service
I/SystemServer( 186): Text Service Manager Service
I/SystemServer( 186): NetworkStats Service
I/SystemServer( 186): NetworkPolicy Service
I/SystemServer( 186): Wi-Fi P2pService
I/SystemServer( 186): Wi-Fi Service
E/EventHub( 186): could not get driver version for /dev/input/mice, Not a typewriter
E/CommandListener( 119): Failed to open /proc/sys/net/ipv6/conf/wlan0/disable_ipv6: No such file or directory
E/WifiStateMachine( 186): Failed to disable IPv6: java.lang.IllegalStateException: Unable to communicate to native daemon for disabling ipv6
I/SystemServer( 186): Connectivity Service
D/ConnectivityService( 186): ConnectivityService starting up
D/NetworkManagementService( 186): rsp <213 e2:47:39:fc:ef:1c 0.0.0.0 0 [down broadcast multicast]>
D/NetworkManagementService( 186): flags <[down broadcast multicast]>
D/NetworkManagementService( 186): Registering observer
E/MobileDataStateTracker( 186): default: Ignoring feature request because could not acquire PhoneService
E/MobileDataStateTracker( 186): default: Could not enable APN type "default"
D/NetworkManagementService( 186): Registering observer
D/NetworkManagementService( 186): Registering observer
I/WifiService( 186): WifiService starting up with Wi-Fi disabled
I/SystemServer( 186): Throttle Service
I/SystemServer( 186): Mount Service
D/MountService( 186): got storage path: /mnt/sdcard description: Internal Storage primary: true removable: false emulated: true mtpReserve: 0 allowMassStorage: false maxFileSize: 0
D/MountService( 186): got storage path: /mnt/ext_sdcard description: SD Card primary: false removable: true emulated: false mtpReserve: 0 allowMassStorage: false maxFileSize: 0
D/MountService( 186): using emulated external storage
I/SystemServer( 186): Notification Manager
I/SystemServer( 186): Device Storage Monitor
I/SystemServer( 186): starting SUPL Service (SystemServer)
D/VoldCmdListener( 115): volume list
D/MountService( 186): volume state changed for /mnt/ext_sdcard (null -> removed)
I/SystemServer( 186): Location Manager
I/SystemServer( 186): Country Detector
D/EventHub( 186): No input device configuration file found for device 'SDP4430 Headset Jack'.
I/EventHub( 186): New device: id=5, fd=160, path='/dev/input/event9', name='SDP4430 Headset Jack', classes=0x80, configuration='', keyLayout='', keyCharacterMap='', builtinKeyboard=false
D/EventHub( 186): No input device configuration file found for device 'sfh7741'.
D/dalvikvm( 186): GC_CONCURRENT freed 247K, 4% free 10346K/10695K, paused 3ms+5ms
D/Ethernet( 186): Interface eth0 link up
I/SystemServer( 186): Search Service
I/SystemServer( 186): DropBox Service
I/SystemServer( 186): Wallpaper Service
D/EventHub( 186): No input device configuration file found for device 'omap4-keypad'.
I/SystemServer( 186): Audio Service
I/EventHub( 186): New device: id=7, fd=120, path='/dev/input/event0', name='omap4-keypad', classes=0x23, configuration='', keyLayout='/system/usr/keylayout/omap4-keypad.kl', keyCharacterMap='/system/usr/keychars/omap4-keypad.kcm', builtinKeyboard=true
I/EventHub( 186): New device: id=8, fd=119, path='/dev/input/event2', name='syn_tm12xx_ts_2', classes=0x105, configuration='/system/usr/idc/syn_tm12xx_ts_2.idc', keyLayout='/system/usr/keylayout/qwerty.kl', keyCharacterMap='/system/usr/keychars/qwerty.kcm', builtinKeyboard=false
E/EventHub( 186): could not get driver version for /dev/input/mouse1, Not a typewriter
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/EventHub( 186): New device: id=9, fd=163, path='/dev/input/event1', name='syn_tm12xx_ts_1', classes=0x105, configuration='/system/usr/idc/syn_tm12xx_ts_1.idc', keyLayout='/system/usr/keylayout/qwerty.kl', keyCharacterMap='/system/usr/keychars/qwerty.kcm', builtinKeyboard=false
E/EventHub( 186): could not get driver version for /dev/input/mouse0, Not a typewriter
D/EventHub( 186): No input device configuration file found for device 'twl6030_pwrbutton'.
I/EventHub( 186): New device: id=10, fd=164, path='/dev/input/event6', name='twl6030_pwrbutton', classes=0x1, configuration='', keyLayout='/system/usr/keylayout/twl6030_pwrbutton.kl', keyCharacterMap='/system/usr/keychars/Generic.kcm', builtinKeyboard=false
I/InputReader( 186): Device added: id=10, name='twl6030_pwrbutton', sources=0x00000101
I/InputReader( 186): Touch device 'syn_tm12xx_ts_1' could not query the properties of its associated display 0. The device will be inoperable until the display size becomes available.
I/InputReader( 186): Device added: id=9, name='syn_tm12xx_ts_1', sources=0x01001113
I/InputReader( 186): Touch device 'syn_tm12xx_ts_2' could not query the properties of its associated display 0. The device will be inoperable until the display size becomes available.
I/InputReader( 186): Device added: id=8, name='syn_tm12xx_ts_2', sources=0x01001113
I/InputReader( 186): Device added: id=0, name='omap4-keypad', sources=0x00000301
I/InputReader( 186): Device added: id=5, name='SDP4430 Headset Jack', sources=0x80000000
I/ActivityManager( 186): Config changed: {1.0 0mcc0mnc en_US layoutdir=0 sw320dp w576dp h294dp nrml long land ?uimode ?night finger qwerty/v/v dpad/v s.3}
I/InputReader( 186): Reconfiguring input devices. changes=0x00000004
I/InputReader( 186): Device reconfigured: id=8, name='syn_tm12xx_ts_2', surface size is now 864x480, mode is 1
I/InputReader( 186): Device reconfigured: id=9, name='syn_tm12xx_ts_1', surface size is now 864x480, mode is 1
I/ServiceManager( 186): Waiting for service media.audio_policy...
D/DhcpInfoInternal( 186): makeLinkProperties with empty dns2!
D/DhcpInfoInternal( 186): makeLinkProperties with empty dns2!
D/ConnectivityService( 186): ConnectivityChange for ETHERNET: CONNECTED/CONNECTED
D/ConnectivityService( 186): ConnectivityChange for ETHERNET: CONNECTED/CONNECTED
D/ConnectivityService( 186): handleConnectivityChange: address are the same reset per doReset linkProperty[9]: resetMask=0
D/DhcpInfoInternal( 186): makeLinkProperties with empty dns2!
D/ConnectivityService( 186): ConnectivityChange for ETHERNET: CONNECTED/CONNECTED
D/ConnectivityService( 186): handleConnectivityChange: address are the same reset per doReset linkProperty[9]: resetMask=0
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
D/dalvikvm( 186): GC_CONCURRENT freed 277K, 4% free 10466K/10887K, paused 3ms+3ms
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
W/AudioSystem( 186): AudioPolicyService not published, waiting...
I/ServiceManager( 186): Waiting for service media.audio_policy...
I/ServiceManager( 186): Waiting for service media.audio_policy...
Hi Alireza,
Tesla software build instructions are not available as a part of the release package for 4AI.x.x releases. Could you please let me know where did you get the reference to enable tesla software? Also please let me know which board are you using to test this. Is it Panda/Blaze or Blaze tablet?
Regards,Satheesh
Hi Satheesh,
I've found the Tesla build instructions in http://omappedia.org/wiki/RPMsg_Tesla . Also I am using the Blaze board. Thanks a lot for your concern.
Alireza
Hi Alireza:
Could you attach a text file with kernel logs too? (to make it easier to read than in the message body)
Regards,
Rodrigo
Hi Alireza:
You may want to move to 4AI.1.4 since modifications on the kernel to support tesla are too new to be included at 4AI.1.3, and make sure to distclean your kernel repository before creating your tesla supporting kernel image. I tested tesla on 4AI.1.4 and seems to be working fine.
http://omappedia.com/wiki/4AI.1.4_OMAP4_Icecream_Sandwich_Release_Notes
Regards,
Rodrigo