This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Configure a DSP/BIOS project on a homemade platform with CCS5.1



Hi all.

First of all, I'd like to apologize: I'm pretty sure my question is dumb, but really, it's been hours I'm trying to solve it, and I don't know what to do anymore... :p

So, here is my problem: I made a project with a TMS320C5502 on it, that can communication with an external ASRAM via the EMIF controller. So, i'd like to create a project, that will use DSP/BIOS v5 (since the V6 is not avaiable for my device...) and the functions associated with the EMIF, the GPIO, etc... I found some documentation, but nothing is up to date...

So, what I did is to set up a project with code studio (v5.1), and I used the "hello world" exemple. First big problem: there is a lot of evaluation board, but I saw nothing regarding the use of the DSP in a custom environment...

The second problem is that apparently most of the function I need (including GPIO, EMIF, DMA or Cache) are in a Chip Support Library, but when I modify my .tcf file, there is nothing about this library.

And third problem: in some documentation (again, not up do date since it's concerning CCS v4...), i should have a software that let me make a .cbd file. So I would be able to set up, for instance, the clock. But I've found nothing...

So here I am, with a hello world project, and absolutly no idea of how to use it in my application... So how could I set up my environment so I can start working on my code?

Thanks a lot in advance,

Matthieu