This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335X - Ethernet using RMII at 1V8



Hi all,

We are going to implement two ethernet ports 10/100 using two RMII interfaces. The phy we have chosen allow interface to AM335X at 1V8.

Does someone have implemented RMII at 1V8? 

Is there any additional care to be taken in the design or layout?

Thanks

Rodrigo

  • Hello Rodrigo,

    Keep in mind that the RMII(1) and MDIO signalling interfaces share the same voltage supply/domain on AM335x; whichever PHY you select will need to support MDIO at 1.8v as well.

  • Thanks DK for remind us this detail.

    I have one special doubt. In this case using 1V8, would it be possible to use an 1V8 oscillator to source clock to the phy and also the RMII_REFCLK ?

    thanks once again

    Rodrigo

  • Rodrigo,

    Assuming RMII spec VIH(MIN) of RMII_REFCLK @ 1.4V and AM335x RMII(x)_REFCLK VIH(MIN) of (0.65*VDDSHVx (where VDDSHVx=1.8V) = (VIH@1.17V) ), I think this should not present a problem. Depending on the PHY you choose, RMII_REFLK VIH(MIN) can actually be as low as 1.3V @ 1.8V operation.

    There may be other AM335x-specific "gotchas" that I am missing, so I will revisit this subject with the team on Monday.