This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMC (write) speed



Using latest kernel, I noticed slow MMC access. Our board supports both eMMC and micro-SD-card memory.

On both memories, an ext4 fs is installed and mounted with default options. I measured write speeds of about 2MBytes/sec on both flash media.

According to the performance guide http://processors.wiki.ti.com/index.php/AM335x-PSP_04.06.00.07_Features_and_Performance_Guide roughly 8MB should be possible.

I merged also following patch: http://arago-project.org/git/projects/?p=linux-am33x.git;a=commit;h=36800bd1ae85fd459f348323c630fd173a18ba4b

In the board setup file I added following capability: MMC_CAP_4_BIT_DATA

Electrical signals are looking fine on a scope.

Kernel log:

[    1.319458] mmc0: host does not support reading read-only switch. assuming write-enable.
[    1.330474] mmc0: new high speed SDHC card at address 1234
[    1.336700] mmcblk0: mmc0:1234 SA04G 3.63 GiB
[    1.344299]  mmcblk0: p1 p2 p3 p4
[    1.427307] mmc1: new high speed MMC card at address 0001
[    1.433410] usb 2-1: new high-speed USB device number 2 using musb-hdrc
[    1.440612] mmcblk1: mmc1:0001 HYNIX  1.68 GiB
[    1.445648] mmcblk1boot0: mmc1:0001 HYNIX  partition 1 1.00 MiB
[    1.451995] mmcblk1boot1: mmc1:0001 HYNIX  partition 2 1.00 MiB
[    1.460449]  mmcblk1: p1 p2 p3 p4
[    1.466766]  mmcblk1boot1: unknown partition table
[    1.473602]  mmcblk1boot0: unknown partition table

Question:

Does anyone have a suggestion to improve (write) speed?

Best regards,

Wim