This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EMIF-16 example project for TMDSEVM6678

Just started with the 320C6678 eval board, and I am feeling overwhelmed.  Ultimately, I will be using the 6678 (or one of the 2- or 4- core models) to collect data from a PCIe bus and send it through a Cypress USB3 chip to the PC.  I believe the EMIF-16 interface will work well between the dsp and the USB3 chip.  Are there any fairly basic example projects that show setup and use of the EMIF-16? 

Thanks in advance for any suggestions on the best way for someone totally unfamiliar with this DSP to get started.