Dear All,
I noticed that on my DM368 IPNC with SW release 4.0 and after setting clock time in the web pages, the date goes back to the beginning of time (1-1-1970) avec reset/power cycle.
I suspected at first a HW problem, but my cam works fine with 2.6.0 SW release.
So i dug a little deeper and found that 2.6.37 kernel provided with 4.0 release do not integrate RTC support. I also noticed that "TI DaVinci DM365 RTC" driver was not available too, whereas it was available on 2.6.18 kernel provided with 2.6.0 release.
Is there anybody that can tell me how to make work RTC with this new Kernel (Patch / Configuration)
I found here : http://processors.wiki.ti.com/index.php/DaVinci_PSP_03.21.00.04_Release_Notes that RTC should be supported with 2.6.37
Any idea would be really appreciated, i'm a quite lost.
Thanks for advance for your help
Best regards
ADB