This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
I'm using IPNC RDK 4.0. Now, it works well on DM368 and TVP5146. However, the default H264 video stream size is 720 x 480 for NTSC mode, for PAL mode, it should be 720 x 576. Please clarify how to change RDK 4.0 to get video resolution 720 x 576. BTW, if we want to get two output video streams with different resolution 720 x 576, and 352 x 480, how to deal with it using RDK4.0.
Any answer will be really appreciated!
Thanks,
Jesse