This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have three AM335x EVM which I'm using as a starting point for a custom AM335x design. I would like to operate the AM335x base board disconnected from the daughter board and LCD. I have unplugged the daughter board. However, the base board doesn't run any more (i.e. no serial output from UART0). I expect to see "CCCC" come out of UART0 when I power up the base board (from the ROM loader), but I see nothing. Any suggestions?
While running the base board alone is not officially supported, the R472 and R68 were placed to allow testing of the base board alone. If you place a zero ohm resistor on R472 (for V1_8D) and a zero ohm resistor on R68 (for V3_3D), the base board will operate without the daughterboard and LCD board.