This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In Datasheet of C6745 page 93, Table 6-24 EMIFB Supported SDRAM Configurations, we can see that when you use 16bits SDRAM , it needs 2pcs.
It doesn't mention it can support 1pcs 16bits SDRAM in the table .
But in Figure 6-19. EMIFB to 2M × 16 × 4 bank SDRAM Interface , it shows 1pcs 16bits SDRAM connected to C6745.
My question is as following :
Can I use only 1pcs 16bits SDRAM (Such as EM639165TS-6G) for DSP C6745 ?
Thanks !
jintao
Jintao
Yes, C6745 supports one 16 bit SDRAM.
Thanks
David