This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Are there any performance android benchmarking tools i can use to test my omap4 custom board.
Also, Can i get the performance numbers for blaze/blaze tablet. I am looking for 2D/3D graphics ests that i can use.
Thanks,
Sriram
Sriram,
I am splitting this into a new thread.
Regards,
Gina
Sriram,
You can register on the PVR developers website (http://www.imgtec.com/) to make use of the PVR tools they provide for performance testing. For performance numbers on Blaze Tablet, please contact your TI representative.
Regards,
Gina
Thanks for the response. I tried to use memory bandwith measurement tool omapconf on a custom board
when i run that. I get an error, Any ideas on why this could occur. Obviosly it is trying to access an address
for which the clock is turned on or is illegal. Everytime i run this tool i get a crash at a different address.
I see the same behaviour on panda. Are there any pre-requisites for running this?
Any help on where i should look?
Thanks.
Error message:
HW Platform Revision:
OMAP4430 ES2.3 GP Device (STANDARD performance (1.0GHz))
TWL6030 ES2.1 (EPROM rev7.0)
TWL6040 ES2.0
SW Build Details:
Build:
Version: vsr-userdebug 4.0.4 IMM76L eng.build.20121128.121745 test-keys
Pastry: Ice Cream Sandwich
Type: userdebug
Date: Wed Nov 28 12:19:05 IST 2012
Kernel:
Version: 3.0.31-01881-ga31ecaa[ 56.557037] Unhandled fault: external abort on non-linefetch (0x1018) at 0x403d5000
-dirty
Author: sriram@hostpc
Toolchain: gcc version 4.4.1 (Sourcery G++ Lite 2010q1-202)
Type: #518 SMP PREEMPT
Date: Wed Nov 28 17:41:36 IST 2012
Counter: 0 Master: alldmm Transaction: w Probe: emif1
Counter: 1 Master: alldmm Transaction: w Probe: emif2
Counter: 2 Master: alldmm Transaction: r Probe: emif1
Counter: 3 Master: alldmm Transaction: r Probe: emif2
delay in us: 1000000
overflow delay in us: 1000000 (iterations=1)
accumulation type: 2
iterations (0=infinite): 0
Overflow counter index: DISABLED (overflow delay used)
Overflow threshold: DISABLED (overflow delay used)
!!! OUPS... MEMORY ERROR @ 0x00000000 !!!
Are you sure that:
MEMORY ADDRESS IS VALID?
TARGETED MODULE IS CLOCKED?