Hi.
NOW I'm using SPL & U-boot with SPI Flash boot
it's config current SPI Flash status
SPI flash is (SPL + U-BOOT ) then Nand is (Kernel , UBIFS )
it's success boot...finish
But
i want change SPI Flash ONLY
i' want plan SPI flash ( SPL + U-boot + kernel + UBIFS ) .
After boot finish then nand mount
i know that possible spi flash with kernel
But .
Is it possible only spi flash boot with UBIFS , now env is config only jffs2
if it possible , how can it change boot env and the other thing (kernel code ,,,etc)
Thank you
Kind Regards,