Other Parts Discussed in Thread: ASH, TPS65910
Hi All
I am using W25Q64CV SPI NOR flash on am335x evm processor. I have performed MTD partition from u-boot and and passing the arguments from command line to kernel. The problem I am facing is UBIFS mount of the ubinized filesystem as seen in kernel log. The filesystem is fine when in sdcard boot. I have added some debug messages manually in the kernel code and it shows till ui_io_read function.
My bootargs:
setenv spiargs 'setenv bootargs console=${console} noinitrd ip=off mem=256M ${mtdparts} ${optargs} ubi.mtd=4,64 rootfstype=ubifs root=/dev/mtdblock4 init=/bin/ash'
setenv spiboot "echo Booting from SPI ...; run spiargs; sf probe ${spibusno}:0; sf read ${fdtaddr} 0xA1000 0x10000; sf read ${loadaddr} 0xC0000 0x320000; bootz ${loadaddr} - ${fdtaddr}"
run spiboot
******************************************************************************
Below shows some of U-boot information
U-Boot# sf probe 0
SF: Detected W25Q64CV with page size 256 Bytes, erase size 4 KiB, total 8 MiB
U-Boot# mtdparts
device nor0 <w25q64cv-flash.0>, # parts = 5
#: name size offset mask_flags
0: MLO 0x00020000 0x00000000 0
1: u-boot 0x00080000 0x00020000 0
2: dtb 0x00020000 0x000a0000 0
3: kernel 0x00320000 0x000c0000 0
4: rootfs 0x00420000 0x003e0000 0
active partition: nor0,0 - (MLO) 0x00020000 @ 0x00000000
defaults:
mtdids : nor0=w25q64cv-flash.0
mtdparts: mtdparts=w25q64cv-flash.0:128k(MLO),512k(u-boot),128k(dtb),3200k(kernel),-(rootfs)
From U-boot when I do UBI part rootfs (mtdblock 4) after sf erase command
U-Boot# ubi part rootfs
UBI: attaching mtd1 to ubi0
UBI: physical eraseblock size: 65536 bytes (64 KiB)
UBI: logical eraseblock size: 65408 bytes
UBI: smallest flash I/O unit: 1
UBI: VID header offset: 64 (aligned 64)
UBI: data offset: 128
UBI: attached mtd1 to ubi0
UBI: MTD device name: "mtd=4"
UBI: MTD device size: 4 MiB
UBI: number of good PEBs: 66
UBI: number of bad PEBs: 0
UBI: max. allowed volumes: 128
UBI: wear-leveling threshold: 4096
UBI: number of internal volumes: 1
UBI: number of user volumes: 1
UBI: available PEBs: 0
UBI: total number of reserved PEBs: 66
UBI: number of PEBs reserved for bad PEB handling: 0
UBI: max/mean erase counter: 4/1
U-Boot#
U-Boot# ubi create rootfs
No size specified -> Using max size (4055296)
Creating dynamic volume rootfs of size 4055296
U-Boot# fatload mmc 0 ${loadaddr} ubi.img
reading ubi.img
3080192 bytes read in 291 ms (10.1 MiB/s)
U-Boot# ubi write ${loadaddr} rootfs 0x2f0000
3080192 bytes written to volume rootfs
******************************************************************
******************************************************************
MY UBIFS commands using the above information is
mkfs.ubifs -r image/ -m 1 -e 65408 -c 62 ubifs.img
ubinize -o ubi.img -m 1 -p 64KiB -O 64 ubinize.cfg
///ubinize.cfg///
[ubifs]
mode=ubi
image=ubifs.img
vol_id=0
vol_size=4MiB
vol_type=dynamic
vol_name=rootfs
vol_flags=autoresize
vol_alignment=1
******************************************************************
After the ubi write and setting the spi args I give spiboot for starting from SPI flash.However kernel hangs with below prints.
Attaching the portion of log I have obtained
Kernel Log....
[ 1.516377] m25p80 spi1.0: w25q64cv (8192 Kbytes)
[ 1.521292]
[ 1.521292] Debug:mtdpart_setup_real start()
[ 1.527344]
[ 1.527344] Debug:mtdpart_partition()
[ 1.532726]
[ 1.532726] Debug:mtdpart_partition()
[ 1.538085]
[ 1.538085] Debug:mtdpart_partition()
[ 1.543458]
[ 1.543458] Debug:mtdpart_partition()
[ 1.548818]
[ 1.548818] Debug:mtdpart_partition()
[ 1.554243]
[ 1.554243] mtdpart_setup_real_end()
[ 1.566010] 5 ofpart partitions found on MTD device spi1.0
[ 1.571747] Creating 5 MTD partitions on "spi1.0":
[ 1.576758] 0x000000000000-0x000000020000 : "MLO"
[ 1.583398] 0x000000020000-0x0000000a0000 : "u-boot"
[ 1.590087] 0x0000000a0000-0x0000000c0000 : "dtb"
[ 1.596546] 0x0000000c0000-0x0000003e0000 : "kernel"
[ 1.603278] 0x0000003e0000-0x000000800000 : "rootfs"
[ 1.611183] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.618062] ehci-pci: EHCI PCI platform driver
[ 1.622951] ehci-omap: OMAP-EHCI Host Controller driver
[ 1.628910] usbcore: registered new interface driver cdc_wdm
[ 1.635073] usbcore: registered new interface driver usb-storage
[ 1.642528] mousedev: PS/2 mouse device common for all mice
[ 1.648882] i2c-core: driver [rtc-ds1307] using legacy suspend method
[ 1.655646] i2c-core: driver [rtc-ds1307] using legacy resume method
[ 1.663198] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc0
[ 1.671571] i2c /dev entries driver
[ 1.676978] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.686045] omap_hsmmc 48060000.mmc: unable to get vmmc regulator -517
[ 1.693177] platform 48060000.mmc: Driver omap_hsmmc requests probe deferral
[ 1.822302] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 1.832956] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 1.839403] omap_hsmmc 47810000.mmc: card claims to support voltages below defined range
[ 1.849254] usbcore: registered new interface driver usbhid
[ 1.855111] usbhid: USB HID core driver
[ 1.859379] platform 44d00000.wkup_m3: Driver wkup_m3 requests probe deferral
[ 1.867761] oprofile: using arm/armv7
[ 1.872997] PM: bootloader does not support rtc-only!
[ 1.878307] ThumbEE CPU extension supported.
[ 1.882947] Registering SWP/SWPB emulation handler
[ 1.889786] lis3_reg: disabling
[ 1.893205] vbat: disabling
[ 1.896144] regulator-dummy: disabling
[ 1.900481] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[ 1.905889] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[ 1.914694] tps65910 0-002d: No interrupt support, no core IRQ
[ 1.922646] mmc0: queuing unknown CIS tuple 0x91 (3 bytes)
[ 1.929957] mmc0: new SDIO card at address 0001
[ 1.934733] vrtc: 1800 mV
[ 1.937853] vrtc: supplied by vbat
[ 1.945020] vio: at 1800 mV
[ 1.948135] vio: supplied by vbat
[ 1.953484] vdd_mpu: 912 <--> 1375 mV at 1137 mV
[ 1.958485] vdd_mpu: supplied by vbat
[ 1.964184] vdd_core: 912 <--> 1150 mV at 1137 mV
[ 1.969269] vdd_core: supplied by vbat
[ 1.974697] vdd3: 5000 mV
[ 1.978901] vdig1: at 1800 mV
[ 1.982203] vdig1: supplied by vbat
[ 1.987236] vdig2: at 1800 mV
[ 1.990503] vdig2: supplied by vbat
[ 1.995567] vpll: at 1800 mV
[ 1.998749] vpll: supplied by vbat
[ 2.003747] vdac: at 1800 mV
[ 2.006924] vdac: supplied by vbat
[ 2.011882] vaux1: at 1800 mV
[ 2.015148] vaux1: supplied by vbat
[ 2.020171] vaux2: at 3300 mV
[ 2.023472] vaux2: supplied by vbat
[ 2.028547] vaux33: at 3300 mV
[ 2.031925] vaux33: supplied by vbat
[ 2.037044] vmmc: 1800 <--> 3300 mV at 3300 mV
[ 2.042093] vmmc: supplied by vbat
[ 2.046986] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 2.053198] pinctrl-single 44e10800.pinmux: pin 44e10958.0 already requested by 44e10800.pinmux; cannot claim for 4802a000.i2c
[ 2.065127] pinctrl-single 44e10800.pinmux: pin-86 (4802a000.i2c) status -22
[ 2.072500] pinctrl-single 44e10800.pinmux: could not request pin 86 (44e10958.0) from group pinmux_i2c1_pins on device pinctrl-single
[ 2.085216] omap_i2c 4802a000.i2c: Error applying setting, reverse things back
[ 2.095524] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 100 kHz
[ 2.141969] remoteproc0: wkup_m3 is available
[ 2.146620] remoteproc0: Note: remoteproc is still under development and considered experimental.
[ 2.156014] remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 2.167025] remoteproc0: Direct firmware load failed with error -2
[ 2.173636] remoteproc0: Falling back to user helper
[ 2.183066] UBI: attaching mtd4 to ubi0
[ 2.187094] UBI:
[ 2.187094] Debug:io_init_end
[ 2.187094]
[ 2.193935] UBI:
[ 2.193935] Debug:vmalloc_end
[ 2.193935]
[ 2.270736] mmc1: new SDHC card at address e624
[ 2.281536] mmcblk0: mmc1:e624 SD04G 3.69 GiB
[ 2.293286] mmcblk0: p1 p2
[ 2.512350] UBI: scanning is finished
[ 2.516178] UBI: div_u64_end
[ 2.519180] UBI: late_analysis_end
[ 2.522754] UBI: ubi_rb_entry_end
[ 2.526212] UBI: list_for_each_entry_1
[ 2.530119] UBI: list_for_each_entry_2
[ 2.534157] UBI: list_for_each_entry_3
[ 2.538067] UBI: self_check_end
[ 2.541340] UBI: ubi_free_hdr_end
[ 2.544810] UBI: kfree_end
[ 2.547630] UBI: scan_all_end
[ 2.550720] UBI: dbg_gen_end
[ 2.553732] UBI: cpu_to_be32_end
[ 2.557094] UBI: ALIGN_end
[ 2.559912] UBI: ubi_find_av_end
[ 2.563284] UBI: UBI_else_!av_end
[ 2.566737] UBI: process_lvol_start
[ 2.570371] UBI: check layout volume
[ 2.574148] UBI: vzalloc_end
[ 2.577150] UBI: ui_io_read_start
[ 2.580705] Unable to handle kernel paging request at virtual address cfe12060
[ 2.588241] pgd = c0004000
[ 2.591062] [cfe12060] *pgd=00000000
[ 2.594803] Internal error: Oops: 5 [#1] ARM
[ 2.599257] Modules linked in:
[ 2.602453] CPU: 0 PID: 508 Comm: spi1 Not tainted 3.14.26-g07d13c6-dirty #22
[ 2.609901] task: cd92e400 ti: cda36000 task.ti: cda36000
[ 2.615555] PC is at dma_cache_maint_page+0x64/0x160
[ 2.620736] LR is at arm_dma_map_page+0x7c/0x8c
[ 2.625464] pc : [<c0016aec>] lr : [<c0016cc0>] psr: 60000113
[ 2.625464] sp : cda37dd8 ip : 00000000 fp : cda37e0c
[ 2.637440] r10: 00000002 r9 : c0594018 r8 : 00090903
[ 2.642890] r7 : 00000f74 r6 : 00010903 r5 : c0594b00 r4 : 00000000
[ 2.649700] r3 : cfc00000 r2 : 00080000 r1 : 00000394 r0 : 00212060
[ 2.656513] Flags: nZCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel
[ 2.664140] Control: 10c5387d Table: 80004019 DAC: 00000015
[ 2.670135] Process spi1 (pid: 508, stack limit = 0xcda36238)
[ 2.676130] Stack: (0xcda37dd8 to 0xcda38000)
[ 2.680676] 7dc0: cda37e2c cda37de8
[ 2.689214] 7de0: c006ec94 00000000 cfe12060 cd87dc20 cd87dbfc 00000000 c0594b00 cd9ff900
[ 2.697750] 7e00: cda37e2c cda37e10 c0016cc0 c0016a94 c001aa74 cd92e400 00000f74 90903000
[ 2.706286] 7e20: cda37f1c cda37e30 c031407c c0016c50 00000002 00000000 c0057830 cd86ec30
[ 2.714823] 7e40: ffffffff cfc00000 cda37e7c cda17800 c03e979c c001333c ffffffff cd87c01c
[ 2.723360] 7e60: cd92e400 c059f408 00000000 00000001 cda37e94 cda37e80 ffffffff 00000000
[ 2.731897] 7e80: cd92e400 c059f408 cda37f2c cda37e98 cda17a00 c0053544 00000000 c05d63e8
[ 2.740437] 7ea0: cda37efc cda37eb0 c02be540 c02be458 cda36000 cd8cb080 00000080 fa200000
[ 2.748973] 7ec0: 0000001c c05c24a0 cda37ef4 cda37ed8 c00085e8 60000113 cd8cb010 c05d63e8
[ 2.757510] 7ee0: 00000001 00000000 00000000 c05d63e8 cda37f1c cda17994 cda17800 c05d63e8
[ 2.766046] 7f00: 00000001 00000000 00000000 c05d63e8 cda37f3c cda37f20 c031127c c0313ed4
[ 2.774584] 7f20: c03110f4 cda17980 cda36000 c05d63e8 cda37f64 cda37f40 c004cc10 c0311100
[ 2.783121] 7f40: 00000000 cda43c00 cda17980 c004cbb8 00000000 00000000 cda37fac cda37f68
[ 2.791659] 7f60: c004ce1c c004cbc4 00000000 00000000 00000000 cda17980 00000000 cda37f7c
[ 2.800196] 7f80: cda37f7c 00000000 cda37f88 cda37f88 cda43c00 c004cd58 00000000 00000000
[ 2.808734] 7fa0: 00000000 cda37fb0 c000e578 c004cd64 00000000 00000000 00000000 00000000
[ 2.817271] 7fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 2.825807] 7fe0: 00000000 00000000 00000000 00000000 00000013 00000000 00400002 0000828a
[ 2.834336] Backtrace:
[ 2.836900] [<c0016a88>] (dma_cache_maint_page) from [<c0016cc0>] (arm_dma_map_page+0x7c/0x8c)
[ 2.845885] r10:cd9ff900 r9:c0594b00 r8:00000000 r7:cd87dbfc r6:cd87dc20 r5:cfe12060
[ 2.854079] r4:00000000
[ 2.856739] [<c0016c44>] (arm_dma_map_page) from [<c031407c>] (omap2_mcspi_transfer_one_message+0x1b4/0x137c)
[ 2.867083] r5:90903000 r4:00000f74
[ 2.870826] [<c0313ec8>] (omap2_mcspi_transfer_one_message) from [<c031127c>] (spi_pump_messages+0x188/0x200)
[ 2.881169] r10:c05d63e8 r9:00000000 r8:00000000 r7:00000001 r6:c05d63e8 r5:cda17800
[ 2.889362] r4:cda17994
[ 2.892016] [<c03110f4>] (spi_pump_messages) from [<c004cc10>] (kthread_worker_fn+0x58/0x130)
[ 2.900909] r6:c05d63e8 r5:cda36000 r4:cda17980 r3:c03110f4
[ 2.906836] [<c004cbb8>] (kthread_worker_fn) from [<c004ce1c>] (kthread+0xc4/0xe0)
[ 2.914733] r10:00000000 r8:00000000 r7:c004cbb8 r6:cda17980 r5:cda43c00 r4:00000000
[ 2.922943] [<c004cd58>] (kthread) from [<c000e578>] (ret_from_fork+0x14/0x3c)
[ 2.930476] r7:00000000 r6:00000000 r5:c004cd58 r4:cda43c00
[ 2.936405] Code: e08882c0 e1866002 e3a01fe5 e0666008 (e7932286)
[ 2.942769] ---[ end trace 9a78d2757aea4543 ]---
Can someone help how to mount my filesystem. Do I need to make any change in kernel or is it ubinizing issue?
Best Regards
Jeffin