This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is it possible UBIFS mount with SPI Flash

Other Parts Discussed in Thread: AM3352

Hi.

NOW I'm using SPL & U-boot with SPI Flash boot

it's config current SPI Flash status

SPI flash is (SPL + U-BOOT ) then Nand  is (Kernel , UBIFS ) 

it's success boot...finish

But

i want change SPI Flash ONLY 

i' want plan SPI flash ( SPL + U-boot + kernel + UBIFS ) .

After boot finish then nand mount

i know that possible spi flash with kernel

But . 

Is it possible only spi flash boot with UBIFS , now env is config  only jffs2

if it possible , how can it change boot env and the other thing (kernel code ,,,etc)

Thank you

Kind Regards,