This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am still experiencing problems using my NAND on a DM8148 using EZSDK 5.05. Here is an example:
1) I boot the unit via an NFS filesystem, and no MTD devices are being used (ie, no jffs2, ubifs, etc... fileystems in use).
2) flash_erase /dev/mtd5 0 0 -> everything seems fine
3) nandtest reports ~1000 bit errors per EB, on every EB as seen below:
root@myunit:~# nandtest /dev/mtd5
ECC corrections: 163947
ECC failures : 0
Bad blocks : 0
BBT blocks : 0
00000000: reading...
1010 bit(s) ECC corrected at 00000000
00020000: reading...
1057 bit(s) ECC corrected at 00020000
00040000: reading...
1056 bit(s) ECC corrected at 00040000
00060000: reading...
1028 bit(s) ECC corrected at 00060000
00080000: reading...
1021 bit(s) ECC corrected at 00080000
000a0000: reading...
983 bit(s) ECC corrected at 000a0000
000c0000: reading...
1025 bit(s) ECC corrected at 000c0000
000e0000: reading...
1018 bit(s) ECC corrected at 000e0000
00100000: reading...
967 bit(s) ECC corrected at 00100000
00120000: reading...
998 bit(s) ECC corrected at 00120000
00140000: reading...
1038 bit(s) ECC corrected at 00140000
00160000: reading...
1046 bit(s) ECC corrected at 00160000
00180000: reading...
1020 bit(s) ECC corrected at 00180000
this continues...
This is using an SLC NAND which previously had no problems with the 1-bit Hamming ECC used in EZSDK 5.03 and prior.
Any ideas? This problem is really blocking our development.
Thanks for any support!
-Joel
Joel,
No guarantees on the below, I am not an expert here.
Here is an answer from the developers again:
"
Q:
In that formula:
http://processors.wiki.ti.com/index.php/Raw_NAND_ECC#Is_it_possible_to_use_any_ECC_algorithm_for_any_NAND.3F
How many bytes should be "B" for Hamming [1 bit]?
Is this use case OK: ECC Hamming [1 bit] + JFFS2, if the NAND supports the 1 bit ECC and it has enough OOB area?
That use case is not officially verified, I guess?
A:
B = 3 for Hamming 1-bit ECC. (as in given equation)
Its not recommended to use 1-bit ECC, multi bit-flips are commonly seen in some scenarios.
- Its highly recommended to upgrade to UBIFS+BCH8, as ECC correction capability is also good with BCH8, and UBIFS has implicit power-failure tolerances.
- UBIFS+BCH8 works seamlessly in most production environments.
"
***************
Thank you.
BR
Vladimir
Hi Vladimir,
Sorry, I was not clear. I am seeing these failures using the EZSDK 5.05.02 default ECC: BCH8. UBIFS/JFFS2 do not come in to play here, as this is a test on the MTD device, and no filesystem is in use.
From what I see so far, it appears that BCH8 ECC for NAND is 'broken' for me in EZSDK 5.05.02. I don't know the root cause or the details, but what I do know is that EZSDK 5.05.02 uses PSP 4.04.00.01, but since the EZSDK was released there has been a PSP 4.04.00.02 release. I back-ported all the NAND-related changes from PSP 4.04.00.02 to EZSDK 5.05.02, and it seems to solve all my ECC/NAND issues - at least it is much better.
I'd still appreciate any comments from anyone out there using EZSDK 5.05.02 with a 2K page NAND with BCH8 ECC. Does it work for you?
Thanks,
Joel
Joel,
Well, I know that there are some issues in PSP04.04.00.01 from that forum thread:
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/211477.aspx
I understand that the NAND tests do not involve particular fs, the commits discussed there seem to me not UBIFS specific.
AFAIK, EZSDK5.05.02.00 is validated only with PSP04.04.00.01 and not with PSP04.04.00.02, but just like you, I would have tried to apply (only) NAND related patches from the arago PSP git repository. I have not seen the NAND test issue before, don't know whether it is related to the other forum thread, but I am glad that applying the patches works for you. Generally, I think you could always read through the arago PSP recent NAND commits, checking what's new, especially when trying to resolve something. But test even more carefully your system, after applying changes. This would be outside EZSDK release.
Thank you.
BR
Vladimir
Joel,
Are you still looking for a solution? Can you share more logs of the issue that you are facing?
All my problems appear to be fixed in yet-to-be-released patches from beyond PSP 4.04.00.02. If anyone else is experiencing NAND problems, please check out my other thread at:
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/p/269235/945846.aspx#945846
Thanks,
Joel