Other Parts Discussed in Thread: OMAP3503
Hai,
In case of NAND booting in OMAP3503 processor, the NAND flash will contain 4 copies of X-Loader in the first 4 blocks of NAND flash. When ROM-code starts execution and reads the first block to load the X-Loader, if non-correctable bit error (more than 1 bit error) occurs then that read will fail and ROM-Code starts reading the 2nd block of X-loader to proceed with booting the system.
Is it possible to retrieve this information from any of the OMAP status register, that is the ROM-code used 2nd block of X-loader instead of 1st block (as there is read error)?
We could not find this information in the OMAP datasheet.
With Regards,
Arun.