Hi.
I write a frame copy api in m3vpss.The IPNC RDK is 3.8.
DM385 ARM: 1000MHz.
DDR: 533MHz.
L3/EDMA: 240MHz.
The source frame size is 12MByte.
The source address and dest address are in DDR3.
I used edma3 to copy the 12MBytes frame from source adrress to dest address.
I found that the edma3 copy need 28 ms.
What is the performance for edma3 copy from DDR to DDR?
Also what can I do to increse the bandwidth?
Thanks.