This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

8148 connected to TLV320AIC3104 with MCLK 12.288MHz playback audio double speed

Other Parts Discussed in Thread: DAC7512, PMP, ADS7846, TSC2007, TSC2004, LM63, LM70, LM73, LM77, LM80, LM83, LM87, LM90, LM92, LM93, LM95241, ADS7828, ADS7871, AMC6821, TMP102, TMP401, TMP421, TPS65010, TPS65910, BQ24022, LP3971, LP3972, TPS65023, TVP5150, TVP7002, THS7303, TLC59108, PCM3008, TLV320AIC26, TPA6130A2, DA8XX

I have a board that is using a 8148 connected with the McASP2 to a AIC3014.  We changed the MCLK from 24.576MHz to 12.288MHz,  I also changed the in the davinci-evm.c evm_hw_param() so the sysclk returned is now 1288000. (instead of 24576000).  This seemed correct.  However now that I play audio it sounds double speed, if I set the rate in alsa from 8000 to 4000 (8000 is the sample rate of my audio file), it sounds correct.  If I change the sysclk  back to 24576000 and play audio it sounds correct.  

I'm pretty much using the McASP2 setup stock from the EVM setup for the codec.

Seems the correct setting for sysclk should be 12288000 if I use a 12.288MHz clock to MCLK.  Can anyone help. 

Thanks,

Craig

  • Here is more data.  I discovered the file I'm using with aplay is a mono 16-bit LE, 8000Hz.  If I play the same file converted to stereo, all sounds correct.  I assume I'm missing a alsa plugin to convert my audio files to be stereo for the AIC3104.  (Sorry typo above not a 3014).

    Thanks,

    Craig

  • Craig,

    From what I understand you are using DM814x custom board (not DM814x EVM), right?

    Are you using EZSDK 5.05.02.00?

    Could you provide me the steps to reproduce this issue on my side?

    Meanwhile you can have a look into the below wiki pages:

    http://processors.wiki.ti.com/index.php/ALSA

    http://processors.wiki.ti.com/index.php/TI81XX_PSP_AUDIO_Driver_User_Guide

    http://processors.wiki.ti.com/index.php/TI81xx_PSP_Porting_Guide#Audio_driver_.28McASP.29

    Regards,
    Pavel

  • Yes we are on the 5.05.02.00 EZSDK and it is a custom board.  I found a post on the internet that is similar, as a stereo file plays back correctly.

    http://mailman.alsa-project.org/pipermail/alsa-devel/2009-July/019304.html

    Using aplay from the alsa-utils

    alsa-utils-aplay_1.0.23-r4.1_armv7a.ipk

    Play a file of the following formats.

    Fails, plays to fast:

    file motion_detector.wav
    motion_detector.wav: RIFF (little-endian) data, WAVE audio, Microsoft PCM, 16 bit, mono 8000 Hz

    Plays at correct speed:

    file motion_detector_stereo.wav
    motion_detector_stereo.wav: RIFF (little-endian) data, WAVE audio, Microsoft PCM, 16 bit, stereo 8000 Hz

    Patch to change sysclk from 24.576 to 12.288 (Only required if your mclk has changed)

    diff -r e0562356ad4d -r f2708e72208e linux-2.6.37/sound/soc/davinci/davinci-evm.c

    --- a/linux-2.6.37/sound/soc/davinci/davinci-evm.c Thu Apr 24 13:33:56 2014 -0600
    +++ b/linux-2.6.37/sound/soc/davinci/davinci-evm.c Mon Apr 28 18:08:38 2014 -0600
    @@ -57,15 +57,15 @@
    * board-dm644x-evm.c using GPIOs from U18. There are six
    * options; here we "know" we use a 48 KHz sample rate.
    */
    - else if (machine_is_davinci_evm())
    + else if (machine_is_davinci_evm()||
    + machine_is_touchlink())
    sysclk = 12288000;

    else if (machine_is_davinci_da830_evm() ||
    machine_is_davinci_da850_evm() ||
    machine_is_ti8168evm() ||
    machine_is_ti8148evm() ||
    - machine_is_dm385evm() ||
    - machine_is_touchlink())
    + machine_is_dm385evm() )
    sysclk = 24576000;

    /*TI811x use McASP2_AUX 20MHz*/

    Kernel config:

    #
    # Automatically generated make config: don't edit
    # Linux/arm 2.6.37 Kernel Configuration
    # Fri Apr 25 14:56:28 2014
    #
    CONFIG_ARM=y
    CONFIG_SYS_SUPPORTS_APM_EMULATION=y
    CONFIG_GENERIC_GPIO=y
    # CONFIG_ARCH_USES_GETTIMEOFFSET is not set
    CONFIG_GENERIC_CLOCKEVENTS=y
    CONFIG_HAVE_PROC_CPU=y
    CONFIG_GENERIC_HARDIRQS=y
    CONFIG_STACKTRACE_SUPPORT=y
    CONFIG_HAVE_LATENCYTOP_SUPPORT=y
    CONFIG_LOCKDEP_SUPPORT=y
    CONFIG_TRACE_IRQFLAGS_SUPPORT=y
    CONFIG_HARDIRQS_SW_RESEND=y
    CONFIG_GENERIC_IRQ_PROBE=y
    CONFIG_RWSEM_GENERIC_SPINLOCK=y
    CONFIG_ARCH_HAS_CPUFREQ=y
    CONFIG_ARCH_HAS_CPU_IDLE_WAIT=y
    CONFIG_GENERIC_HWEIGHT=y
    CONFIG_GENERIC_CALIBRATE_DELAY=y
    CONFIG_NEED_DMA_MAP_STATE=y
    CONFIG_GENERIC_HARDIRQS_NO__DO_IRQ=y
    CONFIG_ARM_L1_CACHE_SHIFT_6=y
    CONFIG_VECTORS_BASE=0xffff0000
    CONFIG_ARM_PATCH_PHYS_VIRT=y
    CONFIG_DEFCONFIG_LIST="/lib/modules/$UNAME_RELEASE/.config"
    CONFIG_CONSTRUCTORS=y
    CONFIG_HAVE_IRQ_WORK=y

    #
    # General setup
    #
    CONFIG_EXPERIMENTAL=y
    CONFIG_BROKEN_ON_SMP=y
    CONFIG_INIT_ENV_ARG_LIMIT=32
    CONFIG_CROSS_COMPILE=""
    CONFIG_LOCALVERSION="-touchlink-07"
    # CONFIG_LOCALVERSION_AUTO is not set
    CONFIG_HAVE_KERNEL_GZIP=y
    CONFIG_HAVE_KERNEL_LZMA=y
    CONFIG_HAVE_KERNEL_LZO=y
    CONFIG_KERNEL_GZIP=y
    # CONFIG_KERNEL_LZMA is not set
    # CONFIG_KERNEL_LZO is not set
    # CONFIG_SWAP is not set
    CONFIG_SYSVIPC=y
    CONFIG_SYSVIPC_SYSCTL=y
    CONFIG_POSIX_MQUEUE=y
    CONFIG_POSIX_MQUEUE_SYSCTL=y
    CONFIG_BSD_PROCESS_ACCT=y
    # CONFIG_BSD_PROCESS_ACCT_V3 is not set
    # CONFIG_TASKSTATS is not set
    # CONFIG_AUDIT is not set
    # CONFIG_HAVE_GENERIC_HARDIRQS is not set
    # CONFIG_SPARSE_IRQ is not set

    #
    # RCU Subsystem
    #
    CONFIG_TINY_RCU=y
    # CONFIG_PREEMPT_RCU is not set
    # CONFIG_TREE_RCU_TRACE is not set
    CONFIG_IKCONFIG=y
    CONFIG_IKCONFIG_PROC=y
    CONFIG_LOG_BUF_SHIFT=17
    # CONFIG_CGROUPS is not set
    CONFIG_NAMESPACES=y
    # CONFIG_UTS_NS is not set
    # CONFIG_IPC_NS is not set
    # CONFIG_USER_NS is not set
    # CONFIG_PID_NS is not set
    # CONFIG_NET_NS is not set
    # CONFIG_SYSFS_DEPRECATED is not set
    # CONFIG_RELAY is not set
    CONFIG_BLK_DEV_INITRD=y
    CONFIG_INITRAMFS_SOURCE="$(TOUCHLINK_INITRAMFS_PATH)"
    CONFIG_INITRAMFS_ROOT_UID=0
    CONFIG_INITRAMFS_ROOT_GID=0
    CONFIG_RD_GZIP=y
    CONFIG_RD_BZIP2=y
    CONFIG_RD_LZMA=y
    CONFIG_RD_LZO=y
    CONFIG_INITRAMFS_COMPRESSION_NONE=y
    # CONFIG_INITRAMFS_COMPRESSION_GZIP is not set
    # CONFIG_INITRAMFS_COMPRESSION_BZIP2 is not set
    # CONFIG_INITRAMFS_COMPRESSION_LZMA is not set
    # CONFIG_INITRAMFS_COMPRESSION_LZO is not set
    CONFIG_CC_OPTIMIZE_FOR_SIZE=y
    CONFIG_SYSCTL=y
    CONFIG_ANON_INODES=y
    # CONFIG_EMBEDDED is not set
    CONFIG_UID16=y
    CONFIG_SYSCTL_SYSCALL=y
    CONFIG_KALLSYMS=y
    # CONFIG_KALLSYMS_ALL is not set
    CONFIG_KALLSYMS_EXTRA_PASS=y
    CONFIG_HOTPLUG=y
    CONFIG_PRINTK=y
    CONFIG_BUG=y
    CONFIG_ELF_CORE=y
    CONFIG_BASE_FULL=y
    CONFIG_FUTEX=y
    CONFIG_EPOLL=y
    CONFIG_SIGNALFD=y
    CONFIG_TIMERFD=y
    CONFIG_EVENTFD=y
    CONFIG_SHMEM=y
    CONFIG_AIO=y
    CONFIG_HAVE_PERF_EVENTS=y
    CONFIG_PERF_USE_VMALLOC=y

    #
    # Kernel Performance Events And Counters
    #
    # CONFIG_PERF_EVENTS is not set
    # CONFIG_PERF_COUNTERS is not set
    CONFIG_VM_EVENT_COUNTERS=y
    CONFIG_SLUB_DEBUG=y
    CONFIG_COMPAT_BRK=y
    # CONFIG_SLAB is not set
    CONFIG_SLUB=y
    # CONFIG_PROFILING is not set
    CONFIG_HAVE_OPROFILE=y
    CONFIG_KPROBES=y
    CONFIG_KRETPROBES=y
    CONFIG_HAVE_KPROBES=y
    CONFIG_HAVE_KRETPROBES=y
    CONFIG_HAVE_REGS_AND_STACK_ACCESS_API=y
    CONFIG_HAVE_CLK=y

    #
    # GCOV-based kernel profiling
    #
    # CONFIG_GCOV_KERNEL is not set
    CONFIG_HAVE_GENERIC_DMA_COHERENT=y
    CONFIG_SLABINFO=y
    CONFIG_RT_MUTEXES=y
    CONFIG_BASE_SMALL=0
    CONFIG_MODULES=y
    # CONFIG_MODULE_FORCE_LOAD is not set
    CONFIG_MODULE_UNLOAD=y
    # CONFIG_MODULE_FORCE_UNLOAD is not set
    CONFIG_MODVERSIONS=y
    # CONFIG_MODULE_SRCVERSION_ALL is not set
    CONFIG_BLOCK=y
    CONFIG_LBDAF=y
    # CONFIG_BLK_DEV_BSG is not set
    # CONFIG_BLK_DEV_INTEGRITY is not set

    #
    # IO Schedulers
    #
    CONFIG_IOSCHED_NOOP=y
    CONFIG_IOSCHED_DEADLINE=y
    CONFIG_IOSCHED_CFQ=y
    # CONFIG_DEFAULT_DEADLINE is not set
    CONFIG_DEFAULT_CFQ=y
    # CONFIG_DEFAULT_NOOP is not set
    CONFIG_DEFAULT_IOSCHED="cfq"
    # CONFIG_INLINE_SPIN_TRYLOCK is not set
    # CONFIG_INLINE_SPIN_TRYLOCK_BH is not set
    # CONFIG_INLINE_SPIN_LOCK is not set
    # CONFIG_INLINE_SPIN_LOCK_BH is not set
    # CONFIG_INLINE_SPIN_LOCK_IRQ is not set
    # CONFIG_INLINE_SPIN_LOCK_IRQSAVE is not set
    CONFIG_INLINE_SPIN_UNLOCK=y
    # CONFIG_INLINE_SPIN_UNLOCK_BH is not set
    CONFIG_INLINE_SPIN_UNLOCK_IRQ=y
    # CONFIG_INLINE_SPIN_UNLOCK_IRQRESTORE is not set
    # CONFIG_INLINE_READ_TRYLOCK is not set
    # CONFIG_INLINE_READ_LOCK is not set
    # CONFIG_INLINE_READ_LOCK_BH is not set
    # CONFIG_INLINE_READ_LOCK_IRQ is not set
    # CONFIG_INLINE_READ_LOCK_IRQSAVE is not set
    CONFIG_INLINE_READ_UNLOCK=y
    # CONFIG_INLINE_READ_UNLOCK_BH is not set
    CONFIG_INLINE_READ_UNLOCK_IRQ=y
    # CONFIG_INLINE_READ_UNLOCK_IRQRESTORE is not set
    # CONFIG_INLINE_WRITE_TRYLOCK is not set
    # CONFIG_INLINE_WRITE_LOCK is not set
    # CONFIG_INLINE_WRITE_LOCK_BH is not set
    # CONFIG_INLINE_WRITE_LOCK_IRQ is not set
    # CONFIG_INLINE_WRITE_LOCK_IRQSAVE is not set
    CONFIG_INLINE_WRITE_UNLOCK=y
    # CONFIG_INLINE_WRITE_UNLOCK_BH is not set
    CONFIG_INLINE_WRITE_UNLOCK_IRQ=y
    # CONFIG_INLINE_WRITE_UNLOCK_IRQRESTORE is not set
    # CONFIG_MUTEX_SPIN_ON_OWNER is not set
    CONFIG_FREEZER=y

    #
    # System Type
    #
    CONFIG_MMU=y
    # CONFIG_ARCH_AAEC2000 is not set
    # CONFIG_ARCH_INTEGRATOR is not set
    # CONFIG_ARCH_REALVIEW is not set
    # CONFIG_ARCH_VERSATILE is not set
    # CONFIG_ARCH_VEXPRESS is not set
    # CONFIG_ARCH_AT91 is not set
    # CONFIG_ARCH_BCMRING is not set
    # CONFIG_ARCH_CLPS711X is not set
    # CONFIG_ARCH_CNS3XXX is not set
    # CONFIG_ARCH_GEMINI is not set
    # CONFIG_ARCH_EBSA110 is not set
    # CONFIG_ARCH_EP93XX is not set
    # CONFIG_ARCH_FOOTBRIDGE is not set
    # CONFIG_ARCH_MXC is not set
    # CONFIG_ARCH_STMP3XXX is not set
    # CONFIG_ARCH_NETX is not set
    # CONFIG_ARCH_H720X is not set
    # CONFIG_ARCH_IOP13XX is not set
    # CONFIG_ARCH_IOP32X is not set
    # CONFIG_ARCH_IOP33X is not set
    # CONFIG_ARCH_IXP23XX is not set
    # CONFIG_ARCH_IXP2000 is not set
    # CONFIG_ARCH_IXP4XX is not set
    # CONFIG_ARCH_DOVE is not set
    # CONFIG_ARCH_KIRKWOOD is not set
    # CONFIG_ARCH_LOKI is not set
    # CONFIG_ARCH_LPC32XX is not set
    # CONFIG_ARCH_MV78XX0 is not set
    # CONFIG_ARCH_ORION5X is not set
    # CONFIG_ARCH_MMP is not set
    # CONFIG_ARCH_KS8695 is not set
    # CONFIG_ARCH_NS9XXX is not set
    # CONFIG_ARCH_W90X900 is not set
    # CONFIG_ARCH_NUC93X is not set
    # CONFIG_ARCH_TEGRA is not set
    # CONFIG_ARCH_PNX4008 is not set
    # CONFIG_ARCH_PXA is not set
    # CONFIG_ARCH_MSM is not set
    # CONFIG_ARCH_SHMOBILE is not set
    # CONFIG_ARCH_RPC is not set
    # CONFIG_ARCH_SA1100 is not set
    # CONFIG_ARCH_S3C2410 is not set
    # CONFIG_ARCH_S3C64XX is not set
    # CONFIG_ARCH_S5P64X0 is not set
    # CONFIG_ARCH_S5P6442 is not set
    # CONFIG_ARCH_S5PC100 is not set
    # CONFIG_ARCH_S5PV210 is not set
    # CONFIG_ARCH_S5PV310 is not set
    # CONFIG_ARCH_SHARK is not set
    # CONFIG_ARCH_TCC_926 is not set
    # CONFIG_ARCH_LH7A40X is not set
    # CONFIG_ARCH_U300 is not set
    # CONFIG_ARCH_U8500 is not set
    # CONFIG_ARCH_NOMADIK is not set
    # CONFIG_ARCH_DAVINCI is not set
    CONFIG_ARCH_OMAP=y
    # CONFIG_PLAT_SPEAR is not set

    #
    # TI OMAP Common Features
    #
    # CONFIG_ARCH_OMAP1 is not set
    CONFIG_ARCH_OMAP2PLUS=y

    #
    # OMAP Feature Selections
    #
    # CONFIG_OMAP_RESET_CLOCKS is not set
    CONFIG_OMAP_MUX=y
    # CONFIG_OMAP_MUX_DEBUG is not set
    CONFIG_OMAP_MUX_WARNINGS=y
    # CONFIG_OMAP_MCBSP is not set
    CONFIG_OMAP_MBOX_FWK=y
    CONFIG_OMAP_MBOX_KFIFO_SIZE=256
    CONFIG_OMAP_IOMMU=y
    # CONFIG_OMAP_IOMMU_DEBUG is not set
    CONFIG_OMAP_MPU_TIMER=y
    # CONFIG_OMAP_32K_TIMER is not set
    CONFIG_OMAP_DM_TIMER=y
    # CONFIG_OMAP_PM_NONE is not set
    CONFIG_OMAP_PM_NOOP=y

    #
    # TI OMAP2/3/4 Specific Features
    #
    CONFIG_ARCH_OMAP2PLUS_TYPICAL=y
    # CONFIG_ARCH_OMAP2 is not set
    # CONFIG_ARCH_OMAP3 is not set
    # CONFIG_ARCH_OMAP4 is not set
    CONFIG_ARCH_TI81XX=y
    # CONFIG_ARCH_TI816X is not set
    CONFIG_ARCH_TI814X=y

    #
    # OMAP Board Type
    #

    #
    # TI81XX Board Type
    #
    CONFIG_MACH_TOUCHLINK=y
    # CONFIG_MACH_TI8148EVM is not set
    # CONFIG_MACH_DM385EVM is not set
    # CONFIG_TI814X_EMAC_RMII is not set
    CONFIG_TI814X_EMAC_RVMII=y
    # CONFIG_MACH_TI811XEVM is not set

    #
    # Processor Type
    #
    CONFIG_CPU_32v6K=y
    CONFIG_CPU_V7=y
    CONFIG_CPU_32v7=y
    CONFIG_CPU_ABRT_EV7=y
    CONFIG_CPU_PABRT_V7=y
    CONFIG_CPU_CACHE_V7=y
    CONFIG_CPU_CACHE_VIPT=y
    CONFIG_CPU_COPY_V6=y
    CONFIG_CPU_TLB_V7=y
    CONFIG_CPU_HAS_ASID=y
    CONFIG_CPU_CP15=y
    CONFIG_CPU_CP15_MMU=y

    #
    # Processor Features
    #
    CONFIG_ARM_THUMB=y
    # CONFIG_ARM_THUMBEE is not set
    # CONFIG_CPU_ICACHE_DISABLE is not set
    # CONFIG_CPU_DCACHE_DISABLE is not set
    # CONFIG_CPU_BPREDICT_DISABLE is not set
    CONFIG_ARM_L1_CACHE_SHIFT=6
    CONFIG_ARM_DMA_MEM_BUFFERABLE=y
    CONFIG_CPU_HAS_PMU=y
    # CONFIG_ARM_ERRATA_430973 is not set
    # CONFIG_ARM_ERRATA_458693 is not set
    # CONFIG_ARM_ERRATA_460075 is not set
    # CONFIG_ARM_ERRATA_743622 is not set
    CONFIG_COMMON_CLKDEV=y

    #
    # Bus support
    #
    # CONFIG_PCI is not set
    # CONFIG_PCI_SYSCALL is not set
    CONFIG_ARCH_SUPPORTS_MSI=y
    # CONFIG_PCCARD is not set

    #
    # Kernel Features
    #
    CONFIG_TICK_ONESHOT=y
    CONFIG_NO_HZ=y
    CONFIG_HIGH_RES_TIMERS=y
    CONFIG_GENERIC_CLOCKEVENTS_BUILD=y
    CONFIG_VMSPLIT_3G=y
    # CONFIG_VMSPLIT_2G is not set
    # CONFIG_VMSPLIT_1G is not set
    CONFIG_PAGE_OFFSET=0xC0000000
    CONFIG_PREEMPT_NONE=y
    # CONFIG_PREEMPT_VOLUNTARY is not set
    # CONFIG_PREEMPT is not set
    CONFIG_HZ=100
    # CONFIG_THUMB2_KERNEL is not set
    CONFIG_AEABI=y
    CONFIG_OABI_COMPAT=y
    CONFIG_ARCH_HAS_HOLES_MEMORYMODEL=y
    # CONFIG_ARCH_SPARSEMEM_DEFAULT is not set
    # CONFIG_ARCH_SELECT_MEMORY_MODEL is not set
    CONFIG_HIGHMEM=y
    # CONFIG_HIGHPTE is not set
    CONFIG_SELECT_MEMORY_MODEL=y
    CONFIG_FLATMEM_MANUAL=y
    CONFIG_FLATMEM=y
    CONFIG_FLAT_NODE_MEM_MAP=y
    CONFIG_HAVE_MEMBLOCK=y
    CONFIG_PAGEFLAGS_EXTENDED=y
    CONFIG_SPLIT_PTLOCK_CPUS=4
    # CONFIG_PHYS_ADDR_T_64BIT is not set
    CONFIG_ZONE_DMA_FLAG=0
    CONFIG_BOUNCE=y
    CONFIG_VIRT_TO_BUS=y
    # CONFIG_KSM is not set
    CONFIG_DEFAULT_MMAP_MIN_ADDR=4096
    CONFIG_NEED_PER_CPU_KM=y
    CONFIG_FORCE_MAX_ZONEORDER=11
    # CONFIG_LEDS is not set
    CONFIG_ALIGNMENT_TRAP=y
    # CONFIG_UACCESS_WITH_MEMCPY is not set
    # CONFIG_SECCOMP is not set
    # CONFIG_CC_STACKPROTECTOR is not set
    # CONFIG_DEPRECATED_PARAM_STRUCT is not set

    #
    # Boot options
    #
    CONFIG_ZBOOT_ROM_TEXT=0
    CONFIG_ZBOOT_ROM_BSS=0
    CONFIG_CMDLINE=""
    # CONFIG_XIP_KERNEL is not set
    # CONFIG_KEXEC is not set
    CONFIG_AUTO_ZRELADDR=y

    #
    # CPU Power Management
    #
    CONFIG_CPU_FREQ=y
    CONFIG_CPU_FREQ_TABLE=y
    # CONFIG_CPU_FREQ_DEBUG is not set
    CONFIG_CPU_FREQ_STAT=y
    # CONFIG_CPU_FREQ_STAT_DETAILS is not set
    # CONFIG_CPU_FREQ_DEFAULT_GOV_PERFORMANCE is not set
    CONFIG_CPU_FREQ_DEFAULT_GOV_USERSPACE=y
    # CONFIG_CPU_FREQ_DEFAULT_GOV_ONDEMAND is not set
    # CONFIG_CPU_FREQ_DEFAULT_GOV_CONSERVATIVE is not set
    CONFIG_CPU_FREQ_GOV_PERFORMANCE=y
    CONFIG_CPU_FREQ_GOV_POWERSAVE=y
    CONFIG_CPU_FREQ_GOV_USERSPACE=y
    CONFIG_CPU_FREQ_GOV_ONDEMAND=y
    CONFIG_CPU_FREQ_GOV_CONSERVATIVE=y
    # CONFIG_CPU_IDLE is not set

    #
    # Floating point emulation
    #

    #
    # At least one emulation must be selected
    #
    CONFIG_FPE_NWFPE=y
    # CONFIG_FPE_NWFPE_XP is not set
    # CONFIG_FPE_FASTFPE is not set
    CONFIG_VFP=y
    CONFIG_VFPv3=y
    CONFIG_NEON=y

    #
    # Userspace binary formats
    #
    CONFIG_BINFMT_ELF=y
    # CONFIG_CORE_DUMP_DEFAULT_ELF_HEADERS is not set
    CONFIG_HAVE_AOUT=y
    # CONFIG_BINFMT_AOUT is not set
    CONFIG_BINFMT_MISC=y

    #
    # Power management options
    #
    CONFIG_PM=y
    CONFIG_PM_DEBUG=y
    # CONFIG_PM_ADVANCED_DEBUG is not set
    CONFIG_PM_VERBOSE=y
    CONFIG_CAN_PM_TRACE=y
    CONFIG_PM_SLEEP=y
    CONFIG_SUSPEND_NVS=y
    CONFIG_SUSPEND=y
    # CONFIG_PM_TEST_SUSPEND is not set
    CONFIG_SUSPEND_FREEZER=y
    # CONFIG_APM_EMULATION is not set
    CONFIG_PM_RUNTIME=y
    CONFIG_PM_OPS=y
    CONFIG_ARCH_HAS_OPP=y
    CONFIG_PM_OPP=y
    CONFIG_ARCH_SUSPEND_POSSIBLE=y
    CONFIG_NET=y

    #
    # Networking options
    #
    CONFIG_PACKET=y
    CONFIG_UNIX=y
    CONFIG_XFRM=y
    # CONFIG_XFRM_USER is not set
    # CONFIG_XFRM_SUB_POLICY is not set
    # CONFIG_XFRM_MIGRATE is not set
    # CONFIG_XFRM_STATISTICS is not set
    # CONFIG_NET_KEY is not set
    CONFIG_INET=y
    # CONFIG_IP_MULTICAST is not set
    # CONFIG_IP_ADVANCED_ROUTER is not set
    CONFIG_IP_FIB_HASH=y
    CONFIG_IP_PNP=y
    CONFIG_IP_PNP_DHCP=y
    CONFIG_IP_PNP_BOOTP=y
    CONFIG_IP_PNP_RARP=y
    # CONFIG_NET_IPIP is not set
    # CONFIG_NET_IPGRE_DEMUX is not set
    # CONFIG_ARPD is not set
    # CONFIG_SYN_COOKIES is not set
    # CONFIG_INET_AH is not set
    # CONFIG_INET_ESP is not set
    # CONFIG_INET_IPCOMP is not set
    # CONFIG_INET_XFRM_TUNNEL is not set
    CONFIG_INET_TUNNEL=m
    CONFIG_INET_XFRM_MODE_TRANSPORT=y
    CONFIG_INET_XFRM_MODE_TUNNEL=y
    CONFIG_INET_XFRM_MODE_BEET=y
    CONFIG_INET_LRO=y
    CONFIG_INET_DIAG=y
    CONFIG_INET_TCP_DIAG=y
    # CONFIG_TCP_CONG_ADVANCED is not set
    CONFIG_TCP_CONG_CUBIC=y
    CONFIG_DEFAULT_TCP_CONG="cubic"
    # CONFIG_TCP_MD5SIG is not set
    CONFIG_IPV6=m
    # CONFIG_IPV6_PRIVACY is not set
    # CONFIG_IPV6_ROUTER_PREF is not set
    # CONFIG_IPV6_OPTIMISTIC_DAD is not set
    # CONFIG_INET6_AH is not set
    # CONFIG_INET6_ESP is not set
    # CONFIG_INET6_IPCOMP is not set
    # CONFIG_IPV6_MIP6 is not set
    # CONFIG_INET6_XFRM_TUNNEL is not set
    # CONFIG_INET6_TUNNEL is not set
    CONFIG_INET6_XFRM_MODE_TRANSPORT=m
    CONFIG_INET6_XFRM_MODE_TUNNEL=m
    CONFIG_INET6_XFRM_MODE_BEET=m
    # CONFIG_INET6_XFRM_MODE_ROUTEOPTIMIZATION is not set
    CONFIG_IPV6_SIT=m
    # CONFIG_IPV6_SIT_6RD is not set
    CONFIG_IPV6_NDISC_NODETYPE=y
    # CONFIG_IPV6_TUNNEL is not set
    # CONFIG_IPV6_MULTIPLE_TABLES is not set
    # CONFIG_IPV6_MROUTE is not set
    # CONFIG_NETLABEL is not set
    # CONFIG_NETWORK_SECMARK is not set
    # CONFIG_NETWORK_PHY_TIMESTAMPING is not set
    # CONFIG_NETFILTER is not set
    # CONFIG_IP_DCCP is not set
    # CONFIG_IP_SCTP is not set
    # CONFIG_RDS is not set
    # CONFIG_TIPC is not set
    # CONFIG_ATM is not set
    # CONFIG_L2TP is not set
    # CONFIG_BRIDGE is not set
    # CONFIG_NET_DSA is not set
    # CONFIG_VLAN_8021Q is not set
    # CONFIG_DECNET is not set
    # CONFIG_LLC2 is not set
    # CONFIG_IPX is not set
    # CONFIG_ATALK is not set
    # CONFIG_X25 is not set
    # CONFIG_LAPB is not set
    # CONFIG_ECONET is not set
    # CONFIG_WAN_ROUTER is not set
    # CONFIG_PHONET is not set
    # CONFIG_IEEE802154 is not set
    # CONFIG_NET_SCHED is not set
    # CONFIG_DCB is not set
    CONFIG_DNS_RESOLVER=y

    #
    # Network testing
    #
    # CONFIG_NET_PKTGEN is not set
    # CONFIG_NET_TCPPROBE is not set
    # CONFIG_HAMRADIO is not set
    # CONFIG_CAN is not set
    # CONFIG_IRDA is not set
    # CONFIG_BT is not set
    # CONFIG_AF_RXRPC is not set
    CONFIG_WIRELESS=y
    CONFIG_WIRELESS_EXT=y
    CONFIG_WEXT_CORE=y
    CONFIG_WEXT_PROC=y
    CONFIG_WEXT_PRIV=y
    CONFIG_CFG80211=y
    # CONFIG_NL80211_TESTMODE is not set
    # CONFIG_CFG80211_DEVELOPER_WARNINGS is not set
    # CONFIG_CFG80211_REG_DEBUG is not set
    CONFIG_CFG80211_DEFAULT_PS=y
    # CONFIG_CFG80211_DEBUGFS is not set
    # CONFIG_CFG80211_INTERNAL_REGDB is not set
    CONFIG_CFG80211_WEXT=y
    CONFIG_WIRELESS_EXT_SYSFS=y
    # CONFIG_LIB80211 is not set
    # CONFIG_MAC80211 is not set

    #
    # Some wireless drivers require a rate control algorithm
    #
    # CONFIG_WIMAX is not set
    # CONFIG_RFKILL is not set
    # CONFIG_NET_9P is not set
    # CONFIG_CAIF is not set
    # CONFIG_CEPH_LIB is not set

    #
    # Device Drivers
    #

    #
    # Generic Driver Options
    #
    CONFIG_UEVENT_HELPER_PATH=""
    CONFIG_DEVTMPFS=y
    CONFIG_DEVTMPFS_MOUNT=y
    CONFIG_STANDALONE=y
    CONFIG_PREVENT_FIRMWARE_BUILD=y
    CONFIG_FW_LOADER=y
    CONFIG_FIRMWARE_IN_KERNEL=y
    CONFIG_EXTRA_FIRMWARE=""
    # CONFIG_DEBUG_DRIVER is not set
    # CONFIG_DEBUG_DEVRES is not set
    # CONFIG_SYS_HYPERVISOR is not set
    # CONFIG_CONNECTOR is not set
    CONFIG_MTD=y
    # CONFIG_MTD_DEBUG is not set
    # CONFIG_MTD_TESTS is not set
    CONFIG_MTD_CONCAT=y
    CONFIG_MTD_PARTITIONS=y
    # CONFIG_MTD_REDBOOT_PARTS is not set
    CONFIG_MTD_CMDLINE_PARTS=y
    # CONFIG_MTD_AFS_PARTS is not set
    # CONFIG_MTD_AR7_PARTS is not set

    #
    # User Modules And Translation Layers
    #
    CONFIG_MTD_CHAR=y
    CONFIG_MTD_BLKDEVS=y
    CONFIG_MTD_BLOCK=y
    # CONFIG_FTL is not set
    # CONFIG_NFTL is not set
    # CONFIG_INFTL is not set
    # CONFIG_RFD_FTL is not set
    # CONFIG_SSFDC is not set
    # CONFIG_SM_FTL is not set
    # CONFIG_MTD_OOPS is not set

    #
    # RAM/ROM/Flash chip drivers
    #
    # CONFIG_MTD_CFI is not set
    # CONFIG_MTD_JEDECPROBE is not set
    CONFIG_MTD_MAP_BANK_WIDTH_1=y
    CONFIG_MTD_MAP_BANK_WIDTH_2=y
    CONFIG_MTD_MAP_BANK_WIDTH_4=y
    # CONFIG_MTD_MAP_BANK_WIDTH_8 is not set
    # CONFIG_MTD_MAP_BANK_WIDTH_16 is not set
    # CONFIG_MTD_MAP_BANK_WIDTH_32 is not set
    CONFIG_MTD_CFI_I1=y
    CONFIG_MTD_CFI_I2=y
    # CONFIG_MTD_CFI_I4 is not set
    # CONFIG_MTD_CFI_I8 is not set
    # CONFIG_MTD_RAM is not set
    # CONFIG_MTD_ROM is not set
    # CONFIG_MTD_ABSENT is not set

    #
    # Mapping drivers for chip access
    #
    # CONFIG_MTD_COMPLEX_MAPPINGS is not set
    # CONFIG_MTD_PLATRAM is not set

    #
    # Self-contained MTD device drivers
    #
    # CONFIG_MTD_DATAFLASH is not set
    CONFIG_MTD_M25P80=y
    CONFIG_M25PXX_USE_FAST_READ=y
    # CONFIG_MTD_SST25L is not set
    # CONFIG_MTD_SLRAM is not set
    # CONFIG_MTD_PHRAM is not set
    # CONFIG_MTD_MTDRAM is not set
    # CONFIG_MTD_BLOCK2MTD is not set

    #
    # Disk-On-Chip Device Drivers
    #
    # CONFIG_MTD_DOC2000 is not set
    # CONFIG_MTD_DOC2001 is not set
    # CONFIG_MTD_DOC2001PLUS is not set
    CONFIG_MTD_NAND_ECC=y
    # CONFIG_MTD_NAND_ECC_SMC is not set
    CONFIG_MTD_NAND=y
    # CONFIG_MTD_NAND_VERIFY_WRITE is not set
    # CONFIG_MTD_SM_COMMON is not set
    # CONFIG_MTD_NAND_MUSEUM_IDS is not set
    # CONFIG_MTD_NAND_GPIO is not set
    CONFIG_MTD_NAND_OMAP2=y
    CONFIG_MTD_NAND_IDS=y
    # CONFIG_MTD_NAND_DISKONCHIP is not set
    # CONFIG_MTD_NAND_NANDSIM is not set
    # CONFIG_MTD_NAND_PLATFORM is not set
    # CONFIG_MTD_ALAUDA is not set
    # CONFIG_MTD_ONENAND is not set

    #
    # LPDDR flash memory drivers
    #
    # CONFIG_MTD_LPDDR is not set
    CONFIG_MTD_UBI=y
    CONFIG_MTD_UBI_WL_THRESHOLD=4096
    CONFIG_MTD_UBI_BEB_RESERVE=1
    # CONFIG_MTD_UBI_GLUEBI is not set
    # CONFIG_MTD_UBI_DEBUG is not set
    # CONFIG_PARPORT is not set
    CONFIG_BLK_DEV=y
    # CONFIG_BLK_DEV_COW_COMMON is not set
    CONFIG_BLK_DEV_LOOP=y
    # CONFIG_BLK_DEV_CRYPTOLOOP is not set

    #
    # DRBD disabled because PROC_FS, INET or CONNECTOR not selected
    #
    # CONFIG_BLK_DEV_NBD is not set
    # CONFIG_BLK_DEV_UB is not set
    CONFIG_BLK_DEV_RAM=y
    CONFIG_BLK_DEV_RAM_COUNT=16
    CONFIG_BLK_DEV_RAM_SIZE=32768
    # CONFIG_BLK_DEV_XIP is not set
    # CONFIG_CDROM_PKTCDVD is not set
    # CONFIG_ATA_OVER_ETH is not set
    # CONFIG_MG_DISK is not set
    # CONFIG_BLK_DEV_RBD is not set
    CONFIG_MISC_DEVICES=y
    # CONFIG_AD525X_DPOT is not set
    # CONFIG_ICS932S401 is not set
    # CONFIG_ENCLOSURE_SERVICES is not set
    # CONFIG_APDS9802ALS is not set
    # CONFIG_ISL29003 is not set
    # CONFIG_ISL29020 is not set
    # CONFIG_SENSORS_TSL2550 is not set
    # CONFIG_SENSORS_BH1780 is not set
    # CONFIG_SENSORS_BH1770 is not set
    # CONFIG_SENSORS_APDS990X is not set
    # CONFIG_HMC6352 is not set
    # CONFIG_DS1682 is not set
    # CONFIG_TI_DAC7512 is not set
    # CONFIG_BMP085 is not set

    #
    # 2GIG Board Information Support
    #
    CONFIG_BOARD_INFO_2GIG=y
    CONFIG_C2PORT=m

    #
    # EEPROM support
    #
    CONFIG_EEPROM_AT24=y
    # CONFIG_EEPROM_AT25 is not set
    # CONFIG_EEPROM_LEGACY is not set
    # CONFIG_EEPROM_MAX6875 is not set
    # CONFIG_EEPROM_93CX6 is not set
    # CONFIG_IWMC3200TOP is not set

    #
    # Texas Instruments shared transport line discipline
    #
    CONFIG_HAVE_IDE=y
    # CONFIG_IDE is not set

    #
    # SCSI device support
    #
    CONFIG_SCSI_MOD=y
    # CONFIG_RAID_ATTRS is not set
    CONFIG_SCSI=y
    CONFIG_SCSI_DMA=y
    # CONFIG_SCSI_TGT is not set
    # CONFIG_SCSI_NETLINK is not set
    CONFIG_SCSI_PROC_FS=y

    #
    # SCSI support type (disk, tape, CD-ROM)
    #
    CONFIG_BLK_DEV_SD=y
    # CONFIG_CHR_DEV_ST is not set
    # CONFIG_CHR_DEV_OSST is not set
    CONFIG_BLK_DEV_SR=y
    CONFIG_BLK_DEV_SR_VENDOR=y
    CONFIG_CHR_DEV_SG=y
    # CONFIG_CHR_DEV_SCH is not set
    # CONFIG_SCSI_MULTI_LUN is not set
    # CONFIG_SCSI_CONSTANTS is not set
    # CONFIG_SCSI_LOGGING is not set
    # CONFIG_SCSI_SCAN_ASYNC is not set
    CONFIG_SCSI_WAIT_SCAN=m

    #
    # SCSI Transports
    #
    # CONFIG_SCSI_SPI_ATTRS is not set
    # CONFIG_SCSI_FC_ATTRS is not set
    # CONFIG_SCSI_ISCSI_ATTRS is not set
    # CONFIG_SCSI_SAS_ATTRS is not set
    # CONFIG_SCSI_SAS_LIBSAS is not set
    # CONFIG_SCSI_SRP_ATTRS is not set
    # CONFIG_SCSI_LOWLEVEL is not set
    # CONFIG_SCSI_DH is not set
    # CONFIG_SCSI_OSD_INITIATOR is not set
    CONFIG_ATA=y
    # CONFIG_ATA_NONSTANDARD is not set
    CONFIG_ATA_VERBOSE_ERROR=y
    CONFIG_SATA_PMP=y

    #
    # Controllers with non-SFF native interface
    #
    CONFIG_SATA_AHCI_PLATFORM=y
    # CONFIG_ATA_SFF is not set
    # CONFIG_MD is not set
    CONFIG_NETDEVICES=y
    # CONFIG_DUMMY is not set
    # CONFIG_BONDING is not set
    # CONFIG_MACVLAN is not set
    # CONFIG_EQUALIZER is not set
    CONFIG_TUN=m
    # CONFIG_VETH is not set
    CONFIG_MII=y
    CONFIG_PHYLIB=y

    #
    # MII PHY device drivers
    #
    # CONFIG_MARVELL_PHY is not set
    # CONFIG_DAVICOM_PHY is not set
    # CONFIG_QSEMI_PHY is not set
    # CONFIG_LXT_PHY is not set
    # CONFIG_CICADA_PHY is not set
    # CONFIG_VITESSE_PHY is not set
    # CONFIG_SMSC_PHY is not set
    # CONFIG_BROADCOM_PHY is not set
    # CONFIG_BCM63XX_PHY is not set
    # CONFIG_ICPLUS_PHY is not set
    # CONFIG_REALTEK_PHY is not set
    # CONFIG_NATIONAL_PHY is not set
    # CONFIG_STE10XP is not set
    # CONFIG_LSI_ET1011C_PHY is not set
    # CONFIG_MICREL_PHY is not set
    # CONFIG_FIXED_PHY is not set
    # CONFIG_MDIO_BITBANG is not set
    # CONFIG_NET_ETHERNET is not set
    CONFIG_NETDEV_1000=y
    CONFIG_TI_DAVINCI_MDIO=y
    CONFIG_TI_DAVINCI_CPDMA=y
    CONFIG_TI_CPSW=y
    # CONFIG_TI_CPSW_DUAL_EMAC is not set
    # CONFIG_STMMAC_ETH is not set
    # CONFIG_NETDEV_10000 is not set
    # CONFIG_WLAN is not set

    #
    # Enable WiMAX (Networking options) to see the WiMAX drivers
    #

    #
    # USB Network Adapters
    #
    # CONFIG_USB_CATC is not set
    # CONFIG_USB_KAWETH is not set
    # CONFIG_USB_PEGASUS is not set
    # CONFIG_USB_RTL8150 is not set
    CONFIG_USB_USBNET=y
    # CONFIG_USB_NET_AX8817X is not set
    CONFIG_USB_NET_CDCETHER=y
    # CONFIG_USB_NET_CDC_EEM is not set
    CONFIG_USB_NET_DM9601=y
    # CONFIG_USB_NET_SMSC75XX is not set
    # CONFIG_USB_NET_SMSC95XX is not set
    # CONFIG_USB_NET_GL620A is not set
    # CONFIG_USB_NET_NET1080 is not set
    # CONFIG_USB_NET_PLUSB is not set
    # CONFIG_USB_NET_MCS7830 is not set
    # CONFIG_USB_NET_RNDIS_HOST is not set
    # CONFIG_USB_NET_CDC_SUBSET is not set
    # CONFIG_USB_NET_ZAURUS is not set
    # CONFIG_USB_NET_CX82310_ETH is not set
    # CONFIG_USB_NET_INT51X1 is not set
    # CONFIG_USB_IPHETH is not set
    # CONFIG_USB_SIERRA_NET is not set
    # CONFIG_WAN is not set

    #
    # CAIF transport drivers
    #
    CONFIG_PPP=y
    # CONFIG_PPP_MULTILINK is not set
    # CONFIG_PPP_FILTER is not set
    CONFIG_PPP_ASYNC=y
    CONFIG_PPP_SYNC_TTY=y
    CONFIG_PPP_DEFLATE=y
    # CONFIG_PPP_BSDCOMP is not set
    # CONFIG_PPP_MPPE is not set
    # CONFIG_PPPOE is not set
    # CONFIG_SLIP is not set
    CONFIG_SLHC=y
    # CONFIG_NETCONSOLE is not set
    # CONFIG_NETPOLL is not set
    # CONFIG_NET_POLL_CONTROLLER is not set
    # CONFIG_ISDN is not set
    # CONFIG_PHONE is not set

    #
    # Input device support
    #
    CONFIG_INPUT=y
    # CONFIG_INPUT_FF_MEMLESS is not set
    # CONFIG_INPUT_POLLDEV is not set
    # CONFIG_INPUT_SPARSEKMAP is not set

    #
    # Userland interfaces
    #
    CONFIG_INPUT_MOUSEDEV=y
    # CONFIG_INPUT_MOUSEDEV_PSAUX is not set
    CONFIG_INPUT_MOUSEDEV_SCREEN_X=1024
    CONFIG_INPUT_MOUSEDEV_SCREEN_Y=768
    # CONFIG_INPUT_JOYDEV is not set
    CONFIG_INPUT_EVDEV=y
    # CONFIG_INPUT_EVBUG is not set

    #
    # Input Device Drivers
    #
    # CONFIG_INPUT_KEYBOARD is not set
    # CONFIG_INPUT_MOUSE is not set
    # CONFIG_INPUT_JOYSTICK is not set
    # CONFIG_INPUT_TABLET is not set
    CONFIG_INPUT_TOUCHSCREEN=y
    # CONFIG_TOUCHSCREEN_ADS7846 is not set
    # CONFIG_TOUCHSCREEN_AD7877 is not set
    # CONFIG_TOUCHSCREEN_AD7879 is not set
    # CONFIG_TOUCHSCREEN_BU21013 is not set
    # CONFIG_TOUCHSCREEN_CY8CTMG110 is not set
    # CONFIG_TOUCHSCREEN_DYNAPRO is not set
    # CONFIG_TOUCHSCREEN_HAMPSHIRE is not set
    # CONFIG_TOUCHSCREEN_EETI is not set
    # CONFIG_TOUCHSCREEN_FUJITSU is not set
    # CONFIG_TOUCHSCREEN_GUNZE is not set
    # CONFIG_TOUCHSCREEN_ELO is not set
    # CONFIG_TOUCHSCREEN_WACOM_W8001 is not set
    # CONFIG_TOUCHSCREEN_MCS5000 is not set
    # CONFIG_TOUCHSCREEN_MTOUCH is not set
    # CONFIG_TOUCHSCREEN_INEXIO is not set
    # CONFIG_TOUCHSCREEN_MK712 is not set
    # CONFIG_TOUCHSCREEN_PENMOUNT is not set
    # CONFIG_TOUCHSCREEN_QT602240 is not set
    # CONFIG_TOUCHSCREEN_TOUCHRIGHT is not set
    # CONFIG_TOUCHSCREEN_TOUCHWIN is not set
    # CONFIG_TOUCHSCREEN_USB_COMPOSITE is not set
    # CONFIG_TOUCHSCREEN_TOUCHIT213 is not set
    CONFIG_TOUCHSCREEN_TSC2007=y
    CONFIG_TOUCHSCREEN_ATMEL_MXT_TS=m
    # CONFIG_TOUCHSCREEN_TSC2004 is not set
    # CONFIG_TOUCHSCREEN_W90X900 is not set
    # CONFIG_TOUCHSCREEN_TPS6507X is not set
    # CONFIG_INPUT_MISC is not set

    #
    # Hardware I/O ports
    #
    CONFIG_SERIO=y
    CONFIG_SERIO_SERPORT=y
    # CONFIG_SERIO_RAW is not set
    # CONFIG_SERIO_ALTERA_PS2 is not set
    # CONFIG_SERIO_PS2MULT is not set
    # CONFIG_GAMEPORT is not set

    #
    # Character devices
    #
    CONFIG_VT=y
    CONFIG_CONSOLE_TRANSLATIONS=y
    CONFIG_VT_CONSOLE=y
    CONFIG_HW_CONSOLE=y
    # CONFIG_VT_HW_CONSOLE_BINDING is not set
    CONFIG_DEVKMEM=y
    CONFIG_SERIAL_NONSTANDARD=y
    # CONFIG_N_HDLC is not set
    # CONFIG_N_GSM is not set
    # CONFIG_RISCOM8 is not set
    # CONFIG_SPECIALIX is not set
    # CONFIG_STALDRV is not set

    #
    # Serial drivers
    #
    CONFIG_SERIAL_8250=y
    CONFIG_SERIAL_8250_CONSOLE=y
    CONFIG_SERIAL_8250_NR_UARTS=64
    CONFIG_SERIAL_8250_RUNTIME_UARTS=4
    CONFIG_SERIAL_8250_EXTENDED=y
    # CONFIG_SERIAL_8250_MANY_PORTS is not set
    CONFIG_SERIAL_8250_SHARE_IRQ=y
    CONFIG_SERIAL_8250_DETECT_IRQ=y
    CONFIG_SERIAL_8250_RSA=y

    #
    # Non-8250 serial port support
    #
    # CONFIG_SERIAL_MAX3100 is not set
    # CONFIG_SERIAL_MAX3107 is not set
    CONFIG_SERIAL_CORE=y
    CONFIG_SERIAL_CORE_CONSOLE=y
    CONFIG_SERIAL_OMAP=y
    CONFIG_SERIAL_OMAP_CONSOLE=y
    # CONFIG_SERIAL_TIMBERDALE is not set
    # CONFIG_SERIAL_ALTERA_JTAGUART is not set
    # CONFIG_SERIAL_ALTERA_UART is not set
    CONFIG_UNIX98_PTYS=y
    # CONFIG_DEVPTS_MULTIPLE_INSTANCES is not set
    # CONFIG_LEGACY_PTYS is not set
    # CONFIG_IPMI_HANDLER is not set
    # CONFIG_HW_RANDOM is not set
    # CONFIG_R3964 is not set
    # CONFIG_RAW_DRIVER is not set
    # CONFIG_TCG_TPM is not set
    # CONFIG_TI81XX_PCIE_EPDRV is not set
    # CONFIG_RAMOOPS is not set
    CONFIG_I2C=y
    CONFIG_I2C_BOARDINFO=y
    CONFIG_I2C_COMPAT=y
    CONFIG_I2C_CHARDEV=y
    # CONFIG_I2C_MUX is not set
    CONFIG_I2C_HELPER_AUTO=y

    #
    # I2C Hardware Bus support
    #

    #
    # I2C system bus drivers (mostly embedded / system-on-chip)
    #
    # CONFIG_I2C_DESIGNWARE is not set
    # CONFIG_I2C_GPIO is not set
    # CONFIG_I2C_OCORES is not set
    CONFIG_I2C_OMAP=y
    # CONFIG_I2C_PCA_PLATFORM is not set
    # CONFIG_I2C_SIMTEC is not set
    # CONFIG_I2C_XILINX is not set

    #
    # External I2C/SMBus adapter drivers
    #
    # CONFIG_I2C_PARPORT_LIGHT is not set
    # CONFIG_I2C_TAOS_EVM is not set
    # CONFIG_I2C_TINY_USB is not set

    #
    # Other I2C/SMBus bus drivers
    #
    # CONFIG_I2C_STUB is not set
    # CONFIG_I2C_DEBUG_CORE is not set
    # CONFIG_I2C_DEBUG_ALGO is not set
    # CONFIG_I2C_DEBUG_BUS is not set
    CONFIG_SPI=y
    # CONFIG_SPI_DEBUG is not set
    CONFIG_SPI_MASTER=y

    #
    # SPI Master Controller Drivers
    #
    # CONFIG_SPI_BITBANG is not set
    # CONFIG_SPI_GPIO is not set
    CONFIG_SPI_OMAP24XX=y
    # CONFIG_SPI_XILINX is not set
    # CONFIG_SPI_DESIGNWARE is not set

    #
    # SPI Protocol Masters
    #
    CONFIG_SPI_SPIDEV=y
    # CONFIG_SPI_TLE62X0 is not set

    #
    # PPS support
    #
    # CONFIG_PPS is not set

    #
    # PTP clock support
    #

    #
    # Enable Device Drivers -> PPS to see the PTP clock options.
    #
    CONFIG_ARCH_REQUIRE_GPIOLIB=y
    CONFIG_GPIOLIB=y
    # CONFIG_DEBUG_GPIO is not set
    CONFIG_GPIO_SYSFS=y

    #
    # Memory mapped GPIO expanders:
    #
    # CONFIG_GPIO_BASIC_MMIO is not set
    # CONFIG_GPIO_IT8761E is not set
    # CONFIG_GPIO_VX855 is not set

    #
    # I2C GPIO expanders:
    #
    # CONFIG_GPIO_MAX7300 is not set
    # CONFIG_GPIO_MAX732X is not set
    # CONFIG_GPIO_PCA953X is not set
    # CONFIG_GPIO_PCF857X is not set
    # CONFIG_GPIO_SX150X is not set
    # CONFIG_GPIO_ADP5588 is not set

    #
    # PCI GPIO expanders:
    #

    #
    # SPI GPIO expanders:
    #
    # CONFIG_GPIO_MAX7301 is not set
    # CONFIG_GPIO_MCP23S08 is not set
    # CONFIG_GPIO_MC33880 is not set
    # CONFIG_GPIO_74X164 is not set

    #
    # AC97 GPIO expanders:
    #

    #
    # MODULbus GPIO expanders:
    #
    # CONFIG_W1 is not set
    # CONFIG_POWER_SUPPLY is not set
    CONFIG_HWMON=y
    # CONFIG_HWMON_VID is not set
    # CONFIG_HWMON_DEBUG_CHIP is not set

    #
    # Native drivers
    #
    # CONFIG_SENSORS_AD7414 is not set
    # CONFIG_SENSORS_AD7418 is not set
    # CONFIG_SENSORS_ADCXX is not set
    # CONFIG_SENSORS_ADM1021 is not set
    # CONFIG_SENSORS_ADM1025 is not set
    # CONFIG_SENSORS_ADM1026 is not set
    # CONFIG_SENSORS_ADM1029 is not set
    # CONFIG_SENSORS_ADM1031 is not set
    # CONFIG_SENSORS_ADM9240 is not set
    # CONFIG_SENSORS_ADT7411 is not set
    # CONFIG_SENSORS_ADT7462 is not set
    # CONFIG_SENSORS_ADT7470 is not set
    # CONFIG_SENSORS_ADT7475 is not set
    # CONFIG_SENSORS_ASC7621 is not set
    # CONFIG_SENSORS_ATXP1 is not set
    # CONFIG_SENSORS_DS1621 is not set
    # CONFIG_SENSORS_F71805F is not set
    # CONFIG_SENSORS_F71882FG is not set
    # CONFIG_SENSORS_F75375S is not set
    # CONFIG_SENSORS_G760A is not set
    # CONFIG_SENSORS_GL518SM is not set
    # CONFIG_SENSORS_GL520SM is not set
    # CONFIG_SENSORS_GPIO_FAN is not set
    # CONFIG_SENSORS_IT87 is not set
    # CONFIG_SENSORS_JC42 is not set
    # CONFIG_SENSORS_LM63 is not set
    # CONFIG_SENSORS_LM70 is not set
    # CONFIG_SENSORS_LM73 is not set
    CONFIG_SENSORS_LM75=m
    # CONFIG_SENSORS_LM77 is not set
    # CONFIG_SENSORS_LM78 is not set
    # CONFIG_SENSORS_LM80 is not set
    # CONFIG_SENSORS_LM83 is not set
    # CONFIG_SENSORS_LM85 is not set
    # CONFIG_SENSORS_LM87 is not set
    # CONFIG_SENSORS_LM90 is not set
    # CONFIG_SENSORS_LM92 is not set
    # CONFIG_SENSORS_LM93 is not set
    # CONFIG_SENSORS_LTC4215 is not set
    # CONFIG_SENSORS_LTC4245 is not set
    # CONFIG_SENSORS_LTC4261 is not set
    # CONFIG_SENSORS_LM95241 is not set
    # CONFIG_SENSORS_MAX1111 is not set
    # CONFIG_SENSORS_MAX1619 is not set
    # CONFIG_SENSORS_MAX6650 is not set
    # CONFIG_SENSORS_PC87360 is not set
    # CONFIG_SENSORS_PC87427 is not set
    # CONFIG_SENSORS_PCF8591 is not set
    # CONFIG_SENSORS_SHT15 is not set
    # CONFIG_SENSORS_SMM665 is not set
    # CONFIG_SENSORS_DME1737 is not set
    # CONFIG_SENSORS_EMC1403 is not set
    # CONFIG_SENSORS_EMC2103 is not set
    # CONFIG_SENSORS_SMSC47M1 is not set
    # CONFIG_SENSORS_SMSC47M192 is not set
    # CONFIG_SENSORS_SMSC47B397 is not set
    # CONFIG_SENSORS_ADS7828 is not set
    # CONFIG_SENSORS_ADS7871 is not set
    # CONFIG_SENSORS_AMC6821 is not set
    # CONFIG_SENSORS_THMC50 is not set
    # CONFIG_SENSORS_TMP102 is not set
    # CONFIG_SENSORS_TMP401 is not set
    # CONFIG_SENSORS_TMP421 is not set
    # CONFIG_SENSORS_VT1211 is not set
    # CONFIG_SENSORS_W83781D is not set
    # CONFIG_SENSORS_W83791D is not set
    # CONFIG_SENSORS_W83792D is not set
    # CONFIG_SENSORS_W83793 is not set
    # CONFIG_SENSORS_W83795 is not set
    # CONFIG_SENSORS_W83L785TS is not set
    # CONFIG_SENSORS_W83L786NG is not set
    # CONFIG_SENSORS_W83627HF is not set
    # CONFIG_SENSORS_W83627EHF is not set
    # CONFIG_SENSORS_LIS3_SPI is not set
    # CONFIG_SENSORS_LIS3_I2C is not set
    # CONFIG_THERMAL is not set
    CONFIG_WATCHDOG=y
    # CONFIG_WATCHDOG_NOWAYOUT is not set

    #
    # Watchdog Device Drivers
    #
    # CONFIG_SOFT_WATCHDOG is not set
    CONFIG_OMAP_WATCHDOG=y
    # CONFIG_MAX63XX_WATCHDOG is not set

    #
    # USB-based Watchdog Cards
    #
    # CONFIG_USBPCWATCHDOG is not set
    CONFIG_SSB_POSSIBLE=y

    #
    # Sonics Silicon Backplane
    #
    CONFIG_SSB=m
    CONFIG_SSB_SDIOHOST_POSSIBLE=y
    # CONFIG_SSB_SDIOHOST is not set
    # CONFIG_SSB_DEBUG is not set
    CONFIG_MFD_SUPPORT=y
    CONFIG_MFD_CORE=y
    # CONFIG_MFD_88PM860X is not set
    # CONFIG_MFD_SM501 is not set
    # CONFIG_MFD_ASIC3 is not set
    # CONFIG_HTC_EGPIO is not set
    # CONFIG_HTC_PASIC3 is not set
    # CONFIG_HTC_I2CPLD is not set
    # CONFIG_TPS65010 is not set
    # CONFIG_TPS6507X is not set
    # CONFIG_MFD_STMPE is not set
    # CONFIG_MFD_TC35892 is not set
    # CONFIG_MFD_TMIO is not set
    # CONFIG_MFD_T7L66XB is not set
    # CONFIG_MFD_TC6387XB is not set
    # CONFIG_MFD_TC6393XB is not set
    # CONFIG_PMIC_DA903X is not set
    # CONFIG_PMIC_ADP5520 is not set
    # CONFIG_MFD_MAX8925 is not set
    # CONFIG_MFD_MAX8998 is not set
    # CONFIG_MFD_WM8400 is not set
    # CONFIG_MFD_WM831X_I2C is not set
    # CONFIG_MFD_WM831X_SPI is not set
    # CONFIG_MFD_WM8350_I2C is not set
    # CONFIG_MFD_WM8994 is not set
    # CONFIG_MFD_PCF50633 is not set
    # CONFIG_MFD_MC13XXX is not set
    # CONFIG_ABX500_CORE is not set
    # CONFIG_EZX_PCAP is not set
    # CONFIG_MFD_TPS6586X is not set
    CONFIG_MFD_TPS65910=y
    CONFIG_REGULATOR=y
    CONFIG_REGULATOR_DEBUG=y
    CONFIG_REGULATOR_DUMMY=y
    # CONFIG_REGULATOR_FIXED_VOLTAGE is not set
    # CONFIG_REGULATOR_VIRTUAL_CONSUMER is not set
    # CONFIG_REGULATOR_USERSPACE_CONSUMER is not set
    # CONFIG_REGULATOR_BQ24022 is not set
    # CONFIG_REGULATOR_MAX1586 is not set
    # CONFIG_REGULATOR_MAX8649 is not set
    # CONFIG_REGULATOR_MAX8660 is not set
    # CONFIG_REGULATOR_MAX8952 is not set
    # CONFIG_REGULATOR_LP3971 is not set
    # CONFIG_REGULATOR_LP3972 is not set
    # CONFIG_REGULATOR_TPS65023 is not set
    # CONFIG_REGULATOR_TPS6507X is not set
    # CONFIG_REGULATOR_ISL6271A is not set
    # CONFIG_REGULATOR_AD5398 is not set
    CONFIG_REGULATOR_TPS65910=y
    CONFIG_MEDIA_SUPPORT=y

    #
    # Multimedia core support
    #
    # CONFIG_MEDIA_CONTROLLER is not set
    CONFIG_VIDEO_DEV=y
    CONFIG_VIDEO_V4L2_COMMON=y
    CONFIG_VIDEO_ALLOW_V4L1=y
    CONFIG_VIDEO_V4L1_COMPAT=y
    # CONFIG_DVB_CORE is not set
    CONFIG_VIDEO_MEDIA=y

    #
    # Multimedia drivers
    #
    # CONFIG_IR_CORE is not set
    # CONFIG_MEDIA_ATTACH is not set
    CONFIG_MEDIA_TUNER=y
    # CONFIG_MEDIA_TUNER_CUSTOMISE is not set
    CONFIG_MEDIA_TUNER_SIMPLE=y
    CONFIG_MEDIA_TUNER_TDA8290=y
    CONFIG_MEDIA_TUNER_TDA827X=y
    CONFIG_MEDIA_TUNER_TDA18271=y
    CONFIG_MEDIA_TUNER_TDA9887=y
    CONFIG_MEDIA_TUNER_TEA5761=y
    CONFIG_MEDIA_TUNER_TEA5767=y
    CONFIG_MEDIA_TUNER_MT20XX=y
    CONFIG_MEDIA_TUNER_XC2028=y
    CONFIG_MEDIA_TUNER_XC5000=y
    CONFIG_MEDIA_TUNER_MC44S803=y
    CONFIG_VIDEO_V4L2=y
    CONFIG_VIDEO_V4L1=y
    CONFIG_VIDEOBUF_GEN=y
    CONFIG_VIDEOBUF_DMA_SG=y
    CONFIG_VIDEOBUF_DMA_CONTIG=y
    CONFIG_VIDEO_CAPTURE_DRIVERS=y
    # CONFIG_VIDEO_ADV_DEBUG is not set
    # CONFIG_VIDEO_FIXED_MINOR_RANGES is not set
    # CONFIG_VIDEO_HELPER_CHIPS_AUTO is not set

    #
    # Encoders/decoders and other helper chips
    #

    #
    # Audio decoders
    #
    # CONFIG_VIDEO_TVAUDIO is not set
    # CONFIG_VIDEO_TDA7432 is not set
    # CONFIG_VIDEO_TDA9840 is not set
    # CONFIG_VIDEO_TDA9875 is not set
    # CONFIG_VIDEO_TEA6415C is not set
    # CONFIG_VIDEO_TEA6420 is not set
    # CONFIG_VIDEO_MSP3400 is not set
    # CONFIG_VIDEO_CS5345 is not set
    # CONFIG_VIDEO_CS53L32A is not set
    # CONFIG_VIDEO_M52790 is not set
    # CONFIG_VIDEO_TLV320AIC23B is not set
    # CONFIG_VIDEO_WM8775 is not set
    # CONFIG_VIDEO_WM8739 is not set
    # CONFIG_VIDEO_VP27SMPX is not set

    #
    # RDS decoders
    #
    # CONFIG_VIDEO_SAA6588 is not set

    #
    # Video decoders
    #
    # CONFIG_VIDEO_ADV7180 is not set
    # CONFIG_VIDEO_BT819 is not set
    # CONFIG_VIDEO_BT856 is not set
    # CONFIG_VIDEO_BT866 is not set
    # CONFIG_VIDEO_KS0127 is not set
    # CONFIG_VIDEO_OV7670 is not set
    # CONFIG_VIDEO_MT9T001 is not set
    # CONFIG_VIDEO_MT9V011 is not set
    # CONFIG_VIDEO_MT9V113 is not set
    # CONFIG_VIDEO_MT9T111 is not set
    # CONFIG_VIDEO_TCM825X is not set
    # CONFIG_VIDEO_SAA7110 is not set
    # CONFIG_VIDEO_SAA711X is not set
    # CONFIG_VIDEO_SAA717X is not set
    # CONFIG_VIDEO_SAA7191 is not set
    # CONFIG_VIDEO_TVP514X is not set
    # CONFIG_VIDEO_TVP5150 is not set
    CONFIG_VIDEO_TVP7002=m
    # CONFIG_VIDEO_VPX3220 is not set

    #
    # Video and audio decoders
    #
    # CONFIG_VIDEO_CX25840 is not set

    #
    # MPEG video encoders
    #
    # CONFIG_VIDEO_CX2341X is not set

    #
    # Video encoders
    #
    # CONFIG_VIDEO_SAA7127 is not set
    # CONFIG_VIDEO_SAA7185 is not set
    # CONFIG_VIDEO_ADV7170 is not set
    # CONFIG_VIDEO_ADV7175 is not set
    # CONFIG_VIDEO_THS7303 is not set
    # CONFIG_VIDEO_ADV7343 is not set
    # CONFIG_VIDEO_AK881X is not set

    #
    # Video improvement chips
    #
    # CONFIG_VIDEO_UPD64031A is not set
    # CONFIG_VIDEO_UPD64083 is not set
    CONFIG_VIDEO_TI81XX_VIDOUT=m
    CONFIG_VIDEO_TI81XX_VIDIN=m
    # CONFIG_VIDEO_CPIA2 is not set
    # CONFIG_VIDEO_SR030PC30 is not set
    # CONFIG_SOC_CAMERA is not set
    CONFIG_V4L_USB_DRIVERS=y
    CONFIG_USB_VIDEO_CLASS=y
    CONFIG_USB_VIDEO_CLASS_INPUT_EVDEV=y
    # CONFIG_USB_GSPCA is not set
    # CONFIG_VIDEO_PVRUSB2 is not set
    # CONFIG_VIDEO_HDPVR is not set
    # CONFIG_VIDEO_USBVISION is not set
    # CONFIG_USB_VICAM is not set
    # CONFIG_USB_IBMCAM is not set
    # CONFIG_USB_KONICAWC is not set
    # CONFIG_USB_ET61X251 is not set
    # CONFIG_USB_SE401 is not set
    # CONFIG_USB_SN9C102 is not set
    # CONFIG_USB_PWC is not set
    # CONFIG_USB_ZR364XX is not set
    # CONFIG_USB_STKWEBCAM is not set
    # CONFIG_USB_S2255 is not set
    # CONFIG_V4L_MEM2MEM_DRIVERS is not set
    # CONFIG_RADIO_ADAPTERS is not set
    # CONFIG_DAB is not set
    CONFIG_HAVE_TI_TILER=y
    # CONFIG_TI_TILER is not set

    #
    # Graphics support
    #
    # CONFIG_DRM is not set
    # CONFIG_VGASTATE is not set
    # CONFIG_VIDEO_OUTPUT_CONTROL is not set
    CONFIG_FB=y
    # CONFIG_FIRMWARE_EDID is not set
    # CONFIG_FB_DDC is not set
    # CONFIG_FB_BOOT_VESA_SUPPORT is not set
    CONFIG_FB_CFB_FILLRECT=y
    CONFIG_FB_CFB_COPYAREA=y
    CONFIG_FB_CFB_IMAGEBLIT=y
    # CONFIG_FB_CFB_REV_PIXELS_IN_BYTE is not set
    # CONFIG_FB_SYS_FILLRECT is not set
    # CONFIG_FB_SYS_COPYAREA is not set
    # CONFIG_FB_SYS_IMAGEBLIT is not set
    # CONFIG_FB_FOREIGN_ENDIAN is not set
    # CONFIG_FB_SYS_FOPS is not set
    # CONFIG_FB_SVGALIB is not set
    # CONFIG_FB_MACMODES is not set
    # CONFIG_FB_BACKLIGHT is not set
    # CONFIG_FB_MODE_HELPERS is not set
    # CONFIG_FB_TILEBLITTING is not set

    #
    # Frame buffer hardware drivers
    #
    # CONFIG_FB_S1D13XXX is not set
    # CONFIG_FB_TMIO is not set
    # CONFIG_FB_VIRTUAL is not set
    # CONFIG_FB_METRONOME is not set
    # CONFIG_FB_MB862XX is not set
    # CONFIG_FB_BROADSHEET is not set
    CONFIG_TI81XX_VPSS=m
    CONFIG_TI81XX_VPSS_VRAM_SIZE=50
    CONFIG_TI81XX_VPSS_DEBUG_SUPPORT=y
    CONFIG_FB_TI81XX=m
    CONFIG_FB_TI81XX_DEBUG_SUPPORT=y
    CONFIG_FB_TI81XX_NUM_FBS=1
    CONFIG_TI81XX_HDMI=m
    # CONFIG_TI81XX_HDMI_HDCP is not set
    # CONFIG_SII9022a is not set
    # CONFIG_TLC59108 is not set
    CONFIG_BACKLIGHT_LCD_SUPPORT=y
    CONFIG_LCD_CLASS_DEVICE=y
    # CONFIG_LCD_L4F00242T03 is not set
    # CONFIG_LCD_LMS283GF05 is not set
    # CONFIG_LCD_LTV350QV is not set
    # CONFIG_LCD_TDO24M is not set
    # CONFIG_LCD_VGG2432A4 is not set
    # CONFIG_LCD_PLATFORM is not set
    # CONFIG_LCD_S6E63M0 is not set
    CONFIG_BACKLIGHT_CLASS_DEVICE=y
    CONFIG_BACKLIGHT_GENERIC=y
    CONFIG_BACKLIGHT_TOUCHLINK=m
    # CONFIG_BACKLIGHT_ADP8860 is not set

    #
    # Display device support
    #
    # CONFIG_DISPLAY_SUPPORT is not set

    #
    # Console display driver support
    #
    CONFIG_DUMMY_CONSOLE=y
    # CONFIG_FRAMEBUFFER_CONSOLE is not set
    # CONFIG_LOGO is not set
    CONFIG_SOUND=y
    # CONFIG_SOUND_OSS_CORE is not set
    CONFIG_SND=y
    CONFIG_SND_TIMER=y
    CONFIG_SND_PCM=y
    CONFIG_SND_HWDEP=y
    CONFIG_SND_RAWMIDI=y
    CONFIG_SND_JACK=y
    # CONFIG_SND_SEQUENCER is not set
    # CONFIG_SND_MIXER_OSS is not set
    # CONFIG_SND_PCM_OSS is not set
    # CONFIG_SND_HRTIMER is not set
    # CONFIG_SND_DYNAMIC_MINORS is not set
    CONFIG_SND_SUPPORT_OLD_API=y
    CONFIG_SND_VERBOSE_PROCFS=y
    CONFIG_SND_VERBOSE_PRINTK=y
    CONFIG_SND_DEBUG=y
    # CONFIG_SND_DEBUG_VERBOSE is not set
    # CONFIG_SND_PCM_XRUN_DEBUG is not set
    # CONFIG_SND_RAWMIDI_SEQ is not set
    # CONFIG_SND_OPL3_LIB_SEQ is not set
    # CONFIG_SND_OPL4_LIB_SEQ is not set
    # CONFIG_SND_SBAWE_SEQ is not set
    # CONFIG_SND_EMU10K1_SEQ is not set
    CONFIG_SND_DRIVERS=y
    # CONFIG_SND_DUMMY is not set
    CONFIG_SND_ALOOP=m
    # CONFIG_SND_MTPAV is not set
    # CONFIG_SND_SERIAL_U16550 is not set
    # CONFIG_SND_MPU401 is not set
    # CONFIG_SND_ARM is not set
    # CONFIG_SND_SPI is not set
    CONFIG_SND_USB=y
    CONFIG_SND_USB_AUDIO=y
    # CONFIG_SND_USB_UA101 is not set
    # CONFIG_SND_USB_CAIAQ is not set
    CONFIG_SND_SOC=y
    CONFIG_SND_TI81XX_SOC=y
    CONFIG_SND_DAVINCI_SOC_MCASP=y
    CONFIG_SND_TI81XX_SOC_EVM=y
    CONFIG_SND_SOC_TI81XX_GSM030X=y
    # CONFIG_SND_SOC_TI81XX_HDMI is not set
    # CONFIG_SND_OMAP_SOC is not set
    CONFIG_SND_SOC_I2C_AND_SPI=y
    CONFIG_SND_SOC_ALL_CODECS=y
    CONFIG_SND_SOC_WM_HUBS=y
    CONFIG_SND_SOC_AD1836=y
    CONFIG_SND_SOC_AD193X=y
    CONFIG_SND_SOC_AD73311=y
    CONFIG_SND_SOC_ADS117X=y
    CONFIG_SND_SOC_AK4104=y
    CONFIG_SND_SOC_AK4535=y
    CONFIG_SND_SOC_AK4642=y
    CONFIG_SND_SOC_AK4671=y
    CONFIG_SND_SOC_CS42L51=y
    CONFIG_SND_SOC_CS4270=y
    CONFIG_SND_SOC_CX20442=y
    CONFIG_SND_SOC_GSM030X=y
    CONFIG_SND_SOC_L3=y
    CONFIG_SND_SOC_DA7210=y
    CONFIG_SND_SOC_MAX98088=y
    CONFIG_SND_SOC_PCM3008=y
    CONFIG_SND_SOC_SPDIF=y
    CONFIG_SND_SOC_SSM2602=y
    CONFIG_SND_SOC_TLV320AIC23=y
    CONFIG_SND_SOC_TLV320AIC26=y
    CONFIG_SND_SOC_TLV320AIC3X=y
    CONFIG_SND_SOC_TLV320DAC33=y
    CONFIG_SND_SOC_UDA134X=y
    CONFIG_SND_SOC_UDA1380=y
    CONFIG_SND_SOC_WM8510=y
    CONFIG_SND_SOC_WM8523=y
    CONFIG_SND_SOC_WM8580=y
    CONFIG_SND_SOC_WM8711=y
    CONFIG_SND_SOC_WM8727=y
    CONFIG_SND_SOC_WM8728=y
    CONFIG_SND_SOC_WM8731=y
    CONFIG_SND_SOC_WM8741=y
    CONFIG_SND_SOC_WM8750=y
    CONFIG_SND_SOC_WM8753=y
    CONFIG_SND_SOC_WM8776=y
    CONFIG_SND_SOC_WM8804=y
    CONFIG_SND_SOC_WM8900=y
    CONFIG_SND_SOC_WM8903=y
    CONFIG_SND_SOC_WM8904=y
    CONFIG_SND_SOC_WM8940=y
    CONFIG_SND_SOC_WM8955=y
    CONFIG_SND_SOC_WM8960=y
    CONFIG_SND_SOC_WM8961=y
    CONFIG_SND_SOC_WM8962=y
    CONFIG_SND_SOC_WM8971=y
    CONFIG_SND_SOC_WM8974=y
    CONFIG_SND_SOC_WM8978=y
    CONFIG_SND_SOC_WM8985=y
    CONFIG_SND_SOC_WM8988=y
    CONFIG_SND_SOC_WM8990=y
    CONFIG_SND_SOC_WM8993=y
    CONFIG_SND_SOC_WM9081=y
    CONFIG_SND_SOC_MAX9877=y
    CONFIG_SND_SOC_TPA6130A2=y
    CONFIG_SND_SOC_WM2000=y
    CONFIG_SND_SOC_WM9090=y
    # CONFIG_SOUND_PRIME is not set
    CONFIG_HID_SUPPORT=y
    CONFIG_HID=y
    # CONFIG_HIDRAW is not set

    #
    # USB Input Devices
    #
    CONFIG_USB_HID=y
    # CONFIG_HID_PID is not set
    # CONFIG_USB_HIDDEV is not set

    #
    # Special HID drivers
    #
    # CONFIG_HID_3M_PCT is not set
    CONFIG_HID_A4TECH=y
    # CONFIG_HID_ACRUX_FF is not set
    CONFIG_HID_APPLE=y
    CONFIG_HID_BELKIN=y
    # CONFIG_HID_CANDO is not set
    CONFIG_HID_CHERRY=y
    CONFIG_HID_CHICONY=y
    # CONFIG_HID_PRODIKEYS is not set
    CONFIG_HID_CYPRESS=y
    # CONFIG_HID_DRAGONRISE is not set
    # CONFIG_HID_EGALAX is not set
    CONFIG_HID_EZKEY=y
    CONFIG_HID_KYE=y
    # CONFIG_HID_UCLOGIC is not set
    # CONFIG_HID_WALTOP is not set
    # CONFIG_HID_GYRATION is not set
    # CONFIG_HID_TWINHAN is not set
    CONFIG_HID_KENSINGTON=y
    CONFIG_HID_LOGITECH=y
    # CONFIG_LOGITECH_FF is not set
    # CONFIG_LOGIRUMBLEPAD2_FF is not set
    # CONFIG_LOGIG940_FF is not set
    # CONFIG_LOGIWII_FF is not set
    CONFIG_HID_MICROSOFT=y
    # CONFIG_HID_MOSART is not set
    CONFIG_HID_MONTEREY=y
    # CONFIG_HID_NTRIG is not set
    # CONFIG_HID_ORTEK is not set
    # CONFIG_HID_PANTHERLORD is not set
    # CONFIG_HID_PETALYNX is not set
    # CONFIG_HID_PICOLCD is not set
    # CONFIG_HID_QUANTA is not set
    # CONFIG_HID_ROCCAT is not set
    # CONFIG_HID_ROCCAT_KONE is not set
    # CONFIG_HID_ROCCAT_PYRA is not set
    # CONFIG_HID_SAMSUNG is not set
    # CONFIG_HID_SONY is not set
    # CONFIG_HID_STANTUM is not set
    # CONFIG_HID_SUNPLUS is not set
    # CONFIG_HID_GREENASIA is not set
    # CONFIG_HID_SMARTJOYPLUS is not set
    # CONFIG_HID_TOPSEED is not set
    # CONFIG_HID_THRUSTMASTER is not set
    # CONFIG_HID_ZEROPLUS is not set
    # CONFIG_HID_ZYDACRON is not set
    CONFIG_USB_SUPPORT=y
    CONFIG_USB_ARCH_HAS_HCD=y
    CONFIG_USB_ARCH_HAS_OHCI=y
    # CONFIG_USB_ARCH_HAS_EHCI is not set
    CONFIG_USB=y
    # CONFIG_USB_DEBUG is not set
    CONFIG_USB_ANNOUNCE_NEW_DEVICES=y

    #
    # Miscellaneous USB options
    #
    CONFIG_USB_DEVICEFS=y
    CONFIG_USB_DEVICE_CLASS=y
    # CONFIG_USB_DYNAMIC_MINORS is not set
    CONFIG_USB_SUSPEND=y
    # CONFIG_USB_OTG is not set
    # CONFIG_USB_MON is not set
    # CONFIG_USB_WUSB is not set
    # CONFIG_USB_WUSB_CBAF is not set

    #
    # USB Host Controller Drivers
    #
    # CONFIG_USB_C67X00_HCD is not set
    # CONFIG_USB_OXU210HP_HCD is not set
    # CONFIG_USB_ISP116X_HCD is not set
    # CONFIG_USB_ISP1760_HCD is not set
    # CONFIG_USB_ISP1362_HCD is not set
    # CONFIG_USB_OHCI_HCD is not set
    # CONFIG_USB_SL811_HCD is not set
    # CONFIG_USB_R8A66597_HCD is not set
    # CONFIG_USB_HWA_HCD is not set
    CONFIG_USB_MUSB_HDRC=y

    #
    # Platform Glue Layer
    #
    # CONFIG_USB_MUSB_TUSB6010_GLUE is not set
    # CONFIG_USB_MUSB_OMAP2PLUS_GLUE is not set
    # CONFIG_USB_MUSB_AM35X_GLUE is not set
    CONFIG_USB_MUSB_TI81XX_GLUE=y
    # CONFIG_USB_MUSB_DAVINCI is not set
    # CONFIG_USB_MUSB_DA8XX is not set
    # CONFIG_USB_MUSB_TUSB6010 is not set
    # CONFIG_USB_MUSB_OMAP2PLUS is not set
    # CONFIG_USB_MUSB_AM35X is not set
    CONFIG_USB_MUSB_TI81XX=y
    # CONFIG_USB_MUSB_BLACKFIN is not set
    # CONFIG_USB_MUSB_UX500 is not set
    CONFIG_USB_TI81XX_USBID_CTRL_SW=y
    # CONFIG_USB_TI81XX_USBID_CTRL_HW is not set
    CONFIG_USB_MUSB_HOST=y
    CONFIG_USB_MUSB_HDRC_HCD=y
    # CONFIG_MUSB_PIO_ONLY is not set
    # CONFIG_USB_INVENTRA_DMA_HW is not set
    # CONFIG_USB_TI_CPPI_DMA_HW is not set
    CONFIG_USB_TI_CPPI41_DMA_HW=y
    # CONFIG_USB_INVENTRA_DMA is not set
    # CONFIG_USB_TI_CPPI_DMA is not set
    CONFIG_USB_TI_CPPI41_DMA=y
    # CONFIG_USB_TUSB_OMAP_DMA is not set
    CONFIG_USB_MUSB_DEBUG=y

    #
    # USB Device Class drivers
    #
    CONFIG_USB_ACM=y
    # CONFIG_USB_PRINTER is not set
    # CONFIG_USB_WDM is not set
    # CONFIG_USB_TMC is not set

    #
    # NOTE: USB_STORAGE depends on SCSI but BLK_DEV_SD may
    #

    #
    # also be needed; see USB_STORAGE Help for more info
    #
    CONFIG_USB_STORAGE=y
    # CONFIG_USB_STORAGE_DEBUG is not set
    # CONFIG_USB_STORAGE_DATAFAB is not set
    # CONFIG_USB_STORAGE_FREECOM is not set
    # CONFIG_USB_STORAGE_ISD200 is not set
    # CONFIG_USB_STORAGE_USBAT is not set
    # CONFIG_USB_STORAGE_SDDR09 is not set
    # CONFIG_USB_STORAGE_SDDR55 is not set
    # CONFIG_USB_STORAGE_JUMPSHOT is not set
    # CONFIG_USB_STORAGE_ALAUDA is not set
    # CONFIG_USB_STORAGE_ONETOUCH is not set
    # CONFIG_USB_STORAGE_KARMA is not set
    # CONFIG_USB_STORAGE_CYPRESS_ATACB is not set
    # CONFIG_USB_UAS is not set
    # CONFIG_USB_LIBUSUAL is not set

    #
    # USB Imaging devices
    #
    # CONFIG_USB_MDC800 is not set
    # CONFIG_USB_MICROTEK is not set

    #
    # USB port drivers
    #
    CONFIG_USB_SERIAL=y
    # CONFIG_USB_SERIAL_CONSOLE is not set
    # CONFIG_USB_EZUSB is not set
    CONFIG_USB_SERIAL_GENERIC=y
    # CONFIG_USB_SERIAL_AIRCABLE is not set
    # CONFIG_USB_SERIAL_ARK3116 is not set
    # CONFIG_USB_SERIAL_BELKIN is not set
    # CONFIG_USB_SERIAL_CH341 is not set
    # CONFIG_USB_SERIAL_WHITEHEAT is not set
    # CONFIG_USB_SERIAL_DIGI_ACCELEPORT is not set
    CONFIG_USB_SERIAL_CP210X=m
    # CONFIG_USB_SERIAL_CYPRESS_M8 is not set
    # CONFIG_USB_SERIAL_EMPEG is not set
    # CONFIG_USB_SERIAL_FTDI_SIO is not set
    # CONFIG_USB_SERIAL_FUNSOFT is not set
    # CONFIG_USB_SERIAL_VISOR is not set
    # CONFIG_USB_SERIAL_IPAQ is not set
    # CONFIG_USB_SERIAL_IR is not set
    # CONFIG_USB_SERIAL_EDGEPORT is not set
    # CONFIG_USB_SERIAL_EDGEPORT_TI is not set
    # CONFIG_USB_SERIAL_GARMIN is not set
    # CONFIG_USB_SERIAL_IPW is not set
    # CONFIG_USB_SERIAL_IUU is not set
    # CONFIG_USB_SERIAL_KEYSPAN_PDA is not set
    # CONFIG_USB_SERIAL_KEYSPAN is not set
    # CONFIG_USB_SERIAL_KLSI is not set
    # CONFIG_USB_SERIAL_KOBIL_SCT is not set
    # CONFIG_USB_SERIAL_MCT_U232 is not set
    # CONFIG_USB_SERIAL_MOS7720 is not set
    # CONFIG_USB_SERIAL_MOS7840 is not set
    # CONFIG_USB_SERIAL_MOTOROLA is not set
    # CONFIG_USB_SERIAL_NAVMAN is not set
    # CONFIG_USB_SERIAL_PL2303 is not set
    # CONFIG_USB_SERIAL_OTI6858 is not set
    # CONFIG_USB_SERIAL_QCAUX is not set
    # CONFIG_USB_SERIAL_QUALCOMM is not set
    # CONFIG_USB_SERIAL_SPCP8X5 is not set
    # CONFIG_USB_SERIAL_HP4X is not set
    # CONFIG_USB_SERIAL_SAFE is not set
    # CONFIG_USB_SERIAL_SAMBA is not set
    # CONFIG_USB_SERIAL_SIEMENS_MPI is not set
    # CONFIG_USB_SERIAL_SIERRAWIRELESS is not set
    # CONFIG_USB_SERIAL_SYMBOL is not set
    # CONFIG_USB_SERIAL_TI is not set
    # CONFIG_USB_SERIAL_CYBERJACK is not set
    # CONFIG_USB_SERIAL_XIRCOM is not set
    CONFIG_USB_SERIAL_WWAN=y
    CONFIG_USB_SERIAL_OPTION=y
    # CONFIG_USB_SERIAL_OMNINET is not set
    # CONFIG_USB_SERIAL_OPTICON is not set
    # CONFIG_USB_SERIAL_VIVOPAY_SERIAL is not set
    # CONFIG_USB_SERIAL_ZIO is not set
    # CONFIG_USB_SERIAL_SSU100 is not set
    # CONFIG_USB_SERIAL_DEBUG is not set

    #
    # USB Miscellaneous drivers
    #
    # CONFIG_USB_EMI62 is not set
    # CONFIG_USB_EMI26 is not set
    # CONFIG_USB_ADUTUX is not set
    # CONFIG_USB_SEVSEG is not set
    # CONFIG_USB_RIO500 is not set
    # CONFIG_USB_LEGOTOWER is not set
    # CONFIG_USB_LCD is not set
    # CONFIG_USB_LED is not set
    # CONFIG_USB_CYPRESS_CY7C63 is not set
    # CONFIG_USB_CYTHERM is not set
    # CONFIG_USB_IDMOUSE is not set
    # CONFIG_USB_FTDI_ELAN is not set
    # CONFIG_USB_APPLEDISPLAY is not set
    # CONFIG_USB_SISUSBVGA is not set
    # CONFIG_USB_LD is not set
    # CONFIG_USB_TRANCEVIBRATOR is not set
    # CONFIG_USB_IOWARRIOR is not set
    # CONFIG_USB_TEST is not set
    # CONFIG_USB_ISIGHTFW is not set
    # CONFIG_USB_YUREX is not set
    # CONFIG_USB_GADGET is not set

    #
    # OTG and related infrastructure
    #
    CONFIG_USB_OTG_UTILS=y
    # CONFIG_USB_GPIO_VBUS is not set
    # CONFIG_USB_ULPI is not set
    CONFIG_NOP_USB_XCEIV=y
    CONFIG_MMC=y
    # CONFIG_MMC_DEBUG is not set
    # CONFIG_MMC_UNSAFE_RESUME is not set

    #
    # MMC/SD/SDIO Card Drivers
    #
    CONFIG_MMC_BLOCK=y
    CONFIG_MMC_BLOCK_MINORS=8
    CONFIG_MMC_BLOCK_BOUNCE=y
    # CONFIG_SDIO_UART is not set
    # CONFIG_MMC_TEST is not set

    #
    # MMC/SD/SDIO Host Controller Drivers
    #
    # CONFIG_MMC_SDHCI is not set
    # CONFIG_MMC_OMAP is not set
    CONFIG_MMC_OMAP_HS=y
    # CONFIG_MMC_USHC is not set
    # CONFIG_MEMSTICK is not set
    # CONFIG_NEW_LEDS is not set
    # CONFIG_ACCESSIBILITY is not set
    CONFIG_RTC_LIB=y
    CONFIG_RTC_CLASS=y
    CONFIG_RTC_HCTOSYS=y
    CONFIG_RTC_HCTOSYS_DEVICE="rtc0"
    # CONFIG_RTC_DEBUG is not set

    #
    # RTC interfaces
    #
    CONFIG_RTC_INTF_SYSFS=y
    CONFIG_RTC_INTF_PROC=y
    CONFIG_RTC_INTF_DEV=y
    # CONFIG_RTC_INTF_DEV_UIE_EMUL is not set
    # CONFIG_RTC_DRV_TEST is not set

    #
    # I2C RTC drivers
    #
    # CONFIG_RTC_DRV_DS1307 is not set
    # CONFIG_RTC_DRV_DS1374 is not set
    # CONFIG_RTC_DRV_DS1672 is not set
    # CONFIG_RTC_DRV_DS3232 is not set
    # CONFIG_RTC_DRV_MAX6900 is not set
    # CONFIG_RTC_DRV_RS5C372 is not set
    # CONFIG_RTC_DRV_ISL1208 is not set
    # CONFIG_RTC_DRV_ISL12022 is not set
    # CONFIG_RTC_DRV_X1205 is not set
    # CONFIG_RTC_DRV_PCF8563 is not set
    # CONFIG_RTC_DRV_PCF8583 is not set
    # CONFIG_RTC_DRV_M41T80 is not set
    # CONFIG_RTC_DRV_BQ32K is not set
    # CONFIG_RTC_DRV_S35390A is not set
    # CONFIG_RTC_DRV_FM3130 is not set
    # CONFIG_RTC_DRV_RX8581 is not set
    # CONFIG_RTC_DRV_RX8025 is not set

    #
    # SPI RTC drivers
    #
    # CONFIG_RTC_DRV_M41T94 is not set
    # CONFIG_RTC_DRV_DS1305 is not set
    # CONFIG_RTC_DRV_DS1390 is not set
    # CONFIG_RTC_DRV_MAX6902 is not set
    # CONFIG_RTC_DRV_R9701 is not set
    # CONFIG_RTC_DRV_RS5C348 is not set
    # CONFIG_RTC_DRV_DS3234 is not set
    # CONFIG_RTC_DRV_PCF2123 is not set

    #
    # Platform RTC drivers
    #
    # CONFIG_RTC_DRV_CMOS is not set
    # CONFIG_RTC_DRV_DS1286 is not set
    # CONFIG_RTC_DRV_DS1511 is not set
    # CONFIG_RTC_DRV_DS1553 is not set
    # CONFIG_RTC_DRV_DS1742 is not set
    # CONFIG_RTC_DRV_STK17TA8 is not set
    # CONFIG_RTC_DRV_M48T86 is not set
    # CONFIG_RTC_DRV_M48T35 is not set
    # CONFIG_RTC_DRV_M48T59 is not set
    # CONFIG_RTC_DRV_MSM6242 is not set
    # CONFIG_RTC_DRV_BQ4802 is not set
    # CONFIG_RTC_DRV_RP5C01 is not set
    # CONFIG_RTC_DRV_V3020 is not set

    #
    # on-CPU RTC drivers
    #
    CONFIG_RTC_DRV_OMAP=y
    # CONFIG_DMADEVICES is not set
    # CONFIG_AUXDISPLAY is not set
    # CONFIG_UIO is not set
    # CONFIG_STAGING is not set
    CONFIG_Sys_Link=y
    CONFIG_SYSLINK_MULTIPROC=y
    CONFIG_SYSLINK_NOTIFY=y

    #
    # File systems
    #
    CONFIG_EXT2_FS=y
    CONFIG_EXT2_FS_XATTR=y
    CONFIG_EXT2_FS_POSIX_ACL=y
    CONFIG_EXT2_FS_SECURITY=y
    # CONFIG_EXT2_FS_XIP is not set
    CONFIG_EXT3_FS=y
    # CONFIG_EXT3_DEFAULTS_TO_ORDERED is not set
    CONFIG_EXT3_FS_XATTR=y
    CONFIG_EXT3_FS_POSIX_ACL=y
    CONFIG_EXT3_FS_SECURITY=y
    CONFIG_EXT4_FS=y
    CONFIG_EXT4_FS_XATTR=y
    CONFIG_EXT4_FS_POSIX_ACL=y
    CONFIG_EXT4_FS_SECURITY=y
    # CONFIG_EXT4_DEBUG is not set
    CONFIG_JBD=y
    # CONFIG_JBD_DEBUG is not set
    CONFIG_JBD2=y
    # CONFIG_JBD2_DEBUG is not set
    CONFIG_FS_MBCACHE=y
    # CONFIG_REISERFS_FS is not set
    # CONFIG_JFS_FS is not set
    CONFIG_FS_POSIX_ACL=y
    # CONFIG_XFS_FS is not set
    # CONFIG_GFS2_FS is not set
    # CONFIG_OCFS2_FS is not set
    # CONFIG_BTRFS_FS is not set
    # CONFIG_NILFS2_FS is not set
    CONFIG_FILE_LOCKING=y
    CONFIG_FSNOTIFY=y
    # CONFIG_DNOTIFY is not set
    CONFIG_INOTIFY_USER=y
    # CONFIG_FANOTIFY is not set
    # CONFIG_QUOTA is not set
    # CONFIG_QUOTACTL is not set
    # CONFIG_AUTOFS4_FS is not set
    # CONFIG_FUSE_FS is not set

    #
    # Caches
    #
    # CONFIG_FSCACHE is not set

    #
    # CD-ROM/DVD Filesystems
    #
    CONFIG_ISO9660_FS=y
    # CONFIG_JOLIET is not set
    # CONFIG_ZISOFS is not set
    # CONFIG_UDF_FS is not set

    #
    # DOS/FAT/NT Filesystems
    #
    CONFIG_FAT_FS=y
    CONFIG_MSDOS_FS=y
    CONFIG_VFAT_FS=y
    CONFIG_FAT_DEFAULT_CODEPAGE=437
    CONFIG_FAT_DEFAULT_IOCHARSET="iso8859-1"
    # CONFIG_NTFS_FS is not set

    #
    # Pseudo filesystems
    #
    CONFIG_PROC_FS=y
    CONFIG_PROC_SYSCTL=y
    CONFIG_PROC_PAGE_MONITOR=y
    CONFIG_SYSFS=y
    CONFIG_TMPFS=y
    # CONFIG_TMPFS_POSIX_ACL is not set
    # CONFIG_HUGETLB_PAGE is not set
    # CONFIG_CONFIGFS_FS is not set
    CONFIG_MISC_FILESYSTEMS=y
    # CONFIG_ADFS_FS is not set
    # CONFIG_AFFS_FS is not set
    # CONFIG_ECRYPT_FS is not set
    # CONFIG_HFS_FS is not set
    # CONFIG_HFSPLUS_FS is not set
    # CONFIG_BEFS_FS is not set
    # CONFIG_BFS_FS is not set
    # CONFIG_EFS_FS is not set
    CONFIG_JFFS2_FS=y
    CONFIG_JFFS2_FS_DEBUG=0
    CONFIG_JFFS2_FS_WRITEBUFFER=y
    CONFIG_JFFS2_FS_WBUF_VERIFY=y
    # CONFIG_JFFS2_SUMMARY is not set
    # CONFIG_JFFS2_FS_XATTR is not set
    # CONFIG_JFFS2_COMPRESSION_OPTIONS is not set
    CONFIG_JFFS2_ZLIB=y
    # CONFIG_JFFS2_LZO is not set
    CONFIG_JFFS2_RTIME=y
    # CONFIG_JFFS2_RUBIN is not set
    # CONFIG_UBIFS_FS is not set
    # CONFIG_LOGFS is not set
    # CONFIG_CRAMFS is not set
    # CONFIG_SQUASHFS is not set
    # CONFIG_VXFS_FS is not set
    CONFIG_MINIX_FS=y
    # CONFIG_OMFS_FS is not set
    # CONFIG_HPFS_FS is not set
    # CONFIG_QNX4FS_FS is not set
    # CONFIG_ROMFS_FS is not set
    # CONFIG_SYSV_FS is not set
    # CONFIG_UFS_FS is not set
    CONFIG_NETWORK_FILESYSTEMS=y
    CONFIG_NFS_FS=y
    CONFIG_NFS_V3=y
    # CONFIG_NFS_V3_ACL is not set
    CONFIG_NFS_V4=y
    # CONFIG_NFS_V4_1 is not set
    CONFIG_ROOT_NFS=y
    # CONFIG_NFS_USE_LEGACY_DNS is not set
    CONFIG_NFS_USE_KERNEL_DNS=y
    # CONFIG_NFS_USE_NEW_IDMAPPER is not set
    # CONFIG_NFSD is not set
    CONFIG_LOCKD=y
    CONFIG_LOCKD_V4=y
    CONFIG_NFS_COMMON=y
    CONFIG_SUNRPC=y
    CONFIG_SUNRPC_GSS=y
    CONFIG_RPCSEC_GSS_KRB5=y
    # CONFIG_CEPH_FS is not set
    # CONFIG_CIFS is not set
    # CONFIG_NCP_FS is not set
    # CONFIG_CODA_FS is not set
    # CONFIG_AFS_FS is not set

    #
    # Partition Types
    #
    # CONFIG_PARTITION_ADVANCED is not set
    CONFIG_MSDOS_PARTITION=y
    CONFIG_NLS=y
    CONFIG_NLS_DEFAULT="utf8"
    CONFIG_NLS_CODEPAGE_437=y
    # CONFIG_NLS_CODEPAGE_737 is not set
    # CONFIG_NLS_CODEPAGE_775 is not set
    # CONFIG_NLS_CODEPAGE_850 is not set
    # CONFIG_NLS_CODEPAGE_852 is not set
    # CONFIG_NLS_CODEPAGE_855 is not set
    # CONFIG_NLS_CODEPAGE_857 is not set
    # CONFIG_NLS_CODEPAGE_860 is not set
    # CONFIG_NLS_CODEPAGE_861 is not set
    # CONFIG_NLS_CODEPAGE_862 is not set
    # CONFIG_NLS_CODEPAGE_863 is not set
    # CONFIG_NLS_CODEPAGE_864 is not set
    # CONFIG_NLS_CODEPAGE_865 is not set
    # CONFIG_NLS_CODEPAGE_866 is not set
    # CONFIG_NLS_CODEPAGE_869 is not set
    # CONFIG_NLS_CODEPAGE_936 is not set
    # CONFIG_NLS_CODEPAGE_950 is not set
    # CONFIG_NLS_CODEPAGE_932 is not set
    # CONFIG_NLS_CODEPAGE_949 is not set
    # CONFIG_NLS_CODEPAGE_874 is not set
    # CONFIG_NLS_ISO8859_8 is not set
    # CONFIG_NLS_CODEPAGE_1250 is not set
    # CONFIG_NLS_CODEPAGE_1251 is not set
    CONFIG_NLS_ASCII=y
    CONFIG_NLS_ISO8859_1=y
    # CONFIG_NLS_ISO8859_2 is not set
    # CONFIG_NLS_ISO8859_3 is not set
    # CONFIG_NLS_ISO8859_4 is not set
    # CONFIG_NLS_ISO8859_5 is not set
    # CONFIG_NLS_ISO8859_6 is not set
    # CONFIG_NLS_ISO8859_7 is not set
    # CONFIG_NLS_ISO8859_9 is not set
    # CONFIG_NLS_ISO8859_13 is not set
    # CONFIG_NLS_ISO8859_14 is not set
    # CONFIG_NLS_ISO8859_15 is not set
    # CONFIG_NLS_KOI8_R is not set
    # CONFIG_NLS_KOI8_U is not set
    CONFIG_NLS_UTF8=y
    # CONFIG_DLM is not set

    #
    # Kernel hacking
    #
    CONFIG_PRINTK_TIME=y
    CONFIG_ENABLE_WARN_DEPRECATED=y
    CONFIG_ENABLE_MUST_CHECK=y
    CONFIG_FRAME_WARN=1024
    CONFIG_MAGIC_SYSRQ=y
    # CONFIG_STRIP_ASM_SYMS is not set
    # CONFIG_UNUSED_SYMBOLS is not set
    CONFIG_DEBUG_FS=y
    # CONFIG_HEADERS_CHECK is not set
    CONFIG_DEBUG_KERNEL=y
    CONFIG_DEBUG_SHIRQ=y
    CONFIG_LOCKUP_DETECTOR=y
    # CONFIG_HARDLOCKUP_DETECTOR is not set
    CONFIG_BOOTPARAM_SOFTLOCKUP_PANIC=y
    CONFIG_BOOTPARAM_SOFTLOCKUP_PANIC_VALUE=1
    CONFIG_DETECT_HUNG_TASK=y
    CONFIG_BOOTPARAM_HUNG_TASK_PANIC=y
    CONFIG_BOOTPARAM_HUNG_TASK_PANIC_VALUE=1
    # CONFIG_SCHED_DEBUG is not set
    # CONFIG_SCHEDSTATS is not set
    # CONFIG_TIMER_STATS is not set
    # CONFIG_DEBUG_OBJECTS is not set
    # CONFIG_SLUB_DEBUG_ON is not set
    # CONFIG_SLUB_STATS is not set
    # CONFIG_DEBUG_KMEMLEAK is not set
    # CONFIG_DEBUG_RT_MUTEXES is not set
    # CONFIG_RT_MUTEX_TESTER is not set
    # CONFIG_DEBUG_SPINLOCK is not set
    # CONFIG_DEBUG_MUTEXES is not set
    CONFIG_BKL=y
    # CONFIG_DEBUG_LOCK_ALLOC is not set
    # CONFIG_PROVE_LOCKING is not set
    # CONFIG_SPARSE_RCU_POINTER is not set
    # CONFIG_LOCK_STAT is not set
    # CONFIG_DEBUG_SPINLOCK_SLEEP is not set
    # CONFIG_DEBUG_LOCKING_API_SELFTESTS is not set
    # CONFIG_DEBUG_KOBJECT is not set
    # CONFIG_DEBUG_HIGHMEM is not set
    CONFIG_DEBUG_BUGVERBOSE=y
    # CONFIG_DEBUG_INFO is not set
    # CONFIG_DEBUG_VM is not set
    # CONFIG_DEBUG_WRITECOUNT is not set
    CONFIG_DEBUG_MEMORY_INIT=y
    # CONFIG_DEBUG_LIST is not set
    # CONFIG_TEST_LIST_SORT is not set
    # CONFIG_DEBUG_SG is not set
    # CONFIG_DEBUG_NOTIFIERS is not set
    # CONFIG_DEBUG_CREDENTIALS is not set
    CONFIG_FRAME_POINTER=y
    # CONFIG_BOOT_PRINTK_DELAY is not set
    # CONFIG_RCU_TORTURE_TEST is not set
    # CONFIG_KPROBES_SANITY_TEST is not set
    # CONFIG_BACKTRACE_SELF_TEST is not set
    # CONFIG_DEBUG_BLOCK_EXT_DEVT is not set
    # CONFIG_DEBUG_FORCE_WEAK_PER_CPU is not set
    # CONFIG_LKDTM is not set
    # CONFIG_FAULT_INJECTION is not set
    # CONFIG_LATENCYTOP is not set
    # CONFIG_SYSCTL_SYSCALL_CHECK is not set
    # CONFIG_PAGE_POISONING is not set
    CONFIG_HAVE_FUNCTION_TRACER=y
    CONFIG_HAVE_DYNAMIC_FTRACE=y
    CONFIG_HAVE_FTRACE_MCOUNT_RECORD=y
    CONFIG_TRACING_SUPPORT=y
    # CONFIG_FTRACE is not set
    CONFIG_DYNAMIC_DEBUG=y
    # CONFIG_ATOMIC64_SELFTEST is not set
    # CONFIG_SAMPLES is not set
    CONFIG_HAVE_ARCH_KGDB=y
    # CONFIG_KGDB is not set
    # CONFIG_STRICT_DEVMEM is not set
    # CONFIG_ARM_UNWIND is not set
    # CONFIG_DEBUG_USER is not set
    # CONFIG_DEBUG_ERRORS is not set
    # CONFIG_DEBUG_STACK_USAGE is not set
    CONFIG_DEBUG_LL=y
    CONFIG_EARLY_PRINTK=y
    # CONFIG_DEBUG_ICEDCC is not set
    # CONFIG_OC_ETM is not set

    #
    # Security options
    #
    CONFIG_KEYS=y
    CONFIG_KEYS_DEBUG_PROC_KEYS=y
    # CONFIG_SECURITY_DMESG_RESTRICT is not set
    CONFIG_SECURITY=y
    # CONFIG_SECURITYFS is not set
    CONFIG_SECURITY_NETWORK=y
    # CONFIG_SECURITY_NETWORK_XFRM is not set
    # CONFIG_SECURITY_PATH is not set
    # CONFIG_SECURITY_TOMOYO is not set
    # CONFIG_SECURITY_APPARMOR is not set
    # CONFIG_IMA is not set
    CONFIG_DEFAULT_SECURITY_DAC=y
    CONFIG_DEFAULT_SECURITY=""
    CONFIG_CRYPTO=y

    #
    # Crypto core or helper
    #
    CONFIG_CRYPTO_ALGAPI=y
    CONFIG_CRYPTO_ALGAPI2=y
    CONFIG_CRYPTO_AEAD2=y
    CONFIG_CRYPTO_BLKCIPHER=y
    CONFIG_CRYPTO_BLKCIPHER2=y
    CONFIG_CRYPTO_HASH=y
    CONFIG_CRYPTO_HASH2=y
    CONFIG_CRYPTO_RNG2=y
    CONFIG_CRYPTO_PCOMP2=y
    CONFIG_CRYPTO_MANAGER=y
    CONFIG_CRYPTO_MANAGER2=y
    CONFIG_CRYPTO_MANAGER_DISABLE_TESTS=y
    # CONFIG_CRYPTO_GF128MUL is not set
    # CONFIG_CRYPTO_NULL is not set
    CONFIG_CRYPTO_WORKQUEUE=y
    # CONFIG_CRYPTO_CRYPTD is not set
    # CONFIG_CRYPTO_AUTHENC is not set
    # CONFIG_CRYPTO_TEST is not set

    #
    # Authenticated Encryption with Associated Data
    #
    # CONFIG_CRYPTO_CCM is not set
    # CONFIG_CRYPTO_GCM is not set
    # CONFIG_CRYPTO_SEQIV is not set

    #
    # Block modes
    #
    CONFIG_CRYPTO_CBC=y
    # CONFIG_CRYPTO_CTR is not set
    # CONFIG_CRYPTO_CTS is not set
    # CONFIG_CRYPTO_ECB is not set
    # CONFIG_CRYPTO_LRW is not set
    # CONFIG_CRYPTO_PCBC is not set
    # CONFIG_CRYPTO_XTS is not set

    #
    # Hash modes
    #
    # CONFIG_CRYPTO_HMAC is not set
    # CONFIG_CRYPTO_XCBC is not set
    # CONFIG_CRYPTO_VMAC is not set

    #
    # Digest
    #
    # CONFIG_CRYPTO_CRC32C is not set
    # CONFIG_CRYPTO_GHASH is not set
    # CONFIG_CRYPTO_MD4 is not set
    CONFIG_CRYPTO_MD5=y
    # CONFIG_CRYPTO_MICHAEL_MIC is not set
    # CONFIG_CRYPTO_RMD128 is not set
    # CONFIG_CRYPTO_RMD160 is not set
    # CONFIG_CRYPTO_RMD256 is not set
    # CONFIG_CRYPTO_RMD320 is not set
    # CONFIG_CRYPTO_SHA1 is not set
    # CONFIG_CRYPTO_SHA256 is not set
    # CONFIG_CRYPTO_SHA512 is not set
    # CONFIG_CRYPTO_TGR192 is not set
    # CONFIG_CRYPTO_WP512 is not set

    #
    # Ciphers
    #
    CONFIG_CRYPTO_AES=m
    # CONFIG_CRYPTO_ANUBIS is not set
    # CONFIG_CRYPTO_ARC4 is not set
    # CONFIG_CRYPTO_BLOWFISH is not set
    # CONFIG_CRYPTO_CAMELLIA is not set
    # CONFIG_CRYPTO_CAST5 is not set
    # CONFIG_CRYPTO_CAST6 is not set
    CONFIG_CRYPTO_DES=y
    # CONFIG_CRYPTO_FCRYPT is not set
    # CONFIG_CRYPTO_KHAZAD is not set
    # CONFIG_CRYPTO_SALSA20 is not set
    # CONFIG_CRYPTO_SEED is not set
    # CONFIG_CRYPTO_SERPENT is not set
    # CONFIG_CRYPTO_TEA is not set
    # CONFIG_CRYPTO_TWOFISH is not set

    #
    # Compression
    #
    # CONFIG_CRYPTO_DEFLATE is not set
    # CONFIG_CRYPTO_ZLIB is not set
    # CONFIG_CRYPTO_LZO is not set

    #
    # Random Number Generation
    #
    # CONFIG_CRYPTO_ANSI_CPRNG is not set
    # CONFIG_CRYPTO_HW is not set
    # CONFIG_BINARY_PRINTF is not set

    #
    # Library routines
    #
    CONFIG_BITREVERSE=y
    CONFIG_GENERIC_FIND_LAST_BIT=y
    CONFIG_CRC_CCITT=y
    CONFIG_CRC16=y
    # CONFIG_CRC_T10DIF is not set
    # CONFIG_CRC_ITU_T is not set
    CONFIG_CRC32=y
    # CONFIG_CRC7 is not set
    # CONFIG_LIBCRC32C is not set
    CONFIG_ZLIB_INFLATE=y
    CONFIG_ZLIB_DEFLATE=y
    CONFIG_LZO_DECOMPRESS=y
    CONFIG_DECOMPRESS_GZIP=y
    CONFIG_DECOMPRESS_BZIP2=y
    CONFIG_DECOMPRESS_LZMA=y
    CONFIG_DECOMPRESS_LZO=y
    CONFIG_HAS_IOMEM=y
    CONFIG_HAS_IOPORT=y
    CONFIG_HAS_DMA=y
    CONFIG_NLATTR=y

  • Craig,

    Craig Matsuura85376 said:
    I discovered the file I'm using with aplay is a mono 16-bit LE, 8000Hz.  If I play the same file converted to stereo, all sounds correct.

    Yes, I think you should work with stereo mode, mono is not supported.

    http://processors.wiki.ti.com/index.php/TI81XX_PSP_AUDIO_Driver_User_Guide

    This section describes the features supported by ALSA SoC Audio driver.

    • Supports AIC31 audio codec on DM81xx in ALSA SoC framework.
    • Multiple sample rates support (8KHz, 11.025KHz, 16KHz, 22.05KHz, 32KHz, 44.1KHz, 48KHz, 64KHz, 88.2KHz and 96KHz) for both capture and playback.
    • Supports audio in stereo mode.


    A minimal playback application
    This program opens an audio interface for playback, configures it for stereo, 16 bit, 44.1kHz, interleaved conventional read/write access.


    Regards,
    Pavel

  • So other that have a problem like this can get there mono files to work they can add thefollowing to the /etc/asound.conf or the home directory .asoundrc

    pcm.main {
    type hw
    card 0
    device 0
    }

    pcm.!mono {
    type route
    slave.pcm main
    slave.channels 2
    ttable.0.0 1
    ttable.0.1 1
    ttable.1.0 1
    ttable.1.1 1
    }

    pcm.!default mono

    Using aplay now plays audio correctly.