This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GPIO interrupt error

Hello, i am trying to do a very basic gpio interrupt example.

I have declared a GPIO as input in order to catch an interrupt in that pin.

However, i'm having some problems in preparing the interrupt. I catch the c5515.cmd and vectors.asm from an example Project and when i compile i have the next error: "Illegal directive or mnemonic".

The vector.asm is the next one:

*****************************************************************************

*  Copyright (c) 2005  Texas Instruments, Inc. All Rights Reserved          *

*  This is proprietary information, not to be published -- TI INTERNAL DATA *

*****************************************************************************        

.mmregs

        

.include "lpva200.inc"   

        

        

.C54CM_off        

.CPL_off        

.ARMS_off

  

;**********************************************************************************

;        predefined stack operation modes 

;**********************************************************************************

;        USE_RETA     : 2x16-bit fast return mode (RETA used)

;        NO_RETA      : 2x16-bit slow return mode (RETA not used)

;        C54X_STK     : 32-bit fast return mode

;**********************************************************************************           

;.global _DMA_Isr        

;.global _SAR_Isr         

;.global _I2S0_TX_Isr        

;.global _I2S1_RX_Isr        

.global _RTC_Isr

.global _Timer_isr

            

;**********************************************************************************       

.sect "vectors"       

.align 256        

;**********************************************************************************

;****************************************************************************

;* Other interrupt vector definitions go here

;****************************************************************************

.def _RST

_RST:

.ivec    reset_isr, USE_RETA; Reset / Software Interrupt #0

NMI:

.ivec    reset_isr ; Nonmaskable Interrupt

INT0:

.ivec    dummy_isr ; External User Interrupt #0

INT1:

.ivec    dummy_isr ; External User Interrupt #1

TINT0:

.ivec    _Timer_isr ; Timer #0 / Software Interrupt #4

;PROG0: .ivec    _I2S0_TX_Isr ; Programmable 0 Interrupt

PROG0:

.ivec    dummy_isr ; Programmable 0 Interrupt

UART:

.ivec    dummy_isr ; IIS #1 Receive Interrupt

PROG1:

.ivec    dummy_isr ; Programmable 1 Interrupt

;DMA: .ivec    _DMA_Isr                ; DMA Interrupt

DMA:

.ivec    dummy_isr                ; DMA Interrupt

PROG2:

.ivec    dummy_isr ; Programmable 2 Interrupt

COPROCFFT:

  .ivec    dummy_isr ; Coprocessor FFT Module Interrupt

;PROG3: .ivec    _I2S1_RX_Isr ; Programmable 3 Interrupt

PROG3:

.ivec    dummy_isr ; Programmable 3 Interrupt

LCD:

.ivec dummy_isr ; LCD Interrupt

SARADC:

.ivec    dummy_isr ; SAR ADC Interrupt

XMIT2:

.ivec dummy_isr     ; I2S2 Tx Interrupt

RCV2:

.ivec dummy_isr     ; I2S2 Rx Interrupt

XMIT3:

.ivec dummy_isr     ; I2S3 Tx Interrupt

RCV3:

.ivec dummy_isr     ; I2S3 Rx Interrupt

RTC:

.ivec    _RTC_Isr ; RTC interrupt

SPI:

    .ivec    dummy_isr ; SPI Receive Interrupt

USB:

.ivec    dummy_isr ; USB Transmit Interrupt

GPIO:

.ivec    dummy_isr ; GPIO Interrupt

EMIF:

    .ivec    dummy_isr     ; EMIF Interrupt

I2C:

.ivec    dummy_isr ; IIC interrupt

BERRIV:

IV24:

.ivec dummy_isr   ; Bus error interrupt;   

.ref  _DLOGINT_isr

DLOGIV:

IV25:

.ivec   dummy_isr  ; Data log (RTDX) interrupt

; .ref _RTOSINT_isr

RTOSIV:

IV26:

.ivec dummy_isr  ; Real-time OS interrupt

IV27:

.ivec dummy_isr  ; General-purpose software-only interrupt

IV28:

.ivec dummy_isr  ; General-purpose software-only interrupt

IV29:

.ivec dummy_isr  ; General-purpose software-only interrupt

IV30:

.ivec dummy_isr  ; General-purpose software-only interrupt

IV31:

.ivec dummy_isr  ; General-purpose software-only interrupt

 

;****************************************************************************

;* Reset

;****************************************************************************

.text

.def reset_isr

.ref _c_int00       

.align 2

reset_isr:

; *port(#0x1C01) = #0x0 ; Clear idles

bit (ST1, #11) = #1 ; Disable interrupts

    @IVPD_L = #(_RST >> 8) || mmap()

    @IVPH_L = #(_RST >> 8) || mmap()  

bit(ST3,#7) = #0 ; Clear bus error interrupts  

bit(ST3,#2) = #1 ; shut off clockout port  

bit(ST1,#13) = #0 ; shut off XF port

@#IFR0_L = #0xffff || mmap()

; clear all pending interrupts

@#IFR1_L = #0xffff || mmap()

*port(#IDLE_ICR) = #(RESERVED_ICR|IPORT_IDLE|HWA_IDLE|DPORT_IDLE)

idle

;**********************************************************************************

;     Reset all peripherals

;**********************************************************************************

*port(#0x1C04) = 0x1

nop_16

*port(#0x1C05) = 0x00FB

; Reset all peripherals

nop_16

 

;**********************************************************************************

;     Enalbe EMIF

;**********************************************************************************

    *port(IDLE_PCGCR) = #0x0   

;/* Config EMIF - System Control Regsiter */

    *port(#0x1C33) = #0x0    

;// for SRAM in memory card (Async_CE1)   

;/* Config EMIF - ASYNC Regsiters */

    *port(#0x1004) = #0x0080    

    *port(#0x1005) = #0x00E4    

;/* Configure as 16-bit data bus */      

;// Async4 ==> Async_CE1 (SRAM)

    *port(#0x101C) = #0x40AD    

    *port(#0x101D) = #0x0020       

;// Async3 ==> Async_CE0(Flash)

    *port(#0x1018) = #0xFFFD    

    *port(#0x1019) = #0x3FFF       

;// do not assign Async_CE0 and Async_CE1 for NAND

    *port(#0x1060) = #0x0003       

;// Turn off page mode for all Chip Selects

    *port(#0x1068) = #0xFCFC    

    *port(#0x1069) = #0xFCFC    

goto _c_int00


********************************************************************************

** Name     : no_isr                                                          **

**                                                                            **

** Purpose  : Spurious interrupt handler                                      **

**                                                                            **

** Author   :                                                                 **

**                                                                            **

********************************************************************************          

.text  

no_isr:

      goto no_isr  

dummy_isr:

    return_int 

   

.end

The fact is that in the example Project there is no error

Thanks in advanced