Dear,
We have to run WIFI maximum throughput test (iperf) in SDR104 mode (SDIO 3.0, 1.8v, UHS-I). We understand OMAP5432 EVM
supports SDR104 (UHS-1), because micro SD card connector is connected to MMC1 module. Main features of the MMC/SDIO
host controllers are:
-Dedicated DLL to support SDR104 mode (MMC1 only)
We will use the GLSDK to create a Linux BSP. Could you please help to tell us if the BSP of OMAP5432 support running
with SDIO 3.0 card in SDR104 mode by default (mmc1 with a WIFI module/SDIO3.0 instead of a SD card)?
Software Development Kits (Evaluation-SW) for OMAP5432 processor-based EVM
http://www.ti.com/tool/omap5432-evm-eval-sw
LINUX-YOCTO-EVALUATION-SW-OMAP5432-EVM:
Linux (Yocto based) Evaluation SW for OMAP5432 EVM
And, does OMAP5432’ SDIO 3.0 (not SD 3.0) be verified in any EV board?
Thanks a lot.
BR
Keith