This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We have a C6455 EVM to check the SRIO program. We use the example program 'master_slave' and modify it to 1x mode. It works well on the EVM. But when I run the same program on our C6455 board, it fails. I find out that:
1, It fails during the SRIO nitialization, that is the SRIO link can't handshake. It loops the following code. Also, if I run the SLAVE DSP before the MASTER DSP , the SLAVE will fail to pass the loop code and the MASTER DSP can pass. If I run the MASTER DSP before the SALVE DSP, the MASTER will fail to pass the loop code and the SLAVE DSP can pass. Who runs first, who die!
do {
status = CSL_srioHwSetup (hSrio, &setup);
if (status != CSL_SOK) {
printf("SRIO: ... Hardware setup, failed\n");
return;
}
delay(100000);
CSL_srioGetHwStatus (hSrio, CSL_SRIO_QUERY_SP_ERR_STAT, &response);
} while(response.data & 0x1);
2,The SRIO CLK on the EVM is 25MHz vs. our board 156.25MHz;
3,The EVM is point to point connected via 4x SRIO vs.our board via 1x SRIO, there 4 DSPs on our board interconnected via SRIO.
4,I can't find other difference.
But WHY the SAME code can't run on our board?
I hope to get your message!
Thanks.
Ma Yongfeng .
Two suggestions to try:
Thank you RandyP!
I have tried configuring the EVM with 1x SRIO and even cut off one of the four lanes to make it sure.So it is really working in 1x mode on the EVM.
I will check the clock difference and hope to work! Thank you again!
HI, I have settled the problem yesterday.
I change the SRIO ref clock from 156.25MHz to 125MHz and insert some delay in the program. It is OK. WHY?
In fact, the hardware is designen by another engineer , the 156.25MHz is selected optionally.
Yes,I changed some settings...
pSetup->periCntlSetup.prescalar = CSL_SRIO_CLK_PRESCALE_6;
pSetup->serDesPllCfg[0].pllMplyFactor = CSL_SRIO_SERDES_PLL_MPLY_BY_10;
pSetup->portIpPrescalar = 25;
Some of them is not so clear to me.
I have to read the datasheet carefully.
It is a good place to discuss problems here, but my English is poor....