This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2H06 DDR3 PGSR0 Errors

Expert 1800 points

Other Parts Discussed in Thread: 66AK2H06

Hi,

We are testing our custom board based on 66AK2H06. We are facing issues with ddr_reset_workaround in U-Boot.  

DDR3A PGSR0 and DDR3B PGSR0 always detects leveling errors.  Write Leveling Error, DQS Gate Training Error, Write Leveling Adjustment Error bits are always set for both DDR3A and DDR3B.  

We disabled the DDR reset workaround in U-Boot temporarily and postponed the investigation.  We did not face any issues with DDR.  But when we started doing  reboot tests for the board and we see that after approx 60 reboots, the DDR initialization fails.  The problem observed was similar to that KeyStoneII.BTS_errata_advisory.21 (DDR3 Leveling issue).  Before enabling the ddr_rest_workaround, we have figure out why PGSR0 status reports leveling errors all the time.  

 We are using Samsung K4B2G1646Q-BCK0 device and tested both Speed grades 1333 and 1600.

Please let us know how to proceed on this issue.

Thanks

Rams

  • Hi Rams,
    Do you see this behavior with all the custom board?
  • Hi Rajasekaran,

    Yes, the behavior is same on all our custom boards.

    Thanks
    Rams
  • Rams,

    Your problem report is confusing in the way that you present the results from your different tests.  Please describe each test and then the result for it clearly.  I think you have 2 tests:

    1.  Standard configuration sequence as contained in uboot code from TI:

    Does this fail leveling on DDR3A and DDR3B on every test run?

    Does leveling fail on DDR3A and DDR3B on every board tested?

    2.  You modified the configuration sequence to disable the DDR reset workaround:

    It appears that it now executes without leveling error.  Is this true?

    Was removal of the DDR reset the only change?

    This test failed after 60 reboots.  Did both DDR3A and DDR3B fail or just one of them?

     

    The DDR3 layouts must meet the length matching rules stated in the DDR3 Design Requirements for KeyStone Devices Application Report (SPRABI1B).  Some PCB layout tools can generate length matching reports automatically.  Otherwise this will need to be generated by hand.  Please provide this report for review.  Below is an example for a discrete layout (this is easier for DIMM layouts):

    Shn_EVM_DDR3_Rules_1201.xls

    The attached spreadsheet is useful for calculating the proper register settings.  It will be released on the K2H web page in the next few weeks.  Please fill out this spreadsheet and attach it.

    4137.K2 DDR3 Register Calc v1p51.xlsx

    We request that customers validate their board design using a GEL file for configuration.  Have you done this?  Please provide this GEL file containing the above calculated register values for review.  If you need the latest K2HK EVM GEL file, it can be downloaded in the latest EMU pack at: http://software-dl.ti.com/sdoemb/sdoemb_public_sw/ti_emupack_keystone2/1_1_0_0/exports/ti_emupack_keystone2_setup_1.1.0.0.exe

    Tom

     

  • Hi Tom,
    Thanks a lot for your response. I will answer your questions first and send you the gel file with register values.
    1. Standard configuration sequence as contained in uboot code from TI:

    Does this fail leveling on DDR3A and DDR3B on every test run?

    Rams> Yes, it fails levelling on DDR3A and DDR3B on every test run.

    Does leveling fail on DDR3A and DDR3B on every board tested?

    Rams> Yes

    2. You modified the configuration sequence to disable the DDR reset workaround:

    It appears that it now executes without leveling error. Is this true?

    Rams> After disabling the DDR reset workaround, it now executes and appears to be without leveling errors.

    Was removal of the DDR reset the only change?

    Rams> Yes, that was the only change

    This test failed after 60 reboots. Did both DDR3A and DDR3B fail or just one of them?

    Rams> We detected failure in DDR3A and ARM as stopped in U-boot. We could not verify the DDR3B.

    I will soon send you the DDR3 layout and the register settings

    Thanks
    Rams
  • Hi Tom,

    Please find the DDR3 layout report spreadsheet and the DDR3 configuration of our custom board.

    K2_DDR3_length

    K2_DDR3_Config

    Let me know your comments.

    Thanks

    Rams

  • Hi Tom,

    Do you have any feedback for us ?

    Thanks
    Rams
  • Rams,

    The length matching for the Clock, Address, Command and Control nets is not complete.  These must be routed in a fly-by configuration.  Then the routes must be length matched for each segment.  For instance, lets assume the fly-by connections are:

    DSP -> SDRAM1 -> SDRAM2 -> SDRAM3 -> SDRAM4 -> VTT_terminations

    Then the length matching must show the rule are met for:

    DSP -> SDRAM1

    DSP -> SDRAM2

    DSP -> SDRAM3

    DSP -> SDRAM4

    Please provide this information.

    Tom

     

  • Hi Tom!
    The figures given in the spreadsheet for the address and command interface are distance between K2 and SDRAM4. The distance between each RAM-chip is close to ideal (delta between SDRAM1 – SDRAM2, SDRAM2 – SDRAM3 and SDRAM3 – SDRAM4). So the length-matching is done between K2 and SDRAM1.

    Sverre
  • Sverre,

    That is not sufficient.  You need to match the lengths as I said:

    DSP -> SDRAM1
    DSP -> SDRAM2
    DSP -> SDRAM3
    DSP -> SDRAM4

    If you match SDRAM to SDRAM, then you are including stub routing twice in the calculations.  Via placement can also cause incorrect fly-by length matching.  Fly-by routing must be individually length matched from the DSP to each SDRAM.  Please populate the table with this information.

    Tom

     

  • Hi Tom,

    We are awaiting details from our layout consultant. But we were able to run DDR3 at 1300 and 1600 speed. Do you still suspect the issue could be related with layout?

    Regards
    Rams
  • Hi Tom!

    We have made some updates.

    On the B-bank there are some small violations (less than 2.5 mils) in command/address lines if we calculate in this way. 

    DDR3_length_matching :

    /cfs-file/__key/communityserver-discussions-components-files/791/5344.K2_5F00_DDR3_5F00_LENGTHMATCHING.xlsx

  • Those small violations would not cause 100% failure.  There is something more fundamental here.  However, the layout should be improved in a future revision to obtain the required margins for robustness.

    You indicated that you tested at 1300 and 1600.  Did you see the same failure at both speeds?

    I am still waiting for a completed K2 REG_CALC spreadsheet.  The spreadsheet and associated App Note are now on the K2H TI product page.  Also, we need to know whether you see the same failure when using a TI-provided GEL file which has been updated with the register values associated with your design.  It is too complicated to debug a board layout through uboot debugging.

    Tom

     

  • Hi Tom!
    The figures in the spreadsheet you sent us: What EVM is that for? I does not fit the Advantek EVM for K2.

    BR

    Sverre
  • Sverre,

    The DDR3 length matching template provided actually is from the C6678 EVM also produced by Advantech.  The spreadsheet is formatted in an easily understandable format.  As a template, it is equally applicable for K2 DDR3 layouts.

    Tom

     

     

  • Hi Tom,

    We have reviewed our configurations settings against the excel sheet values. According to SPRABX7, section 3.4.1, the default is ECC enable. We do not have ECC, we had to explicitly clear DATX8 General configuration Register (address offset 0x3C0) to disable the leveling and training for the ECC byte lane. This cleared our PGSR0 errors.

    Thanks for the help and SPRABX7 document was very useful.

    Thanks
    Rams