Hi,
I am flashing IBL program to C6678 EVM. With both BIOS MCSDK 2.0 User Guide and some posts, such as this one:
(e) Load i2cConfig.gel (in CCSv5 Tools->GEL Files, right click mouse in GEL Files
window and select "Load GEL"
(f) Run the GEL script "EVM c6678 IBL"->setConfig_c6678_main, this will set the
default boot parameters for booting application images from NOR, NAND and
Ethernet.
After loading i2cConfig.gel, I cannot "Run the GEL script "EVM c6678 IBL"->setConfig_c6678_main ". I have check under menu "Scripts", which has no drop down menu shown when clicking on "Scripts". That is, I am stuck at "EVM c6678 IBL"->setConfig_c6678_main ".
CCS version 5.3.0.00090, Ubuntu 14.04, 32-bit. Can you tell me where to find scripts: "EVM c6678 IBL"->setConfig_c6678_main "?
Thanks,