This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6713B PLLCSR Reserved Bits 2 and 5 are set



I am bringing up a custom board with the C6713B processor. When trying to configure and enable the PLL my target gets lost and try to execute from a random location right after I try to enable the PLL. When looking from the memory browser I can see that after I attempt to enable the PLL the settings go back to the defaults. Occassionally instead of going back to the defaults I receive a value of 0x64 or 0x60 for PLLCSR. The data sheet shows bits 2 and 5 as reserved but the thread included below says these relate to the status of the PLL. Can I get a summary of what bits 2, 4, and 5 represent? My PLL settings work on the DSK6713 so it shouldn't be my code. The electronics team left out the EMI filter on the PLLHV. Could this be related?

https://e2e.ti.com/support/dsp/tms320c6000_high_performance_dsps/f/115/p/143068/529283

Thanks