This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AIF2 CPRI LTE 10MHz AxC mapping

Other Parts Discussed in Thread: TCI6638K2K

Hi,

I have a question regarding the mapping of the AxC samples in 10 MHz LTE configuration of CPRI protocol using AIF2 on TCI6638K2K.

I'd like to set the following mapping on CPRI link 0 (link rate = 4x):

 //For 15.36MHz  {AxC0, AxC1, AxC0, AxC1, AxC0, AxC1, AxC0, AxC1, null , null , null , null , null , null , null , null}

I have changed the following part of code:

   PeLinkSetup.PeCpriDualBitMap.DbmX = 15;

   PeCommonSetup.ChIndex0       [0] = 0;
   PeCommonSetup.bEnableChIndex0[0] = TRUE;
   PeCommonSetup.CpriPktEn0     [0] = FALSE;

   PeCommonSetup.ChIndex0       [1] = 1;
   PeCommonSetup.bEnableChIndex0[1] = TRUE;
   PeCommonSetup.CpriPktEn0     [1] = FALSE;

   PeCommonSetup.ChIndex0       [2] = 0;
   PeCommonSetup.bEnableChIndex0[2] = TRUE;
   PeCommonSetup.CpriPktEn0     [2] = FALSE;

   PeCommonSetup.ChIndex0       [3] = 1;
   PeCommonSetup.bEnableChIndex0[3] = TRUE;
   PeCommonSetup.CpriPktEn0     [3] = FALSE;

   PeCommonSetup.ChIndex0       [4] = 0;
   PeCommonSetup.bEnableChIndex0[4] = TRUE;
   PeCommonSetup.CpriPktEn0     [4] = FALSE;

   PeCommonSetup.ChIndex0       [5] = 1;
   PeCommonSetup.bEnableChIndex0[5] = TRUE;
   PeCommonSetup.CpriPktEn0     [5] = FALSE;

   PeCommonSetup.ChIndex0       [6] = 0;
   PeCommonSetup.bEnableChIndex0[6] = TRUE;
   PeCommonSetup.CpriPktEn0     [6] = FALSE;

   PeCommonSetup.ChIndex0       [7] = 1;
   PeCommonSetup.bEnableChIndex0[7] = TRUE;
   PeCommonSetup.CpriPktEn0     [7] = FALSE;

   PdLinkSetup.PdCpriDualBitMap.DbmX = 15;
  
    PdLinkSetup.CpriDmaCh[0]       = 0;       
    PdLinkSetup.bEnableCpriX[0]    = TRUE;                          
    PdLinkSetup.bEnableCpriPkt[0]  = FALSE;                       
    PdLinkSetup.Cpri8WordOffset[0] = 0;

    PdLinkSetup.CpriDmaCh[1]       = 1;       
    PdLinkSetup.bEnableCpriX[1]    = TRUE;                          
    PdLinkSetup.bEnableCpriPkt[1]  = FALSE;                       
    PdLinkSetup.Cpri8WordOffset[1] = 0;

    PdLinkSetup.CpriDmaCh[2]       = 0;       
    PdLinkSetup.bEnableCpriX[2]    = TRUE;                          
    PdLinkSetup.bEnableCpriPkt[2]  = FALSE;                       
    PdLinkSetup.Cpri8WordOffset[2] = 0;   

    PdLinkSetup.CpriDmaCh[3]       = 1;       
    PdLinkSetup.bEnableCpriX[3]    = TRUE;                          
    PdLinkSetup.bEnableCpriPkt[3]  = FALSE;                       
    PdLinkSetup.Cpri8WordOffset[3] = 0;

    PdLinkSetup.CpriDmaCh[4]       = 0;       
    PdLinkSetup.bEnableCpriX[4]    = TRUE;                          
    PdLinkSetup.bEnableCpriPkt[4]  = FALSE;                       
    PdLinkSetup.Cpri8WordOffset[4] = 0;
   

    PdLinkSetup.CpriDmaCh[5]       = 1;       
    PdLinkSetup.bEnableCpriX[5]    = TRUE;                          
    PdLinkSetup.bEnableCpriPkt[5]  = FALSE;                       
    PdLinkSetup.Cpri8WordOffset[5] = 0;

    PdLinkSetup.CpriDmaCh[6]       = 0;       
    PdLinkSetup.bEnableCpriX[6]    = TRUE;                          
    PdLinkSetup.bEnableCpriPkt[6]  = FALSE;                       
    PdLinkSetup.Cpri8WordOffset[6] = 0;
   

    PdLinkSetup.CpriDmaCh[7]       = 1;       
    PdLinkSetup.bEnableCpriX[7]    = TRUE;                          
    PdLinkSetup.bEnableCpriPkt[7]  = FALSE;                       
    PdLinkSetup.Cpri8WordOffset[7] = 0;

But unfortunately it does not work correctly. Could you help me to set the correct PE and PD parameters in order to to match the indicated configuration ?

Thanks.

Best Regards.

  • Response may be delayed due to holidays in USA. Thank you for your patience.
  • Hi Angelo,

    This should probably be moved to the private forums.

    It's a bit difficult to debug with only a piece of the configuration. Perhaps you can reduce the number of AxCs/mapping and try to get that working first. (start with 1, then 2, etc). If you look at Table 3-2 and Figure 3-4 of the AIF2 User Guide (SPRUHL2A), you'll see that for 10Mhz LTE with 4x link rate, AIF2 supports 4 AxCs per link, with a mapping of AxC0, AxC1, AxC2, AxC3 per frame. AxCs are mapped to PD/PE channels. UG Section 9.1.4 shows a similar configuration 4x LTE (ignore the RT stuff for 2 DSPs(devices)).

    -dave