This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

usb 3.0 got disconnected

getting this error after booting the board

xhci_hcd 0000:01:00.0: xHCI host not responding to stop endpoint command.
xhci_hcd 0000:01:00.0: Assuming host is dying, halting host.
xhci_hcd 0000:01:00.0: Non-responsive xHCI host is not halting.
xhci_hcd 0000:01:00.0: Completing active URBs anyway.
xhci_hcd 0000:01:00.0: HC died; cleaning up
usb 3-1: USB disconnect, address 2
sd 2:0:0:0: Device offlined - not ready after error recovery
sd 2:0:0:0: [sda] Unhandled error code
sd 2:0:0:0: [sda]  Result: hostbyte=0x01 driverbyte=0x00
sd 2:0:0:0: [sda] CDB: cdb[0]=0x2a: 2a 00 00 00 08 01 00 00 01 00
end_request: I/O error, dev sda, sector 2049
Buffer I/O error on device sda1, logical block 1
lost page write due to I/O error on sda1
No external device has been connected