This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

eMMC 5.0 with DM37xx

Other Parts Discussed in Thread: CSD, DM3730

Hello All,

I have a custom DM37xx based hardware platform that currently boots off a Samsung eMMC.  This eMMC follows an older version of the MMC Spec (3.14) and is supported well by the Linux kernel running on the platform (2.6.37)

I now have a need to interface a more recent eMMC flash memory that follows eMMC specification 5.0.  As expected, Linux-2.6.37 currently running on the platform fails to detect the new eMMC flash memory (reporting errors reading/deciphering the contents of the CSD register)

I am aware that the latest kernel officially supported by TI for the DM37xx EVM is linux-2.6.37, which is way too old to provide a solution to my problem.  

From information available on the internet, I gathered that there are more recent version (Linux-3.14.x) kernels that support DM37xx.  

May I request for members to kindly help find a link to the sources of the most recent version of the Linux kernel that provides support for DM37xx EVM/processor

Thank you for your time.

Best Regards,

Kanagesh