i want to connect two DM8168' io port each other for data communication. one dm8168 chip of the IO ports is configured as output mode,another dm8168 chip of the IO ports is configured as input mode.
my question is whether external pullup/pulldown resistors are needed between io port for meeting the level requirement.