Hello,
we need to run Qt5 with EGLFS platform plugin without Wayland/Weston on TI Sitara AM3359.
1) I've tested Processor SDK 02.00.02 and SDK 03.00.00 with Weston/Wayland. Everything seems to be OK. Then i disabled Weston and tried to execute the Qt5 opengl examples with the platform plugin EGLFS:
/usr/share/qt5/examples/opengl/..
./hellogl2 --platform eglfs --> works
./cube --platform eglfs --> !display remains dark!
I added 'WindowSystem=libpvrDRMWSEGL.so' to /etc/powervr.ini.
How can I solve this?
The EGLFS Plugin is included in the SDK Filesystem: usr/lib/qt5/plugins/platforms
2) I have the same behavior with a Debian 8 based Rootfilesystem and a custom Build of Qt5.5.1. Is there any documentation how to configure (qmake.conf) Qt5 to use SGX with the EGLFS platform plugin?
Is there a documentation which librarys are needed to support SGX with Qt5 platform EGLFS.
Best regards,
Ludwig